49 #define USB_HID_SCLASS_NONE 0x00 50 #define USB_HID_SCLASS_BOOT 0x01 57 #define USB_HID_PROTOCOL_NONE 0 58 #define USB_HID_PROTOCOL_KEYB 1 59 #define USB_HID_PROTOCOL_MOUSE 2 66 #define USB_HID_DTYPE_HID 0x21 67 #define USB_HID_DTYPE_REPORT 0x22 68 #define USB_HID_DTYPE_PHYSICAL 0x23 75 #define USBREQ_GET_REPORT 0x01 76 #define USBREQ_GET_IDLE 0x02 77 #define USBREQ_GET_PROTOCOL 0x03 78 #define USBREQ_SET_REPORT 0x09 79 #define USBREQ_SET_IDLE 0x0a 80 #define USBREQ_SET_PROTOCOL 0x0b 87 #define USB_HID_REPORT_IN 0x01 88 #define USB_HID_REPORT_OUTPUT 0x02 89 #define USB_HID_REPORT_FEATURE 0x03 96 #define USB_HID_PROTOCOL_BOOT 0 97 #define USB_HID_PROTOCOL_REPORT 1 104 #define USB_HID_GENERIC_DESKTOP 0x01 105 #define USB_HID_BUTTONS 0x09 106 #define USB_HID_SENSOR 0x20 107 #define USB_HID_X 0x30 108 #define USB_HID_Y 0x31 109 #define USB_HID_Z 0x32 110 #define USB_HID_RX 0x33 111 #define USB_HID_RY 0x34 112 #define USB_HID_RZ 0x35 114 #define USB_HID_POINTER 0x01 115 #define USB_HID_MOUSE 0x02 116 #define USB_HID_JOYSTICK 0x04 117 #define USB_HID_GAME_PAD 0x05 118 #define USB_HID_KEYBOARD 0x06 119 #define USB_HID_SENSOR_TYPE_COLLECTION 0X01 120 #define USB_HID_ENVIRONMENTAL_TEMPERATURE 0x33 122 #define USB_HID_PHYSICAL 0x00 123 #define USB_HID_APPLICATION 0x01 124 #define USB_HID_LOGICAL 0x02 126 #define USB_HID_USAGE_POINTER 0x0109 127 #define USB_HID_USAGE_BUTTONS 0x0509 128 #define USB_HID_USAGE_LEDS 0x0508 129 #define USB_HID_USAGE_KEYCODES 0x0507 137 #define HID_MOUSE_BUTTON_1 0x01 138 #define HID_MOUSE_BUTTON_2 0x02 139 #define HID_MOUSE_BUTTON_3 0x04 147 #define HID_KEYB_NUM_LOCK 0x01 148 #define HID_KEYB_CAPS_LOCK 0x02 149 #define HID_KEYB_SCROLL_LOCK 0x04 150 #define HID_KEYB_COMPOSE 0x08 151 #define HID_KEYB_KANA 0x10 159 #define HID_KEYB_LEFT_CTRL 0x01 160 #define HID_KEYB_LEFT_SHIFT 0x02 161 #define HID_KEYB_LEFT_ALT 0x04 162 #define HID_KEYB_LEFT_GUI 0x08 163 #define HID_KEYB_RIGHT_CTRL 0x10 164 #define HID_KEYB_RIGHT_SHIFT 0x20 165 #define HID_KEYB_RIGHT_ALT 0x40 166 #define HID_KEYB_RIGHT_GUI 0x80 173 #define HID_KEYB_USAGE_RESERVED 0x00 174 #define HID_KEYB_USAGE_ROLLOVER 0x01 175 #define HID_KEYB_USAGE_A 0x04 176 #define HID_KEYB_USAGE_B 0x05 177 #define HID_KEYB_USAGE_C 0x06 178 #define HID_KEYB_USAGE_D 0x07 179 #define HID_KEYB_USAGE_E 0x08 180 #define HID_KEYB_USAGE_F 0x09 181 #define HID_KEYB_USAGE_G 0x0A 182 #define HID_KEYB_USAGE_H 0x0B 183 #define HID_KEYB_USAGE_I 0x0C 184 #define HID_KEYB_USAGE_J 0x0D 185 #define HID_KEYB_USAGE_K 0x0E 186 #define HID_KEYB_USAGE_L 0x0F 187 #define HID_KEYB_USAGE_M 0x10 188 #define HID_KEYB_USAGE_N 0x11 189 #define HID_KEYB_USAGE_O 0x12 190 #define HID_KEYB_USAGE_P 0x13 191 #define HID_KEYB_USAGE_Q 0x14 192 #define HID_KEYB_USAGE_R 0x15 193 #define HID_KEYB_USAGE_S 0x16 194 #define HID_KEYB_USAGE_T 0x17 195 #define HID_KEYB_USAGE_U 0x18 196 #define HID_KEYB_USAGE_V 0x19 197 #define HID_KEYB_USAGE_W 0x1A 198 #define HID_KEYB_USAGE_X 0x1B 199 #define HID_KEYB_USAGE_Y 0x1C 200 #define HID_KEYB_USAGE_Z 0x1D 201 #define HID_KEYB_USAGE_1 0x1E 202 #define HID_KEYB_USAGE_2 0x1F 203 #define HID_KEYB_USAGE_3 0x20 204 #define HID_KEYB_USAGE_4 0x21 205 #define HID_KEYB_USAGE_5 0x22 206 #define HID_KEYB_USAGE_6 0x23 207 #define HID_KEYB_USAGE_7 0x24 208 #define HID_KEYB_USAGE_8 0x25 209 #define HID_KEYB_USAGE_9 0x26 210 #define HID_KEYB_USAGE_0 0x27 211 #define HID_KEYB_USAGE_ENTER 0x28 212 #define HID_KEYB_USAGE_ESCAPE 0x29 213 #define HID_KEYB_USAGE_BACKSPACE \ 215 #define HID_KEYB_USAGE_TAB 0x2B 216 #define HID_KEYB_USAGE_SPACE 0x2C 217 #define HID_KEYB_USAGE_MINUS 0x2D 218 #define HID_KEYB_USAGE_EQUAL 0x2E 219 #define HID_KEYB_USAGE_LBRACKET 0x2F 220 #define HID_KEYB_USAGE_RBRACKET 0x30 221 #define HID_KEYB_USAGE_BSLASH 0x31 222 #define HID_KEYB_USAGE_SEMICOLON \ 224 #define HID_KEYB_USAGE_FQUOTE 0x34 225 #define HID_KEYB_USAGE_BQUOTE 0x35 226 #define HID_KEYB_USAGE_COMMA 0x36 227 #define HID_KEYB_USAGE_PERIOD 0x37 228 #define HID_KEYB_USAGE_FSLASH 0x38 229 #define HID_KEYB_USAGE_CAPSLOCK 0x39 230 #define HID_KEYB_USAGE_F1 0x3A 231 #define HID_KEYB_USAGE_F2 0x3B 232 #define HID_KEYB_USAGE_F3 0x3C 233 #define HID_KEYB_USAGE_F4 0x3D 234 #define HID_KEYB_USAGE_F5 0x3E 235 #define HID_KEYB_USAGE_F6 0x3F 236 #define HID_KEYB_USAGE_F7 0x40 237 #define HID_KEYB_USAGE_F8 0x41 238 #define HID_KEYB_USAGE_F9 0x42 239 #define HID_KEYB_USAGE_F10 0x43 240 #define HID_KEYB_USAGE_F11 0x44 241 #define HID_KEYB_USAGE_F12 0x45 242 #define HID_KEYB_USAGE_SCROLLOCK \ 244 #define HID_KEYB_USAGE_PAGE_UP 0x4B 245 #define HID_KEYB_USAGE_PAGE_DOWN \ 247 #define HID_KEYB_USAGE_RIGHT_ARROW \ 249 #define HID_KEYB_USAGE_LEFT_ARROW \ 251 #define HID_KEYB_USAGE_DOWN_ARROW \ 253 #define HID_KEYB_USAGE_UP_ARROW 0x52 254 #define HID_KEYB_USAGE_NUMLOCK 0x53 255 #define HID_KEYB_USAGE_KEYPAD_SLASH \ 257 #define HID_KEYB_USAGE_KEYPAD_STAR \ 259 #define HID_KEYB_USAGE_KEYPAD_MINUS \ 261 #define HID_KEYB_USAGE_KEYPAD_PLUS \ 263 #define HID_KEYB_USAGE_KEPAD_ENTER \ 265 #define HID_KEYB_USAGE_KEYPAD_1 0x59 266 #define HID_KEYB_USAGE_KEYPAD_2 0x5A 267 #define HID_KEYB_USAGE_KEYPAD_3 0x5B 268 #define HID_KEYB_USAGE_KEYPAD_4 0x5C 269 #define HID_KEYB_USAGE_KEYPAD_5 0x5D 270 #define HID_KEYB_USAGE_KEYPAD_6 0x5E 271 #define HID_KEYB_USAGE_KEYPAD_7 0x5F 272 #define HID_KEYB_USAGE_KEYPAD_8 0x60 273 #define HID_KEYB_USAGE_KEYPAD_9 0x61 274 #define HID_KEYB_USAGE_KEYPAD_0 0x62 275 #define HID_KEYB_USAGE_KEPAD_PERIOD \ 284 #define USB_HID_COUNTRY_NONE 0x00 285 #define USB_HID_COUNTRY_ARABIC 0x01 286 #define USB_HID_COUNTRY_BELGIAN 0x02 287 #define USB_HID_COUNTRY_CANADA_BI \ 289 #define USB_HID_COUNTRY_CANADA_FR \ 291 #define USB_HID_COUNTRY_CZECH_REPUBLIC \ 293 #define USB_HID_COUNTRY_DANISH 0x06 294 #define USB_HID_COUNTRY_FINNISH 0x07 295 #define USB_HID_COUNTRY_FRENCH 0x08 296 #define USB_HID_COUNTRY_GERMAN 0x09 297 #define USB_HID_COUNTRY_GREEK 0x0A 298 #define USB_HID_COUNTRY_HEBREW 0x0B 299 #define USB_HID_COUNTRY_HUNGARY 0x0C 300 #define USB_HID_COUNTRY_INTERNATIONAL_ISO \ 302 #define USB_HID_COUNTRY_ITALIAN 0x0E 303 #define USB_HID_COUNTRY_JAPAN_KATAKANA \ 305 #define USB_HID_COUNTRY_KOREAN 0x10 306 #define USB_HID_COUNTRY_LATIN_AMERICAN \ 308 #define USB_HID_COUNTRY_NETHERLANDS \ 310 #define USB_HID_COUNTRY_NORWEGIAN \ 312 #define USB_HID_COUNTRY_PERSIAN 0x14 313 #define USB_HID_COUNTRY_POLAND 0x15 314 #define USB_HID_COUNTRY_PORTUGUESE \ 316 #define USB_HID_COUNTRY_RUSSIA 0x17 317 #define USB_HID_COUNTRY_SLOVAKIA \ 319 #define USB_HID_COUNTRY_SPANISH 0x19 320 #define USB_HID_COUNTRY_SWEDISH 0x1A 321 #define USB_HID_COUNTRY_SWISS_FRENCH \ 323 #define USB_HID_COUNTRY_SWISS_GERMAN \ 325 #define USB_HID_COUNTRY_SWITZERLAND \ 327 #define USB_HID_COUNTRY_TAIWAN 0x1E 328 #define USB_HID_COUNTRY_TURKISH_Q \ 330 #define USB_HID_COUNTRY_UK 0x20 331 #define USB_HID_COUNTRY_US 0x21 332 #define USB_HID_COUNTRY_YUGOSLAVIA \ 334 #define USB_HID_COUNTRY_TURKISH_F \ 342 #define USB_HID_INPUT_DATA 0x0000 343 #define USB_HID_INPUT_CONSTANT 0x0001 344 #define USB_HID_INPUT_ARRAY 0x0000 345 #define USB_HID_INPUT_VARIABLE 0x0002 346 #define USB_HID_INPUT_ABS 0x0000 347 #define USB_HID_INPUT_RELATIVE 0x0004 348 #define USB_HID_INPUT_NOWRAP 0x0000 349 #define USB_HID_INPUT_WRAP 0x0008 350 #define USB_HID_INPUT_LINEAR 0x0000 351 #define USB_HID_INPUT_NONLINEAR 0x0010 352 #define USB_HID_INPUT_PREFER 0x0000 353 #define USB_HID_INPUT_NONPREFER 0x0020 354 #define USB_HID_INPUT_NONULL 0x0000 355 #define USB_HID_INPUT_NULL 0x0040 356 #define USB_HID_INPUT_BITF 0x0100 357 #define USB_HID_INPUT_BYTES 0x0000 364 #define USB_HID_FEATURE_DATA 0x0000 365 #define USB_HID_FEATURE_CONSTANT \ 367 #define USB_HID_FEATURE_ARRAY 0x0000 368 #define USB_HID_FEATURE_VARIABLE \ 370 #define USB_HID_FEATURE_ABS 0x0000 371 #define USB_HID_FEATURE_RELATIVE \ 373 #define USB_HID_FEATURE_NOWRAP 0x0000 374 #define USB_HID_FEATURE_WRAP 0x0008 375 #define USB_HID_FEATURE_LINEAR 0x0000 376 #define USB_HID_FEATURE_NONLINEAR \ 378 #define USB_HID_FEATURE_PREFER 0x0000 379 #define USB_HID_FEATURE_NONPREFER \ 381 #define USB_HID_FEATURE_NONULL 0x0000 382 #define USB_HID_FEATURE_NULL 0x0040 383 #define USB_HID_FEATURE_BITF 0x0100 384 #define USB_HID_FEATURE_BYTES 0x0000 391 #define USB_HID_OUTPUT_DATA 0x0000 392 #define USB_HID_OUTPUT_CONSTANT 0x0001 393 #define USB_HID_OUTPUT_ARRAY 0x0000 394 #define USB_HID_OUTPUT_VARIABLE 0x0002 395 #define USB_HID_OUTPUT_ABS 0x0000 396 #define USB_HID_OUTPUT_RELATIVE 0x0004 397 #define USB_HID_OUTPUT_NOWRAP 0x0000 398 #define USB_HID_OUTPUT_WRAP 0x0008 399 #define USB_HID_OUTPUT_LINEAR 0x0000 400 #define USB_HID_OUTPUT_NONLINEAR \ 402 #define USB_HID_OUTPUT_PREFER 0x0000 403 #define USB_HID_OUTPUT_NONPREFER \ 405 #define USB_HID_OUTPUT_NONULL 0x0000 406 #define USB_HID_OUTPUT_NULL 0x0040 407 #define USB_HID_OUTPUT_BITF 0x0100 408 #define USB_HID_OUTPUT_BYTES 0x0000 415 #define USB_HID_BIAS_NOT_APPLICABLE \ 417 #define USB_HID_BIAS_RIGHT_HAND 0x01 418 #define USB_HID_BIAS_LEFT_HAND 0x02 419 #define USB_HID_BIAS_BOTH_HANDS 0x03 420 #define USB_HID_BIAS_EITHER_HAND \ 428 #define USB_HID_DESIGNATOR_NONE 0x00 429 #define USB_HID_DESIGNATOR_HAND 0x01 430 #define USB_HID_DESIGNATOR_EYEBALL \ 432 #define USB_HID_DESIGNATOR_EYEBROW \ 434 #define USB_HID_DESIGNATOR_EYELID \ 436 #define USB_HID_DESIGNATOR_EAR 0x05 437 #define USB_HID_DESIGNATOR_NOSE 0x06 438 #define USB_HID_DESIGNATOR_MOUTH \ 440 #define USB_HID_DESIGNATOR_UPPER_LIP \ 442 #define USB_HID_DESIGNATOR_LOWER_LIP \ 444 #define USB_HID_DESIGNATOR_JAW 0x0A 445 #define USB_HID_DESIGNATOR_NECK 0x0B 446 #define USB_HID_DESIGNATOR_UPPER_ARM \ 448 #define USB_HID_DESIGNATOR_ELBOW \ 450 #define USB_HID_DESIGNATOR_FOREARM \ 452 #define USB_HID_DESIGNATOR_WRIST \ 454 #define USB_HID_DESIGNATOR_PALM 0x10 455 #define USB_HID_DESIGNATOR_THUMB \ 457 #define USB_HID_DESIGNATOR_INDEX_FINGER \ 459 #define USB_HID_DESIGNATOR_MIDDLE_FINGER \ 461 #define USB_HID_DESIGNATOR_RING_FINGER \ 463 #define USB_HID_DESIGNATOR_LITTLE_FINGER \ 465 #define USB_HID_DESIGNATOR_HEAD 0x16 466 #define USB_HID_DESIGNATOR_SHOULDER \ 468 #define USB_HID_DESIGNATOR_HIP 0x18 469 #define USB_HID_DESIGNATOR_WAIST \ 471 #define USB_HID_DESIGNATOR_THIGH \ 473 #define USB_HID_DESIGNATOR_KNEE 0x1B 474 #define USB_HID_DESIGNATOR_CALF 0x1C 475 #define USB_HID_DESIGNATOR_ANKLE \ 477 #define USB_HID_DESIGNATOR_FOOT 0x1E 478 #define USB_HID_DESIGNATOR_HEEL 0x1F 479 #define USB_HID_DESIGNATOR_BALL_OF_FOOT \ 481 #define USB_HID_DESIGNATOR_BIG_TOE \ 483 #define USB_HID_DESIGNATOR_SECOND_TOE \ 485 #define USB_HID_DESIGNATOR_THIRD_TOE \ 487 #define USB_HID_DESIGNATOR_FOURTH_TOE \ 489 #define USB_HID_DESIGNATOR_LITTLE_TOE \ 491 #define USB_HID_DESIGNATOR_BROW 0x26 492 #define USB_HID_DESIGNATOR_CHEEK \ 500 #define USB_HID_QUALIFIER_NOT_APPLICABLE \ 502 #define USB_HID_QUALIFIER_RIGHT (0x01 << 5) 503 #define USB_HID_QUALIFIER_LEFT (0x02 << 5) 504 #define USB_HID_QUALIFIER_BOTH (0x03 << 5) 505 #define USB_HID_QUALIFIER_EITHER \ 507 #define USB_HID_QUALIFIER_CENTER \ 515 #define USBH_HID_MAX_USAGE 256 516 #define USBH_HID_CAPS_ARRAY_SZ (USBH_HID_MAX_USAGE/sizeof(uint32_t)) 541 uint8_t bDescriptorType;
548 PACKED tHIDClassDescriptorInfo;
567 uint8_t bDescriptorType;
595 tHIDClassDescriptorInfo sClassDescriptor[1];
668 #endif // __USBHID_H__ const tHIDKeyboardUsageTable g_sUSKeyboardMap
Definition: usbkeyboardmap.c:120
uint16_t bcdHID
Definition: usbhid.h:574
uint8_t bNumDescriptors
Definition: usbhid.h:588
uint8_t bCountryCode
Definition: usbhid.h:580
uint16_t wDescriptorLength
The total length of the HID class descriptor.
Definition: usbhid.h:546
void * pvCharMapping
Definition: usbhid.h:641
uint8_t ui8BytesPerChar
Definition: usbhid.h:627
#define USBH_HID_CAPS_ARRAY_SZ
Definition: usbhid.h:516
USB_CDC_GET/SET_LINE_CODING request-specific data.
Definition: usbdhidgamepad.h:217