CAN.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2018, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file CAN.h
34  * @brief <b>PRELIMINARY</b> CAN driver interface
35  *
36  * <b>WARNING</b> These APIs are <b>PRELIMINARY</b>, and subject to
37  * change in the next few months.
38  *
39  * To use the CAN driver, ensure that the correct driver library for your
40  * device is linked in and include this header file as follows:
41  * @code
42  * #include <ti/drivers/CAN.h>
43  * @endcode
44  *
45  * This module serves as the main interface for applications. Its purpose
46  * is to redirect the CAN APIs to specific driver implementations
47  * which are specified using a pointer to a #CAN_FxnTable.
48  *
49  * # Overview #
50  * The Controller Area Network (CAN) driver is a generic driver that allows
51  * for communication on a CAN bus. It is a two-wire, half-duplex, LAN system
52  * that is collision free. The main method of transfer is by broadcasting.
53  * The CAN protocol defines the format of data transfer, and this CAN driver
54  * allows full functionality as a transmitting and receiving node on a bus.
55  * However, there can be higher-level software layers and stacks that use this
56  * driver to enable more advanced features.
57  * Functional modes available in this driver include blocking and non-blocking.
58  *
59  * The APIs in this driver serve as an interface to a typical RTOS
60  * application. The specific peripheral implementations are responsible for
61  * creating all the RTOS specific primitives to allow for thread-safe
62  * operation.
63  *
64  * # Usage #
65  *
66  * The CAN driver interface provides device independent APIs, data types,
67  * and macros. The following code example opens a CAN instance, creates
68  * an incrementing CAN frame, and continually writes them to the CAN bus.
69  * NOTE: a CAN receiver on this bus is needed, or else this transmitter will
70  * continually throw an error if it does not detect an ACK.
71  *
72  * @code
73  * uint8_t i;
74  * // Initialize the CAN driver
75  * CAN_init();
76  *
77  * CAN_Handle canHandle;
78  * CAN_Params canParams;
79  * CAN_Params_init(&canParams);
80  * canHandle = CAN_open(Board_CAN0, &canParams);
81  *
82  * if (canHandle == NULL) {
83  * // CAN_open() failed
84  * while (1);
85  * }
86  *
87  * for (i = 0; ; ++i) {
88  * CAN_Frame canFrame[1];
89  * canFrame[0].can_id = i;
90  * canFrame[0].err = 0;
91  * canFrame[0].rtr = 0;
92  * canFrame[0].eff = 1;
93  * canFrame[0].dlc = i % 9;
94  * canFrame[0].data[0] = i;
95  * canFrame[0].data[1] = i + 1;
96  * canFrame[0].data[2] = i + 2;
97  * canFrame[0].data[3] = i + 3;
98  * canFrame[0].data[4] = i + 4;
99  * canFrame[0].data[5] = i + 5;
100  * canFrame[0].data[6] = i + 6;
101  * canFrame[0].data[7] = i + 7;
102  *
103  * CAN_write(canHandle, canFrame, sizeof(canFrame));
104  * }
105  * @endcode
106  *
107  * Details for the example code above are described in the following
108  * subsections.
109  *
110  *
111  * ### CAN Driver Configuration #
112  *
113  * In order to use the CAN APIs, the application is required
114  * to provide device-specific CAN configuration in the Board.c file.
115  * The CAN driver interface defines a configuration data structure:
116  *
117  * @code
118  * typedef struct CAN_Config_ {
119  * CAN_FxnTable const *fxnTablePtr;
120  * void *object;
121  * void const *hwAttrs;
122  * CAN_Frame *rxBufPtr;
123  * CAN_frame *txBufPtr;
124  * size_t rxBufSize;
125  * size_t txBufSize;
126  * } CAN_Config;
127  * @endcode
128  *
129  * You will need to check the device-specific CAN driver implementation's
130  * header file for example configuration. Please also refer to the
131  * Board.c file of any of your examples to see the CAN configuration.
132  *
133  * ### Initializing the CAN Driver #
134  *
135  * CAN_init() must be called before any other CAN APIs. This function
136  * calls the device implementation's CAN initialization function, for each
137  * element of CAN_config[].
138  *
139  * ### Opening the CAN Driver #
140  *
141  * Opening a CAN requires four steps:
142  * 1. Create and initialize a CAN_Params structure.
143  * 2. Fill in the desired parameters.
144  * 3. Call CAN_open(), passing the index of the CAN in the CAN_config
145  * structure, and the address of the CAN_Params structure. The
146  * CAN instance is specified by the index in the CAN_config structure.
147  * 4. Check that the CAN handle returned by CAN_open() is non-NULL,
148  * and save it. The handle will be used to read and write to the
149  * CAN you just opened.
150  *
151  * Only one CAN index can be used at a time; calling CAN_open() a second
152  * time with the same index previously passed to CAN_open() will result in
153  * an error. You can, though, re-use the index if the instance is closed
154  * via CAN_close().
155  * In the example code, Board_CAN0 is passed to CAN_open(). This macro
156  * is defined in the example's Board.h file.
157  *
158  *
159  * ### Modes of Operation #
160  *
161  * The CAN driver can operate in blocking mode or nonblocking mode, by
162  * setting the mode parameters passed to CAN_open().
163  * If these parameters are not set, as in the example code, the CAN
164  * driver defaults to blocking mode. Options for the mode parameter are
165  * #CAN_MODE_BLOCKING and #CAN_MODE_NONBLOCKING:
166  *
167  * - #CAN_MODE_BLOCKING uses a semaphore to block while data is being sent
168  * or read. The context of calling CAN_read() or CAN_write() must be a Task
169  * when using #CAN_MODE_BLOCKING. The CAN_write() or CAN_read() call
170  * will block until all data is sent or received, or the write timeout or
171  * read timeout expires, whichever happens first.
172  *
173  * - #CAN_MODE_NONBLOCKING is non-blocking and CAN_read() and CAN_write()
174  * will return either with the number of bytes successfully read/written,
175  * or a negative error number.
176  *
177  * ### Reading and Writing data #
178  *
179  * The example code reads one CAN frame from the CAN instance, and then writes
180  * one CAN frame back to the same instance:
181  *
182  * @code
183  * CAN_read(can, &canFrame, sizeof(canFrame));
184  * CAN_write(can, &canFrame, sizeof(canFrame));
185  * @endcode
186  *
187  * The CAN driver allows CAN_read() and CAN_write() calls to happen for any
188  * node at any time from the CAN bus. Please see the CAN protocol for how it
189  * handles collisions. The ability to filter incoming messages are also
190  * available through CAN_Params.
191  *
192  * # Implementation #
193  *
194  * The CAN driver interface module is joined (at link time) to an
195  * array of CAN_Config data structures named *CAN_config*.
196  * CAN_config is implemented in the application with each entry being an
197  * instance of a CAN peripheral. Each entry in *CAN_config* contains a:
198  * - (CAN_FxnTable *) to a set of functions that implement a CAN peripheral
199  * - (void *) data object that is associated with the CAN_FxnTable
200  * - (void *) hardware attributes that are associated with the CAN_FxnTable
201  *
202  * The CAN APIs are redirected to the device specific implementations
203  * using the CAN_FxnTable pointer of the CAN_config entry.
204  * In order to use device specific functions of the CAN driver directly,
205  * link in the correct driver library for your device and include the
206  * device specific CAN driver header file (which in turn includes CAN.h).
207  * For example, for the MSP432 family of devices, you would include the
208  * following header file:
209  * @code
210  * #include <ti/drivers/can/CANMSP432.h>
211  * @endcode
212  *
213  * ============================================================================
214  */
215 
216 #ifndef ti_drivers_CAN__include
217 #define ti_drivers_CAN__include
218 
219 #ifdef __cplusplus
220 extern "C" {
221 #endif
222 
223 #include <stddef.h>
224 #include <stdint.h>
225 
226 #include <ti/drivers/can/types.h>
227 
245 #define CAN_CMD_RESERVED (32)
246 
259 #define CAN_STATUS_RESERVED (-32)
260 
274 #define CAN_STATUS_SUCCESS (0)
275 
282 #define CAN_STATUS_ERROR (-1)
283 
291 #define CAN_STATUS_UNDEFINEDCMD (-2)
292 
298 #define CAN_WAIT_FOREVER (~(0U))
299 
303 typedef struct CAN_Config_ *CAN_Handle;
304 
311 typedef enum CAN_Mode_ {
324 } CAN_Mode;
325 
332 typedef enum CAN_Direction_ {
342 } CAN_Direction;
343 
352 typedef struct CAN_Params_ {
353  CAN_Mode mode;
355  uint32_t filterID;
356  uint32_t filterMask;
357  uint32_t readTimeout;
358  uint32_t writeTimeout;
359 } CAN_Params;
360 
373 typedef struct can_frame CAN_Frame;
374 
379 typedef void (*CAN_CloseFxn) (CAN_Handle handle);
380 
385 typedef int_fast16_t (*CAN_ControlFxn) (CAN_Handle handle, uint_fast16_t cmd, void *arg);
386 
391 typedef void (*CAN_InitFxn) (CAN_Handle handle);
392 
397 typedef CAN_Handle (*CAN_OpenFxn) (CAN_Handle handle, CAN_Params *params);
398 
403 typedef int_fast32_t (*CAN_ReadFxn) (CAN_Handle handle, void *buffer,
404  size_t size);
405 
410 typedef int_fast32_t (*CAN_WriteFxn) (CAN_Handle handle, const void *buffer,
411  size_t size);
412 
417 typedef void (*CAN_TxMsgFxn) (CAN_Handle handle);
418 
424 typedef struct CAN_FxnTable_ {
427 
430 
433 
436 
439 
442 
445 } CAN_FxnTable;
446 
458 typedef struct CAN_Config_ {
461 
463  void *object;
464 
466  void const *hwAttrs;
467 
470 
473 
475  size_t rxBufSize;
476 
478  size_t txBufSize;
479 } CAN_Config;
480 
491 extern void CAN_close(CAN_Handle handle);
492 
500 extern void CAN_init(void);
501 
535 extern int_fast16_t CAN_control(CAN_Handle handle, uint_fast16_t cmd, void *arg);
536 
558 extern CAN_Handle CAN_open(uint_least8_t index, CAN_Params *params);
559 
573 extern void CAN_Params_init(CAN_Params *params);
574 
603 extern int_fast32_t CAN_write(CAN_Handle handle, const void *buffer, size_t size);
604 
634 extern int_fast32_t CAN_read(CAN_Handle handle, void *buffer, size_t size);
635 
636 #ifdef __cplusplus
637 }
638 #endif
639 
640 #endif /* ti_drivers_CAN__include */
int_fast32_t CAN_write(CAN_Handle handle, const void *buffer, size_t size)
Function that writes data to a CAN with interrupts enabled.
int_fast32_t(* CAN_ReadFxn)(CAN_Handle handle, void *buffer, size_t size)
A function pointer to a driver specific implementation of CAN_ReadFxn().
Definition: CAN.h:403
int_fast32_t(* CAN_WriteFxn)(CAN_Handle handle, const void *buffer, size_t size)
A function pointer to a driver specific implementation of CAN_WriteFxn().
Definition: CAN.h:410
int_fast16_t CAN_control(CAN_Handle handle, uint_fast16_t cmd, void *arg)
Function performs implementation specific features on a given CAN_Handle.
void(* CAN_InitFxn)(CAN_Handle handle)
A function pointer to a driver specific implementation of CAN_InitFxn().
Definition: CAN.h:391
void CAN_init(void)
Function to initialize the CAN module.
struct CAN_Config_ * CAN_Handle
A handle that is returned from a CAN_open() call.
Definition: CAN.h:303
uint32_t writeTimeout
Definition: CAN.h:358
Definition: CAN.h:336
int_fast16_t(* CAN_ControlFxn)(CAN_Handle handle, uint_fast16_t cmd, void *arg)
A function pointer to a driver specific implementation of CAN_ControlFxn().
Definition: CAN.h:385
CAN_Direction direction
Definition: CAN.h:354
size_t txBufSize
Definition: CAN.h:478
struct CAN_Config_ CAN_Config
CAN Global configuration.
CAN_Direction_
CAN communication mode.
Definition: CAN.h:332
CAN_Handle CAN_open(uint_least8_t index, CAN_Params *params)
Function to initialize a given CAN peripheral.
Definition: CAN.h:323
void * object
Definition: CAN.h:463
enum CAN_Direction_ CAN_Direction
CAN communication mode.
CAN Global configuration.
Definition: CAN.h:458
struct CAN_FxnTable_ CAN_FxnTable
The definition of a CAN function table that contains the required set of functions to control a speci...
void(* CAN_TxMsgFxn)(CAN_Handle handle)
A function pointer to a driver specific implementation of CAN_TxMsgFxn().
Definition: CAN.h:417
void const * hwAttrs
Definition: CAN.h:466
CAN_ReadFxn readFxn
Definition: CAN.h:438
CAN_TxMsgFxn txMsgFxn
Definition: CAN.h:444
CAN Parameters.
Definition: CAN.h:352
CAN_Frame * txBufPtr
Definition: CAN.h:472
Definition: CAN.h:317
CAN_WriteFxn writeFxn
Definition: CAN.h:441
CAN frame structure.
Definition: source/ti/drivers/can/types.h:65
enum CAN_Mode_ CAN_Mode
CAN mode settings.
int_fast32_t CAN_read(CAN_Handle handle, void *buffer, size_t size)
Function that reads data from a CAN with interrupt enabled.
CAN_ControlFxn controlFxn
Definition: CAN.h:429
size_t rxBufSize
Definition: CAN.h:475
void CAN_Params_init(CAN_Params *params)
Function to initialize the CAN_Params struct to its defaults.
uint32_t readTimeout
Definition: CAN.h:357
CAN_Frame * rxBufPtr
Definition: CAN.h:469
CAN_InitFxn initFxn
Definition: CAN.h:432
struct CAN_Params_ CAN_Params
CAN Parameters.
Definition: CAN.h:341
uint32_t filterID
Definition: CAN.h:355
void CAN_close(CAN_Handle handle)
Function to close a CAN peripheral specified by the CAN handle.
The definition of a CAN function table that contains the required set of functions to control a speci...
Definition: CAN.h:424
CAN_CloseFxn closeFxn
Definition: CAN.h:426
CAN_OpenFxn openFxn
Definition: CAN.h:435
CAN_Handle(* CAN_OpenFxn)(CAN_Handle handle, CAN_Params *params)
A function pointer to a driver specific implementation of CAN_OpenFxn().
Definition: CAN.h:397
CAN_Mode mode
Definition: CAN.h:353
uint32_t filterMask
Definition: CAN.h:356
Definition: CAN.h:334
CAN_Mode_
CAN mode settings.
Definition: CAN.h:311
void(* CAN_CloseFxn)(CAN_Handle handle)
A function pointer to a driver specific implementation of CAN_CloseFxn().
Definition: CAN.h:379
CAN_FxnTable const * fxnTablePtr
Definition: CAN.h:460
Copyright 2018, Texas Instruments Incorporated