Network Services 2.40.00.11 Release Notes
Table of Contents
Introduction
The Network Services Component is a portable networking API that abstracts different network stacks found on TI devices. A BSD/POSIX socket API is provided as well.
Network Services also includes a SNTP client, HTTP 1.x client, MQTT client/server, and JSON parser/builder.
Documentation
The following documentation is provided with this release.
What’s New
2.40.00.11
Defects
The following Defects were resolved
ID | Summary |
---|---|
NS-172 | Introduce several SLNETSOCK TCP socket options |
NS-167 | HTTPClient reconnects fail for secure connections |
NS-166 | Add support for ENETDOWN in ErrnoUtil_set |
NS-159 | TCP_NODELAY should be defined in netinet/tcp.h |
NS-157 | SlNetSock_create() does not use the highest priority interface |
NS-155 | Memory leak in HTTPClient_connect's call to startSecureMode |
NS-129 | gethostbyname is not returning correct data structure |
NS-124 | Add support for SLNETSOCK_OPSOCK_BROADCAST socket option |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
NS-107 | Add A8F (gcc), A9F (gcc), A15F (gcc), A53F (gcc) and R5F (ccs) libraries |
Upgrade and Compatibility Information
- To address NS-129,
gethostbyname()
now correctly complies with the POSIX spec. Users should not expect the previous, errant implementation. - To address NS-159,
TCP_NODELAY
is now correctly declared innetinet/tcp.h
. Previously it was errantly declared insys/socket.h
. Users of this definition should update their code to use the new, now-POSIX-compliant header.h
Host Support
- Windows
- Linux
- Mac
Device Support
This release supports the following devices/platforms:
- MSP432E4
- CC3220
Validation Information
Network Services product was validated for the following platforms.
- SimpleLink MSP432E4 LaunchPad
- SimpleLink WiFi CC3220SF LaunchPad
Known Issues
- The Network Services Component is still fairly new, and there remains an expectation that issues will be found requiring minor API evolutions in the next few releases before stabilizing. We don’t expect significant changes, but it is likely there may be a few compatibility breaks. Please report issues on the TI E2E forums.
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 2.10.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Technical Support
Last updated: 2018-08-14