USBLib API Guide  1.00.00.01
Functions | Variables
usbtick.c File Reference
#include <stdbool.h>
#include <stdint.h>
#include "ti/devices/msp432e4/driverlib/driverlib.h"
#include "usblib.h"
#include "usblibpriv.h"
Include dependency graph for usbtick.c:

Functions

void InternalUSBTickInit (void)
 
void InternalUSBTickReset (void)
 
int32_t InternalUSBRegisterTickHandler (tUSBTickHandler pfHandler, void *pvInstance)
 
void InternalUSBStartOfFrameTick (uint32_t ui32TicksmS)
 

Variables

tUSBTickHandler g_pfnTickHandlers [MAX_USB_TICK_HANDLERS]
 
void * g_pvTickInstance [MAX_USB_TICK_HANDLERS]
 
bool g_bUSBTimerInitialized = false
 
uint32_t g_ui32CurrentUSBTick = 0
 
uint32_t g_ui32USBSOFCount = 0
 
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale