USBLib API Guide  1.00.00.01
Data Structures | Macros | Functions
usbddfu-rt.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  tDFUInstance
 
struct  tUSBDDFUDevice
 

Macros

#define DFUINTERFACE_SIZE   (9)
 
#define DFUFUNCTIONALDESC_SIZE   (9)
 
#define COMPOSITE_DDFU_SIZE   (DFUINTERFACE_SIZE + DFUFUNCTIONALDESC_SIZE)
 
#define USBD_DFU_EVENT_DETACH   (USBD_DFU_EVENT_BASE + 0)
 

Functions

void * USBDDFUCompositeInit (uint32_t ui32Index, tUSBDDFUDevice *psDFUDevice, tCompositeEntry *psCompEntry)
 
void USBDDFUCompositeTerm (void *pvDFUInstance)
 
void USBDDFUUpdateBegin (void)
 
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale