![]() |
![]() |
#include <ti/devices/msp432e4/inc/msp432e411y.h>
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_nvic.h"
#include "debug.h"
#include "interrupt.h"
#include "mpu.h"
Functions | |
void | MPUEnable (uint32_t ui32MPUConfig) |
void | MPUDisable (void) |
uint32_t | MPURegionCountGet (void) |
void | MPURegionEnable (uint32_t ui32Region) |
void | MPURegionDisable (uint32_t ui32Region) |
void | MPURegionSet (uint32_t ui32Region, uint32_t ui32Addr, uint32_t ui32Flags) |
void | MPURegionGet (uint32_t ui32Region, uint32_t *pui32Addr, uint32_t *pui32Flags) |
void | MPUIntRegister (void(*pfnHandler)(void)) |
void | MPUIntUnregister (void) |