![]() |
![]() |
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_nvic.h"
#include "cpu.h"
#include "debug.h"
#include "interrupt.h"
Macros | |
#define | NUM_INTERRUPTS 155 |
Functions | |
bool | IntMasterDisable (void) |
void | IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void)) |
void | IntUnregister (uint32_t ui32Interrupt) |
void | IntPriorityGroupingSet (uint32_t ui32Bits) |
uint32_t | IntPriorityGroupingGet (void) |
void | IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority) |
int32_t | IntPriorityGet (uint32_t ui32Interrupt) |
void | IntEnable (uint32_t ui32Interrupt) |
void | IntDisable (uint32_t ui32Interrupt) |
uint32_t | IntIsEnabled (uint32_t ui32Interrupt) |
void | IntPendSet (uint32_t ui32Interrupt) |
void | IntPendClear (uint32_t ui32Interrupt) |
void | IntPriorityMaskSet (uint32_t ui32PriorityMask) |
uint32_t | IntPriorityMaskGet (void) |
void | IntTrigger (uint32_t ui32Interrupt) |