![]() |
![]() |

Go to the source code of this file.
Macros | |
| #define | USBH_EVENT_HID_SETRPT USBH_HID_EVENT_BASE + 0 |
| #define | USBH_EVENT_HID_REPORT USBH_HID_EVENT_BASE + 1 |
| #define | USBH_EVENT_HID_KB_PRESS USBH_HID_EVENT_BASE + 16 |
| The HID keyboard detected a key being pressed. More... | |
| #define | USBH_EVENT_HID_KB_REL USBH_HID_EVENT_BASE + 17 |
| The HID keyboard detected a key being released. More... | |
| #define | USBH_EVENT_HID_KB_MOD USBH_HID_EVENT_BASE + 18 |
| The HID keyboard detected one of the keyboard modifiers being pressed. More... | |
| #define | USBH_EVENT_HID_MS_PRESS USBH_HID_EVENT_BASE + 32 |
| A button was pressed on a HID mouse. More... | |
| #define | USBH_EVENT_HID_MS_REL USBH_HID_EVENT_BASE + 33 |
| A button was released on a HID mouse. More... | |
| #define | USBH_EVENT_HID_MS_X USBH_HID_EVENT_BASE + 34 |
| The HID mouse detected movement in the X direction. More... | |
| #define | USBH_EVENT_HID_MS_Y USBH_HID_EVENT_BASE + 35 |
| The HID mouse detected movement in the Y direction. More... | |
Typedefs | |
| typedef struct tHIDInstance | tHIDInstance |
Enumerations | |
| enum | tHIDSubClassProtocol { eUSBHHIDClassNone = 0, eUSBHHIDClassKeyboard, eUSBHHIDClassMouse, eUSBHHIDClassVendor } |
Functions | |
| tHIDInstance * | USBHHIDOpen (tHIDSubClassProtocol iDeviceType, tUSBCallback pfnCallback, void *pvCBData) |
| void | USBHHIDClose (tHIDInstance *psHIDInstance) |
| uint32_t | USBHHIDGetReportDescriptor (tHIDInstance *psHIDInstance, uint8_t *pui8Buffer, uint32_t ui32Size) |
| uint32_t | USBHHIDSetIdle (tHIDInstance *psHIDInstance, uint8_t ui8Duration, uint8_t ui8ReportID) |
| uint32_t | USBHHIDSetProtocol (tHIDInstance *psHIDInstance, uint32_t ui32BootProtocol) |
| uint32_t | USBHHIDSetReport (tHIDInstance *psHIDInstance, uint32_t ui32Interface, uint8_t *pui8Data, uint32_t ui32Size) |
| uint32_t | USBHHIDGetReport (tHIDInstance *psHIDInstance, uint32_t ui32Interface, uint8_t *pui8Data, uint32_t ui32Size) |
| uint32_t | USBHHIDLPMSleep (tHIDInstance *psHIDInstance) |
| uint32_t | USBHHIDLPMStatus (tHIDInstance *psHIDInstance) |
Variables | |
| const tUSBHostClassDriver | g_sUSBHIDClassDriver |