|
| void | USBDCDDeviceInfoInit (uint32_t ui32Index, tDeviceInfo *psDeviceInfo) |
| |
| void | USBDCDInit (uint32_t ui32Index, tDeviceInfo *psDevice, void *pvDCDCBData) |
| |
| void | USBDCDTerm (uint32_t ui32Index) |
| |
| void | USBDCDRequestDataEP0 (uint32_t ui32Index, uint8_t *pui8Data, uint32_t ui32Size) |
| |
| void | USBDCDSendDataEP0 (uint32_t ui32Index, uint8_t *pui8Data, uint32_t ui32Size) |
| |
| void | USBDCDSetDefaultConfiguration (uint32_t ui32Index, uint32_t ui32DefaultConfig) |
| |
| void | USBDCDStallEP0 (uint32_t ui32Index) |
| |
| void | USBDCDPowerStatusSet (uint32_t ui32Index, uint8_t ui8Power) |
| |
| bool | USBDCDFeatureSet (uint32_t ui32Index, uint32_t ui32Feature, void *pvFeature) |
| |
| bool | USBDCDFeatureGet (uint32_t ui32Index, uint32_t ui32Feature, void *pvFeature) |
| |
| bool | USBDCDRemoteWakeLPM (uint32_t ui32Index) |
| |
| bool | USBDCDRemoteWakeupRequest (uint32_t ui32Index) |
| |
| void | USBDeviceResumeTickHandler (tDCDInstance *psDevInst) |
| |
| void | USBDeviceEnumHandler (tDCDInstance *pDevInstance) |
| |
| void | USBDeviceEnumResetHandler (tDCDInstance *pDevInstance) |
| |
| void | USBDeviceIntHandlerInternal (uint32_t ui32Index, uint32_t ui32Status) |
| |