Go to the source code of this file.
|
| void * | USBDCDCCompositeInit (uint32_t ui32Index, tUSBDCDCDevice *psCDCDevice, tCompositeEntry *psCompEntry) |
| |
| void * | USBDCDCInit (uint32_t ui32Index, tUSBDCDCDevice *psCDCDevice) |
| |
| void | USBDCDCTerm (void *pvCDCDevice) |
| |
| void * | USBDCDCSetControlCBData (void *pvCDCDevice, void *pvCBData) |
| |
| void * | USBDCDCSetRxCBData (void *pvCDCDevice, void *pvCBData) |
| |
| void * | USBDCDCSetTxCBData (void *pvCDCDevice, void *pvCBData) |
| |
| uint32_t | USBDCDCPacketWrite (void *pvCDCDevice, uint8_t *pi8Data, uint32_t ui32Length, bool bLast) |
| |
| uint32_t | USBDCDCPacketRead (void *pvCDCDevice, uint8_t *pi8Data, uint32_t ui32Length, bool bLast) |
| |
| uint32_t | USBDCDCTxPacketAvailable (void *pvCDCDevice) |
| |
| uint32_t | USBDCDCRxPacketAvailable (void *pvCDCDevice) |
| |
| void | USBDCDCSerialStateChange (void *pvCDCDevice, uint16_t ui16State) |
| |
| bool | USBDCDCRemoteWakeupRequest (void *pvCDCDevice) |
| |
| void | USBDCDCPowerStatusSet (void *pvCDCDevice, uint8_t ui8Power) |
| |