![]() |
![]() |
|
Network Services API
2.10.01.02
|
SlNetSock provides a standard BSD API for TCP and UDP transport layers, and a lower-level SlNetSock API for basic and extended usage. Supported use cases include:
The SlNetSock API's lead to easier portability to microcontrollers, without compromising the capabilities and robustness of the final application.
TI's SlNetSock layer is divided into the following software modules:
In addition, SlNetSock provides a standard BSD API, built atop the SlNet* APIs. The BSD headers are placed in ti/net/bsd directory, which users should place on their include path.
Also, there is a light SL Interface Porting Guide with information available for adding SlNetSock support for other stacks.