|
| int32_t | FlashErase (uint32_t ui32Address) |
| |
| int32_t | FlashProgram (uint32_t *pui32Data, uint32_t ui32Address, uint32_t ui32Count) |
| |
| tFlashProtection | FlashProtectGet (uint32_t ui32Address) |
| |
| int32_t | FlashProtectSet (uint32_t ui32Address, tFlashProtection eProtect) |
| |
| int32_t | FlashProtectSave (void) |
| |
| int32_t | FlashUserGet (uint32_t *pui32User0, uint32_t *pui32User1) |
| |
| int32_t | FlashUserSet (uint32_t ui32User0, uint32_t ui32User1) |
| |
| int32_t | FlashAllUserRegisterGet (uint32_t *pui32User0, uint32_t *pui32User1, uint32_t *pui32User2, uint32_t *pui32User3) |
| |
| int32_t | FlashAllUserRegisterSet (uint32_t ui32User0, uint32_t ui32User1, uint32_t ui32User2, uint32_t ui32User3) |
| |
| int32_t | FlashUserSave (void) |
| |
| int32_t | FlashAllUserRegisterSave (void) |
| |
| void | FlashIntRegister (void(*pfnHandler)(void)) |
| |
| void | FlashIntUnregister (void) |
| |
| void | FlashIntEnable (uint32_t ui32IntFlags) |
| |
| void | FlashIntDisable (uint32_t ui32IntFlags) |
| |
| uint32_t | FlashIntStatus (bool bMasked) |
| |
| void | FlashIntClear (uint32_t ui32IntFlags) |
| |