|
| uint32_t | EEPROMInit (void) |
| |
| uint32_t | EEPROMSizeGet (void) |
| |
| uint32_t | EEPROMBlockCountGet (void) |
| |
| void | EEPROMRead (uint32_t *pui32Data, uint32_t ui32Address, uint32_t ui32Count) |
| |
| uint32_t | EEPROMProgram (uint32_t *pui32Data, uint32_t ui32Address, uint32_t ui32Count) |
| |
| uint32_t | EEPROMProgramNonBlocking (uint32_t ui32Data, uint32_t ui32Address) |
| |
| uint32_t | EEPROMMassErase (void) |
| |
| uint32_t | EEPROMBlockProtectGet (uint32_t ui32Block) |
| |
| uint32_t | EEPROMBlockProtectSet (uint32_t ui32Block, uint32_t ui32Protect) |
| |
| uint32_t | EEPROMBlockPasswordSet (uint32_t ui32Block, uint32_t *pui32Password, uint32_t ui32Count) |
| |
| uint32_t | EEPROMBlockLock (uint32_t ui32Block) |
| |
| uint32_t | EEPROMBlockUnlock (uint32_t ui32Block, uint32_t *pui32Password, uint32_t ui32Count) |
| |
| void | EEPROMBlockHide (uint32_t ui32Block) |
| |
| void | EEPROMIntEnable (uint32_t ui32IntFlags) |
| |
| void | EEPROMIntDisable (uint32_t ui32IntFlags) |
| |
| uint32_t | EEPROMIntStatus (bool bMasked) |
| |
| void | EEPROMIntClear (uint32_t ui32IntFlags) |
| |
| uint32_t | EEPROMStatusGet (void) |
| |