|
| void | ComparatorConfigure (uint32_t ui32Base, uint32_t ui32Comp, uint32_t ui32Config) |
| |
| void | ComparatorRefSet (uint32_t ui32Base, uint32_t ui32Ref) |
| |
| bool | ComparatorValueGet (uint32_t ui32Base, uint32_t ui32Comp) |
| |
| void | ComparatorIntRegister (uint32_t ui32Base, uint32_t ui32Comp, void(*pfnHandler)(void)) |
| |
| void | ComparatorIntUnregister (uint32_t ui32Base, uint32_t ui32Comp) |
| |
| void | ComparatorIntEnable (uint32_t ui32Base, uint32_t ui32Comp) |
| |
| void | ComparatorIntDisable (uint32_t ui32Base, uint32_t ui32Comp) |
| |
| bool | ComparatorIntStatus (uint32_t ui32Base, uint32_t ui32Comp, bool bMasked) |
| |
| void | ComparatorIntClear (uint32_t ui32Base, uint32_t ui32Comp) |
| |