|
| void | ADCIntRegister (uint32_t ui32Base, uint32_t ui32SequenceNum, void(*pfnHandler)(void)) |
| |
| void | ADCIntUnregister (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCIntDisable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCIntEnable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| uint32_t | ADCIntStatus (uint32_t ui32Base, uint32_t ui32SequenceNum, bool bMasked) |
| |
| void | ADCIntClear (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceEnable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceDisable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Trigger, uint32_t ui32Priority) |
| |
| void | ADCSequenceStepConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Step, uint32_t ui32Config) |
| |
| int32_t | ADCSequenceOverflow (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceOverflowClear (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| int32_t | ADCSequenceUnderflow (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceUnderflowClear (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| int32_t | ADCSequenceDataGet (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t *pui32Buffer) |
| |
| void | ADCProcessorTrigger (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSoftwareOversampleConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Factor) |
| |
| void | ADCSoftwareOversampleStepConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Step, uint32_t ui32Config) |
| |
| void | ADCSoftwareOversampleDataGet (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t *pui32Buffer, uint32_t ui32Count) |
| |
| void | ADCHardwareOversampleConfigure (uint32_t ui32Base, uint32_t ui32Factor) |
| |
| void | ADCComparatorConfigure (uint32_t ui32Base, uint32_t ui32Comp, uint32_t ui32Config) |
| |
| void | ADCComparatorRegionSet (uint32_t ui32Base, uint32_t ui32Comp, uint32_t ui32LowRef, uint32_t ui32HighRef) |
| |
| void | ADCComparatorReset (uint32_t ui32Base, uint32_t ui32Comp, bool bTrigger, bool bInterrupt) |
| |
| void | ADCComparatorIntDisable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCComparatorIntEnable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| uint32_t | ADCComparatorIntStatus (uint32_t ui32Base) |
| |
| void | ADCComparatorIntClear (uint32_t ui32Base, uint32_t ui32Status) |
| |
| void | ADCIntDisableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
| |
| void | ADCIntEnableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
| |
| uint32_t | ADCIntStatusEx (uint32_t ui32Base, bool bMasked) |
| |
| void | ADCIntClearEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
| |
| void | ADCReferenceSet (uint32_t ui32Base, uint32_t ui32Ref) |
| |
| uint32_t | ADCReferenceGet (uint32_t ui32Base) |
| |
| void | ADCPhaseDelaySet (uint32_t ui32Base, uint32_t ui32Phase) |
| |
| uint32_t | ADCPhaseDelayGet (uint32_t ui32Base) |
| |
| void | ADCSequenceDMAEnable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| void | ADCSequenceDMADisable (uint32_t ui32Base, uint32_t ui32SequenceNum) |
| |
| bool | ADCBusy (uint32_t ui32Base) |
| |
| void | ADCClockConfigSet (uint32_t ui32Base, uint32_t ui32Config, uint32_t ui32ClockDiv) |
| |
| uint32_t | ADCClockConfigGet (uint32_t ui32Base, uint32_t *pui32ClockDiv) |
| |