MSP432E4 USB Library Release Notes
Introduction
The Texas Instrument USB Library is a set of data types and functions for creating USB device, host or On-The-Go (OTG) applications.
This is 1.00.00.01 version of the MSP432E4 USB Library.
Documentation
What’s New
- Implemented USB Library for MSP432E4 Devices
- RTOS and No RTOS examples showcasing USB Library features
- User’s Guide describing how to use the library
- API Guide showing all APIs provided in the library
Upgrade and Compatibility Information
No code compatibility breaks, initial release of software library.
Host Support
- Windows 7, Windows 8, Windows 10
- Ubuntu 14.04 64-bit, Ubuntu 16.04 64-bit
- macOS Sierra
Dependencies
This release requires the following other software components and tools.
- CCS 7.3.0
- TI Code Generation Tools
- ARM version 16.9.4.LTS or later
- GNU Code Generation Tools
- ARM gcc-arm-none-eabi-6-2017-q1-update
- IAR Code Generation Tools
- ARM 8.11.3
- Keil uVision
- 5.23
- TexasInstruments.MSP432E4_DFP.3.2.0.pack
Device Support
- MSP432E401Y
- MSP432E411Y
Known Issues
No known issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.