All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
usbmsc.h
Go to the documentation of this file.
1 //*****************************************************************************
2 //
3 // usbmsc.h - Generic types and defines use by the mass storage class.
4 //
5 // Copyright (c) 2008-2017 Texas Instruments Incorporated. All rights reserved.
6 // Software License Agreement
7 //
8 // Texas Instruments (TI) is supplying this software for use solely and
9 // exclusively on TI's microcontroller products. The software is owned by
10 // TI and/or its suppliers, and is protected under applicable copyright
11 // laws. You may not combine this software with "viral" open-source
12 // software in order to form a larger program.
13 //
14 // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
15 // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
16 // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
17 // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
18 // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
19 // DAMAGES, FOR ANY REASON WHATSOEVER.
20 //
21 //*****************************************************************************
22 
23 #ifndef __USBMSC_H__
24 #define __USBMSC_H__
25 
26 //*****************************************************************************
27 //
28 // If building with a C++ compiler, make all of the definitions in this header
29 // have a C binding.
30 //
31 //*****************************************************************************
32 #ifdef __cplusplus
33 extern "C"
34 {
35 #endif
36 
37 //*****************************************************************************
38 //
39 // The request for the maximum number of logical units on a mass storage
40 // device.
41 //
42 //*****************************************************************************
43 #define USBREQ_GET_MAX_LUN 0xfe
44 
45 //*****************************************************************************
46 //
47 // The request for the bulk only reset of a mass storage device.
48 //
49 //*****************************************************************************
50 #define USBREQ_BULK_ONLY_RESET 0xff
51 
52 //*****************************************************************************
53 //
54 // The signatures defined by USB MSC class specification.
55 //
56 //*****************************************************************************
57 #define CBW_SIGNATURE 0x43425355
58 #define CSW_SIGNATURE 0x53425355
59 
60 //*****************************************************************************
61 //
62 // Flag for the bmCBWFlags member of tMSCCBW
63 //
64 //*****************************************************************************
65 #define CBWFLAGS_DIR_M 0x80
66 #define CBWFLAGS_DIR_IN 0x80
67 #define CBWFLAGS_DIR_OUT 0x00
68 
69 //*****************************************************************************
70 //
71 // All structures defined in this section of the header require byte packing of
72 // fields. This is usually accomplished using the PACKED macro but, for IAR
73 // Embedded Workbench, this requries a pragma.
74 //
75 //*****************************************************************************
76 #ifdef __ICCARM__
77 #pragma pack(1)
78 #endif
79 
80 //*****************************************************************************
81 //
82 // The following packed structure is used to access the Command Block Wrapper
83 // (CBW) data structure that is used when communicating with USB Mass Storage
84 // Class devices.
85 //
86 //*****************************************************************************
87 typedef struct
88 {
89  //
90  // Signature that helps identify this data packet as a CBW. The signature
91  // field shall contain the value 0x43425355 (little endian), indicating a
92  // CBW.
93  //
94  uint32_t dCBWSignature;
95 
96  //
97  // The Command Block Tag sent by the host controller. The device shall
98  // echo the contents of this field back to the host in the dCSWTag field
99  // of the associated CSW. The dCSWTag positively associates a CSW with the
100  // corresponding CBW.
101  //
102  uint32_t dCBWTag;
103 
104  //
105  // The number of bytes of data that the host expects to transfer on the
106  // Bulk-In or Bulk-Out endpoint (as indicated by the Direction bit) during
107  // the execution of this command. If this field is zero, the device and
108  // the host will not transfer data between the CBW and the associated CSW,
109  // and the device will ignore the value of the Direction bit in
110  // bmCBWFlags.
111  //
113 
114  //
115  // The device will ignore these bits if the dCBWDataTransferLength value
116  // is set to 0.
117  //
118  // The bits of this field are defined as follows:
119  // Bit 7 Direction
120  // 0 = Data-Out from host to the device,
121  // 1 = Data-In from the device to the host.
122  // Bit 6 Obsolete - The host shall set this bit to zero.
123  // Bits 5..0 Reserved - the host shall set these bits to zero.
124  //
125  uint8_t bmCBWFlags;
126 
127  //
128  // The device Logical Unit Number (LUN) to which the command block is being
129  // sent. For devices that support multiple LUNs, the host shall place into
130  // this field the LUN to which this command block is addressed. Otherwise,
131  // the host shall set this field to zero.
132  //
133  uint8_t bCBWLUN;
134 
135  //
136  // The valid length of the CBWCB in bytes. This defines the valid length
137  // of the command block. The only legal values are 1 through 16. All
138  // other values are reserved.
139  //
140  uint8_t bCBWCBLength;
141 
142  //
143  // This array holds the command block to be executed by the device. The
144  // MSC device will interpret the first bCBWCBLength bytes in this field as
145  // a command block as defined by the command set identified by
146  // bInterfaceSubClass. If the command set supported by the device uses
147  // command blocks of fewer than 16 bytes in length, the significant bytes
148  // shall be transferred first, beginning with the byte at offset 15. The
149  // device will ignore the content of the CBWCB field past the byte at
150  // offset (15 + bCBWCBLength - 1).
151  //
152  uint8_t CBWCB[16];
153 }
154 PACKED tMSCCBW;
155 
156 //*****************************************************************************
157 //
158 // Flags for the bCSWStatus member of tMSCCSW
159 //
160 //*****************************************************************************
161 #define CSWSTATUS_CMD_SUCCESS 0
162 #define CSWSTATUS_CMD_FAILED 1
163 #define CSWSTATUS_PHASE_ERROR 2
164 
165 //*****************************************************************************
166 //
167 // This structure encapsulates the Command Status Word (CSW) structure that is
168 // sent in response to all CBW commands.
169 //
170 //*****************************************************************************
171 typedef struct
172 {
173  //
174  // Signature that identifies this data packet as a CSW. The signature
175  // field must contain the value 53425355h (little endian) to indicate CSW.
176  //
177  uint32_t dCSWSignature;
178 
179  //
180  // The device will set this field to the value received in the dCBWTag of
181  // the associated CBW.
182  //
183  uint32_t dCSWTag;
184 
185  //
186  // For OUT transactions the device will fill the dCSWDataResidue field with
187  // the difference between the amount of data expected as stated in the
188  // dCBWDataTransferLength, and the actual amount of data processed by the
189  // device. For IN transactions the device will fill the dCSWDataResidue
190  // field with the difference between the amount of data expected as stated
191  // in the dCBWDataTransferLength and the actual amount of relevant data
192  // sent by the device. The dCSWDataResidue will not exceed the value sent
193  // in the dCBWDataTransferLength.
194  //
195  uint32_t dCSWDataResidue;
196 
197  //
198  // The bCSWStatus field indicates the success or failure of the command.
199  // The device shall set this byte to zero if the command completed
200  // successfully. A non-zero value shall indicate a failure during command
201  // execution.
202  //
203  uint8_t bCSWStatus;
204 }
205 PACKED tMSCCSW;
206 
207 //*****************************************************************************
208 //
209 // Return to default packing when using the IAR Embedded Workbench compiler.
210 //
211 //*****************************************************************************
212 #ifdef __ICCARM__
213 #pragma pack()
214 #endif
215 
216 //*****************************************************************************
217 //
218 // SCSI Command return codes.
219 //
220 //*****************************************************************************
221 #define SCSI_CMD_STATUS_PASS 0x00
222 #define SCSI_CMD_STATUS_FAIL 0x01
223 
224 //*****************************************************************************
225 //
226 // SCSI commands.
227 //
228 //*****************************************************************************
229 #define SCSI_TEST_UNIT_READY 0x00
230 #define SCSI_REQUEST_SENSE 0x03
231 #define SCSI_INQUIRY_CMD 0x12
232 #define SCSI_MODE_SENSE_6 0x1a
233 #define SCSI_START_STOP_UNIT 0x1b
234 #define SCSI_MEDIUM_REMOVAL 0x1e
235 #define SCSI_READ_CAPACITIES 0x23
236 #define SCSI_READ_CAPACITY 0x25
237 #define SCSI_READ_10 0x28
238 #define SCSI_WRITE_10 0x2a
239 
240 //*****************************************************************************
241 //
242 // SCSI Test Unit Ready definitions.
243 //
244 //*****************************************************************************
245 
246 //*****************************************************************************
247 //
248 // SCSI Inquiry command definitions.
249 //
250 //*****************************************************************************
251 
252 //*****************************************************************************
253 //
254 // Size of the SCSI inquiry response data.
255 //
256 //*****************************************************************************
257 #define SCSI_INQUIRY_DATA_SZ 36
258 
259 //*****************************************************************************
260 //
261 // Offset 0 of the Inquiry Data.
262 //
263 //*****************************************************************************
264 #define SCSI_INQ_PQ_M 0xe0 // Peripheral Qualifier Mask.
265 #define SCSI_INQ_PQ_CNCT 0x00 // Device connected.
266 #define SCSI_INQ_PQ_DISC 0x20 // Device disconnected.
267 #define SCSI_INQ_PDT_M 0x1f // Peripheral Device Type Mask.
268 #define SCSI_INQ_PDT_SBC 0x00 // Direct Access device.
269 
270 //*****************************************************************************
271 //
272 // Offset 1 of the Inquiry Data.
273 //
274 //*****************************************************************************
275 #define SCSI_INQ_RMB 0x80 // Device is removable.
276 
277 //*****************************************************************************
278 //
279 // Macro to check if removeable.
280 //
281 //*****************************************************************************
282 #define SCSIIsRemovable(pData) \
283  (((uint8_t *)pData)[1] & SCSI_INQ_RMB)
284 
285 //*****************************************************************************
286 //
287 // SCSI Read Capacity definitions.
288 //
289 //*****************************************************************************
290 
291 //*****************************************************************************
292 //
293 // Size of the SCSI Read Capacity response data.
294 //
295 //*****************************************************************************
296 #define SCSI_READ_CAPACITY_SZ 0x08
297 
298 //*****************************************************************************
299 //
300 // SCSI Mode Sense definitions, these are passed in via the ui32Flags parameter
301 // of the SCSIModeSense() function call.
302 //
303 //*****************************************************************************
304 
305 //*****************************************************************************
306 //
307 // Disable block descriptors.
308 //
309 //*****************************************************************************
310 #define SCSI_MS_DBD 0x00000800
311 
312 //*****************************************************************************
313 //
314 // Page Code values, used in combination with Page Control values.
315 //
316 //*****************************************************************************
317 #define SCSI_MS_PC_VENDOR 0x00000000
318 #define SCSI_MS_PC_DISCO 0x00020000
319 #define SCSI_MS_PC_CONTROL 0x000a0000
320 #define SCSI_MS_PC_LUN 0x00180000
321 #define SCSI_MS_PC_PORT 0x00190000
322 #define SCSI_MS_PC_POWER 0x001a0000
323 #define SCSI_MS_PC_INFORM 0x001c0000
324 #define SCSI_MS_PC_ALL 0x003f0000
325 
326 //*****************************************************************************
327 //
328 // Page Control values.
329 //
330 //*****************************************************************************
331 #define SCSI_MS_PC_CURRENT 0x00000000
332 #define SCSI_MS_PC_CHANGEABLE 0x00400000
333 #define SCSI_MS_PC_DEFAULT 0x00800000
334 #define SCSI_MS_PC_SAVED 0x00c00000
335 
336 //*****************************************************************************
337 //
338 // Request Sense Definitions.
339 //
340 //*****************************************************************************
341 
342 //*****************************************************************************
343 //
344 // Size of the data returned by the Request Sense command.
345 //
346 //*****************************************************************************
347 #define SCSI_REQUEST_SENSE_SZ 18
348 
349 #define SCSI_RS_SKEY 2 // Sense Key offset.
350 #define SCSI_RS_SKEY_AD_SKEY 12 // Additional Sense Key offset.
351 
352 //*****************************************************************************
353 //
354 // Offset 0 in the Request Sense response.
355 //
356 //*****************************************************************************
357 #define SCSI_RS_VALID 0x80 // Response is valid.
358 #define SCSI_RS_CUR_ERRORS 0x70 // Current errors returned.
359 #define SCSI_RS_DEFER_ERRORS 0x71 // Deferred errors returned.
360 
361 //*****************************************************************************
362 //
363 // Offset 2 in the Request Sense response.
364 //
365 //*****************************************************************************
366 #define SCSI_RS_KEY_M 0x0f // Sense Key.
367 #define SCSI_RS_KEY_NO_SENSE 0x00 // No Sense Data.
368 #define SCSI_RS_KEY_RECOVRD_ERR 0x01 // Recovered Error.
369 #define SCSI_RS_KEY_NOT_READY 0x02 // Not Ready.
370 #define SCSI_RS_KEY_MEDIUM_ERR 0x03 // Error in the media.
371 #define SCSI_RS_KEY_HW_ERR 0x04 // Hardware Error, non recoverable.
372 #define SCSI_RS_KEY_ILGL_RQST 0x05 // Illegal request.
373 #define SCSI_RS_KEY_UNIT_ATTN 0x06 // Unit changed or reset.
374 #define SCSI_RS_KEY_DATA_PROT 0x07 // Write Protect error.
375 #define SCSI_RS_KEY_BLANK_CHK 0x08 // Write once error, block not clear.
376 #define SCSI_RS_KEY_ABORT 0x0b // Last command was aborted.
377 #define SCSI_RS_ILI 0x20 // Incorrect length indicator.
378 #define SCSI_RS_EOM 0x40 // End of medium condition.
379 #define SCSI_RS_FILEMARK 0x80 // Command has read a filemark/setmark.
380 #define SCSI_RS_MED_NOT_PRSNT 0x003a // Medium not present.
381 #define SCSI_RS_MED_NOTRDY2RDY 0x0028 // Not ready to ready transition.
382 #define SCSI_RS_PV_INVALID 0x0226 // Parameter Value Invalid.
383 
384 //*****************************************************************************
385 //
386 // Additional information for SCSI_RS_KEY_NOT_READY
387 //
388 //*****************************************************************************
389 #define SCSI_RS_KEY_NOTPRSNT 0x3A // Media Not Present.
390 
391 //*****************************************************************************
392 //
393 // Prevent/Allow Medium Removal Definitions.
394 //
395 //*****************************************************************************
396 
397 //*****************************************************************************
398 //
399 // Offset 4 in the Prevent/Allow Medium Removal command.
400 //
401 //*****************************************************************************
402 #define SCSI_PE_MEDRMV_M 0x03
403 #define SCSI_PE_MEDRMV_ALLOW 0x00
404 #define SCSI_PE_MEDRMV_PREVENT 0x01
405 
406 //*****************************************************************************
407 //
408 // Start/Stop Unit Definitions.
409 //
410 //*****************************************************************************
411 
412 //*****************************************************************************
413 //
414 // Offset 1 in the Start/Stop Unit command.
415 //
416 //*****************************************************************************
417 #define SCSI_SS_UNIT_IMMED 0x01
418 #define SCSI_SS_UNIT_LUN_M 0xe0
419 
420 //*****************************************************************************
421 //
422 // Offset 4 in the Start/Stop Unit command.
423 //
424 //*****************************************************************************
425 #define SCSI_SS_UNIT_START 0x01
426 #define SCSI_SS_UNIT_LOEJ 0x02
427 #define SCSI_SS_UNIT_PWR_M 0xf0
428 #define SCSI_SS_UNIT_PWR_ACTIVE 0x10
429 #define SCSI_SS_UNIT_PWR_IDLE 0x20
430 #define SCSI_SS_UNIT_PWR_STDBY 0x30
431 #define SCSI_SS_UNIT_PWR_DSLEEP 0x50
432 
433 //*****************************************************************************
434 //
435 // Mark the end of the C bindings section for C++ compilers.
436 //
437 //*****************************************************************************
438 #ifdef __cplusplus
439 }
440 #endif
441 
442 #endif // __USBMSC_H__
uint8_t bmCBWFlags
Definition: usbmsc.h:125
uint8_t bCSWStatus
Definition: usbmsc.h:203
uint32_t dCSWDataResidue
Definition: usbmsc.h:195
uint8_t bCBWCBLength
Definition: usbmsc.h:140
uint32_t dCBWTag
Definition: usbmsc.h:102
uint8_t bCBWLUN
Definition: usbmsc.h:133
uint32_t dCBWSignature
Definition: usbmsc.h:94
uint32_t dCBWDataTransferLength
Definition: usbmsc.h:112
uint32_t dCSWSignature
Definition: usbmsc.h:177
uint32_t dCSWTag
Definition: usbmsc.h:183
USB_CDC_GET/SET_LINE_CODING request-specific data.
Definition: usbaudio.h:288
Copyright 2017, Texas Instruments Incorporated