415 #ifndef ti_drivers_SPI__include 416 #define ti_drivers_SPI__include 443 #define SPI_CMD_RESERVED (32) 457 #define SPI_STATUS_RESERVED (-32) 472 #define SPI_STATUS_SUCCESS (0) 480 #define SPI_STATUS_ERROR (-1) 489 #define SPI_STATUS_UNDEFINEDCMD (-2) 509 #define SPI_WAIT_FOREVER (~(0U)) 718 extern void SPI_close(SPI_Handle handle);
757 extern int_fast16_t
SPI_control(SPI_Handle handle, uint_fast16_t cmd,
void SPI_init(void)
This function initializes the SPI module.
SPI_Mode mode
Definition: SPI.h:616
enum SPI_Status_ SPI_Status
Status codes that are set by the SPI driver.
void * rxBuf
Definition: SPI.h:539
SPI_FrameFormat_
Definitions for various SPI data frame formats.
Definition: SPI.h:568
SPI_CloseFxn closeFxn
Definition: SPI.h:669
void const * hwAttrs
Definition: SPI.h:706
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:553
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation.
SPI_InitFxn initFxn
Definition: SPI.h:675
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:535
SPI_ControlFxn controlFxn
Definition: SPI.h:672
SPI_TransferFxn transferFxn
Definition: SPI.h:681
uint32_t bitRate
Definition: SPI.h:617
uint32_t dataSize
Definition: SPI.h:618
void SPI_transferCancel(SPI_Handle handle)
Function to cancel SPI transactions.
SPI_FxnTable const * fxnTablePtr
Definition: SPI.h:700
void SPI_Params_init(SPI_Params *params)
Function to initialize the SPI_Params struct to its defaults.
bool(* SPI_TransferFxn)(SPI_Handle handle, SPI_Transaction *transaction)
A function pointer to a driver specific implementation of SPI_transfer().
Definition: SPI.h:653
size_t count
Definition: SPI.h:537
struct SPI_Transaction_ SPI_Transaction
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
SPI_TransferCancelFxn transferCancelFxn
Definition: SPI.h:684
void(* SPI_TransferCancelFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_transferCancel().
Definition: SPI.h:660
SPI_Status_
Status codes that are set by the SPI driver.
Definition: SPI.h:519
uint32_t transferTimeout
Definition: SPI.h:613
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
void(* SPI_CloseFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_close().
Definition: SPI.h:628
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:667
SPI Parameters.
Definition: SPI.h:611
SPI_Status status
Definition: SPI.h:543
int_fast16_t SPI_control(SPI_Handle handle, uint_fast16_t cmd, void *controlArg)
Function performs implementation specific features on a given SPI_Handle.
struct SPI_Params_ SPI_Params
SPI Parameters.
void * txBuf
Definition: SPI.h:538
bool SPI_transfer(SPI_Handle handle, SPI_Transaction *transaction)
Function to perform SPI transactions.
struct SPI_Config_ SPI_Config
SPI Global configuration.
SPI Global configuration.
Definition: SPI.h:698
SPI_OpenFxn openFxn
Definition: SPI.h:678
SPI_Mode_
Definitions for various SPI modes of operation.
Definition: SPI.h:559
void * custom
Definition: SPI.h:620
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
void SPI_close(SPI_Handle handle)
Function to close a SPI peripheral specified by the SPI handle.
SPI_TransferMode transferMode
Definition: SPI.h:612
struct SPI_Config_ * SPI_Handle
A handle that is returned from a SPI_open() call.
Definition: SPI.h:514
SPI_Handle SPI_open(uint_least8_t index, SPI_Params *params)
This function opens a given SPI peripheral.
void * arg
Definition: SPI.h:540
int_fast16_t(* SPI_ControlFxn)(SPI_Handle handle, uint_fast16_t cmd, void *arg)
A function pointer to a driver specific implementation of SPI_control().
Definition: SPI.h:634
void(* SPI_InitFxn)(SPI_Handle handle)
A function pointer to a driver specific implementation of SPI_init().
Definition: SPI.h:641
SPI_Handle(* SPI_OpenFxn)(SPI_Handle handle, SPI_Params *params)
A function pointer to a driver specific implementation of SPI_open().
Definition: SPI.h:647
SPI_FrameFormat frameFormat
Definition: SPI.h:619
struct SPI_FxnTable_ SPI_FxnTable
The definition of a SPI function table that contains the required set of functions to control a speci...
SPI_CallbackFxn transferCallbackFxn
Definition: SPI.h:615
SPI_TransferMode_
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:589
void * object
Definition: SPI.h:703