50 #ifndef ti_drivers_cryptoutils_ecc_ECCParams__include 51 #define ti_drivers_cryptoutils_ecc_ECCParams__include const uint8_t * b
Coefficient b of the equation.
Definition: ECCParams.h:75
A structure containing the parameters of an elliptic curve in short Weierstrass form.
Definition: ECCParams.h:70
const size_t length
Length of the curve in bytes. All other buffers have this length.
Definition: ECCParams.h:71
const ECCParams_CurveParams ECCParams_NISTP256
The NISTP256 curve in short Weierstrass form.
const uint8_t * generatorX
X coordinate of the generator point of the curve.
Definition: ECCParams.h:76
const uint8_t * generatorY
Y coordinate of the generator point of the curve.
Definition: ECCParams.h:77
const uint8_t * prime
The prime that defines the field of the curve.
Definition: ECCParams.h:72
const uint8_t * order
Order of the curve.
Definition: ECCParams.h:73
struct ECCParams_CurveParams_ ECCParams_CurveParams
A structure containing the parameters of an elliptic curve in short Weierstrass form.
const uint8_t * a
Coefficient a of the equation.
Definition: ECCParams.h:74