Network Services API  2.00.00.16
Data Structures | Macros | Typedefs | Enumerations | Functions
slnetsock.h File Reference
#include <stdint.h>
#include "slnetif.h"
#include "slnetutils.h"
#include "slneterr.h"
Include dependency graph for slnetsock.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  _SlNetSock_InAddr_t
 Internet address. More...
 
struct  _SlNetSock_In6Addr_t
 IpV6 or Ipv6 EUI64. More...
 
struct  _SlNetSock_Keepalive_t
 The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...
 
struct  _SlNetSock_NonIpBoundary_t
 The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...
 
struct  _SlNetSock_Winsize_t
 The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option. More...
 
struct  _SlNetSock_Nonblocking_t
 The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...
 
struct  _SlNetSock_SecAttribNode_t
 Secure socket attribute context. More...
 
struct  _SlNetSock_SecureALPN_t
 Secure ALPN structure. More...
 
struct  _SlNetSock_SecureMask_t
 Secure Mask structure. More...
 
struct  _SlNetSock_SecureMethod_t
 Secure Method structure. More...
 
struct  _SlNetSock_IpMreq_t
 The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP/SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option. More...
 
struct  _SlNetSock_IpV6Mreq_t
 The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP/SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...
 
struct  _SlNetSock_linger_t
 The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option. More...
 
struct  _SlNetSock_Timeval_t
 The SlNetSock_Timeval_t structure is used in SLNETSOCK_OPSOCK_RCV_TIMEO socket level option. More...
 
struct  _SlNetSock_Addr_t
 IpV4 socket address. More...
 
struct  _SlNetSock_AddrIn6_t
 SlNetSock IPv6 address, Internet style. More...
 
struct  _SlNetSock_AddrIn_t
 SlNetSock IPv4 address, Internet style. More...
 
struct  _SlNetSock_SdSet_t
 The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...
 
struct  _SlNetSock_TransceiverRxOverHead_t
 The SlNetSock_TransceiverRxOverHead_t structure holds the data for Rx transceiver mode using a raw socket when using SlNetSock_recv function. More...
 

Macros

#define SLNETSOCK_MAX_CONCURRENT_SOCKETS   (32) /* Declares the maximum sockets that can be opened */
 
#define SLNETSOCK_AF_INET   (2) /* IPv4 socket (UDP, TCP, etc) */
 
#define SLNETSOCK_AF_INET6   (3) /* IPv6 socket (UDP, TCP, etc) */
 
#define SLNETSOCK_AF_RF   (6) /* data include RF parameter, All layer by user (Wifi could be disconnected) */
 
#define SLNETSOCK_AF_PACKET   (17) /* Network bypass */
 
#define SLNETSOCK_PF_INET   SLNETSOCK_AF_INET
 
#define SLNETSOCK_PF_INET6   SLNETSOCK_AF_INET6
 
#define SLNETSOCK_SOCK_STREAM   (1) /* TCP Socket */
 
#define SLNETSOCK_SOCK_DGRAM   (2) /* UDP Socket */
 
#define SLNETSOCK_SOCK_RAW   (3) /* Raw socket */
 
#define SLNETSOCK_SOCK_RX_MTR   (4) /* RX Metrics socket */
 
#define SLNETSOCK_SOCK_MAC_WITH_CCA   (5)
 
#define SLNETSOCK_SOCK_MAC_WITH_NO_CCA   (6)
 
#define SLNETSOCK_SOCK_BRIDGE   (7)
 
#define SLNETSOCK_SOCK_ROUTER   (8)
 
#define SLNETSOCK_PROTO_TCP   (6) /* TCP Raw Socket */
 
#define SLNETSOCK_PROTO_UDP   (17) /* UDP Raw Socket */
 
#define SLNETSOCK_PROTO_RAW   (255) /* Raw Socket */
 
#define SLNETSOCK_PROTO_SECURE   (100) /* Secured Socket Layer (SSL,TLS) */
 
#define SLNETSOCK_INADDR_ANY   (0)
 
#define SLNETSOCK_IN6ADDR_ANY   (0)
 
#define SLNETSOCK_LVL_SOCKET   (1) /* Define the socket option category. */
 
#define SLNETSOCK_LVL_IP   (2) /* Define the IP option category. */
 
#define SLNETSOCK_LVL_PHY   (3) /* Define the PHY option category. */
 
#define SLNETSOCK_OPSOCK_RCV_BUF   (8) /* Setting TCP receive buffer size (window size) - This options takes SlNetSock_Winsize_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_RCV_TIMEO   (20) /* Enable receive timeout - This options takes SlNetSock_Timeval_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_KEEPALIVE   (9) /* Connections are kept alive with periodic messages - This options takes SlNetSock_Keepalive_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_KEEPALIVE_TIME   (36) /* keepalive time out - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPSOCK_LINGER   (13) /* Socket lingers on close pending remaining send/receive packets - This options takes SlNetSock_linger_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_NON_BLOCKING   (24) /* Enable/disable nonblocking mode - This options takes SlNetSock_Nonblocking_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_NON_IP_BOUNDARY   (38) /* connectionless socket disable rx boundary - This options takes SlNetSock_NonIpBoundary_t struct as parameter */
 
#define SLNETSOCK_OPSOCK_SLNETSOCKSD   (59) /* Used by the BSD layer in order to retrieve the slnetsock sd */
 
#define SLNETSOCK_OPIP_MULTICAST_TTL   (61) /* Specify the TTL value to use for outgoing multicast packet. - This options takes <b>uint8_t</b> as parameter */
 
#define SLNETSOCK_OPIP_ADD_MEMBERSHIP   (65) /* Join IPv4 multicast membership - This options takes SlNetSock_IpMreq_t struct as parameter */
 
#define SLNETSOCK_OPIP_DROP_MEMBERSHIP   (66) /* Leave IPv4 multicast membership - This options takes SlNetSock_IpMreq_t struct as parameter */
 
#define SLNETSOCK_OPIP_HDRINCL   (67) /* Raw socket IPv4 header included - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPIP_RAW_RX_NO_HEADER   (68) /* Proprietary socket option that does not includeIPv4/IPv6 header (and extension headers) on received raw sockets - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPIP_RAW_IPV6_HDRINCL   (69) /* Transmitted buffer over IPv6 socket contains IPv6 header - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPIPV6_ADD_MEMBERSHIP   (70) /* Join IPv6 multicast membership - This options takes SlNetSock_IpV6Mreq_t struct as parameter */
 
#define SLNETSOCK_OPIPV6_DROP_MEMBERSHIP   (71) /* Leave IPv6 multicast membership - This options takes SlNetSock_IpV6Mreq_t struct as parameter */
 
#define SLNETSOCK_OPIPV6_MULTICAST_HOPS   (72) /* Specify the hops value to use for outgoing multicast packet. */
 
#define SLNETSOCK_OPPHY_CHANNEL   (107) /* This option is available only when transceiver started - This options takes <b>uint32_t</b> as channel number parameter */
 
#define SLNETSOCK_OPPHY_RATE   (100) /* WLAN Transmit rate - This options takes <b>uint32_t</b> as parameter based on SlWlanRateIndex_e */
 
#define SLNETSOCK_OPPHY_TX_POWER   (101) /* TX Power level - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPPHY_NUM_FRAMES_TO_TX   (102) /* Number of frames to transmit - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPPHY_PREAMBLE   (103) /* Preamble for transmission - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPPHY_TX_INHIBIT_THRESHOLD   (104) /* TX Inhibit Threshold (CCA) - This options takes <b>uint32_t</b> as parameter based on SlNetSockTxInhibitThreshold_e */
 
#define SLNETSOCK_OPPHY_TX_TIMEOUT   (105) /* TX timeout for Transceiver frames (lifetime) in miliseconds (max value is 100ms) - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_OPPHY_ALLOW_ACKS   (106) /* Enable sending ACKs in transceiver mode - This options takes <b>uint32_t</b> as parameter */
 
#define SLNETSOCK_SEC_METHOD_SSLV3   (0) /* security metohd SSL v3 */
 
#define SLNETSOCK_SEC_METHOD_TLSV1   (1) /* security metohd TLS v1 */
 
#define SLNETSOCK_SEC_METHOD_TLSV1_1   (2) /* security metohd TLS v1_1 */
 
#define SLNETSOCK_SEC_METHOD_TLSV1_2   (3) /* security metohd TLS v1_2 */
 
#define SLNETSOCK_SEC_METHOD_SSLv3_TLSV1_2   (4) /* use highest possible version from SSLv3 - TLS 1.2 */
 
#define SLNETSOCK_SEC_METHOD_DLSV1   (5) /* security metohd DTL v1 */
 
#define SLNETSOCK_SEC_CIPHER_SSL_RSA_WITH_RC4_128_SHA   (1 << 0)
 
#define SLNETSOCK_SEC_CIPHER_SSL_RSA_WITH_RC4_128_MD5   (1 << 1)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_CBC_SHA   (1 << 2)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_256_CBC_SHA   (1 << 3)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_256_CBC_SHA   (1 << 4)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_RC4_128_SHA   (1 << 5)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_128_CBC_SHA256   (1 << 6)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_CBC_SHA256   (1 << 7)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA256   (1 << 8)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256   (1 << 9)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA   (1 << 10)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_256_CBC_SHA   (1 << 11)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_128_GCM_SHA256   (1 << 12)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_GCM_SHA384   (1 << 13)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_128_GCM_SHA256   (1 << 14)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_256_GCM_SHA384   (1 << 15)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_128_GCM_SHA256   (1 << 16)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_256_GCM_SHA384   (1 << 17)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256   (1 << 18)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_256_GCM_SHA384   (1 << 19)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 20)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 21)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 22)
 
#define SLNETSOCK_SEC_ALPN_H1   (1 << 0)
 
#define SLNETSOCK_SEC_ALPN_H2   (1 << 1)
 
#define SLNETSOCK_SEC_ALPN_H2C   (1 << 2)
 
#define SLNETSOCK_SEC_ALPN_H2_14   (1 << 3)
 
#define SLNETSOCK_SEC_ALPN_H2_16   (1 << 4)
 
#define SLNETSOCK_SEC_ALPN_FULL_LIST   ((SLNETSOCK_SEC_ALPN_H2_16 << 1 ) - 1)
 
#define SLNETSOCK_SEC_START_SECURITY_SESSION_ONLY   (1 << 0) /* Sends the command that will start the security session for a specific socket descriptor */
 
#define SLNETSOCK_SEC_BIND_CONTEXT_ONLY   (1 << 1) /* Binds the security context to a specific socket descriptor */
 
#define SLNETSOCK_SEC_IS_SERVER   (1 << 2) /* Used to define if the socket is client/server socket */
 
#define SLNETSOCK_CREATE_IF_STATE_ENABLE   (1 << 0) /* Creation of the socket will be on enabled state */
 
#define SLNETSOCK_CREATE_IF_STATUS_CONNECTED   (1 << 1) /* Creation of the socket will be on status connected */
 
#define SLNETSOCK_CREATE_ALLOW_PARTIAL_MATCH
 
#define SLNETSOCK_SHUT_RD   (0) /* Further receptions will be disallowed */
 
#define SLNETSOCK_SHUT_WR   (1) /* Further transmissions will be disallowed */
 
#define SLNETSOCK_SHUT_RDWR   (2) /* Further receptions and transmissions will be disallowed */
 
#define SLNETSOCK_INET6_ADDRSTRLEN   (40)
 
#define SLNETSOCK_INET_ADDRSTRLEN   (15)
 
#define SLNETSOCK_RECV_MSG_DONTWAIT   (1 << 0)
 

Typedefs

typedef struct _SlNetSock_InAddr_t SlNetSock_InAddr_t
 Internet address. More...
 
typedef struct _SlNetSock_In6Addr_t SlNetSock_In6Addr_t
 IpV6 or Ipv6 EUI64. More...
 
typedef struct _SlNetSock_Keepalive_t SlNetSock_Keepalive_t
 The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...
 
typedef struct _SlNetSock_NonIpBoundary_t SlNetSock_NonIpBoundary_t
 The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...
 
typedef struct _SlNetSock_Winsize_t SlNetSock_Winsize_t
 The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option. More...
 
typedef struct _SlNetSock_Nonblocking_t SlNetSock_Nonblocking_t
 The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...
 
typedef struct _SlNetSock_SecAttribNode_t SlNetSock_SecAttribNode_t
 Secure socket attribute context. More...
 
typedef SlNetSock_SecAttribNode_t * SlNetSockSecAttrib_t
 Secure socket attribute handler. More...
 
typedef struct _SlNetSock_SecureALPN_t SlNetSock_SecureALPN_t
 Secure ALPN structure. More...
 
typedef struct _SlNetSock_SecureMask_t SlNetSock_SecureMask_t
 Secure Mask structure. More...
 
typedef struct _SlNetSock_SecureMethod_t SlNetSock_SecureMethod_t
 Secure Method structure. More...
 
typedef struct _SlNetSock_IpMreq_t SlNetSock_IpMreq_t
 The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP/SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option. More...
 
typedef struct _SlNetSock_IpV6Mreq_t SlNetSock_IpV6Mreq_t
 The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP/SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...
 
typedef struct _SlNetSock_linger_t SlNetSock_linger_t
 The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option. More...
 
typedef int32_t SlNetSockTime_t
 The SlNetSockTime_t is used for setting/getting time in seconds. More...
 
typedef int32_t SlNetSockuseconds_t
 The SlNetSockuseconds_t is used for setting/getting time in micro-seconds. More...
 
typedef struct _SlNetSock_Timeval_t SlNetSock_Timeval_t
 The SlNetSock_Timeval_t structure is used in SLNETSOCK_OPSOCK_RCV_TIMEO socket level option. More...
 
typedef uint16_t SlNetSocklen_t
 The SlNetSocklen_t is used for declaring the socket length parameter. More...
 
typedef struct _SlNetSock_Addr_t SlNetSock_Addr_t
 IpV4 socket address. More...
 
typedef struct _SlNetSock_AddrIn6_t SlNetSock_AddrIn6_t
 SlNetSock IPv6 address, Internet style. More...
 
typedef struct _SlNetSock_AddrIn_t SlNetSock_AddrIn_t
 SlNetSock IPv4 address, Internet style. More...
 
typedef struct _SlNetSock_SdSet_t SlNetSock_SdSet_t
 The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...
 
typedef struct _SlNetSock_TransceiverRxOverHead_t SlNetSock_TransceiverRxOverHead_t
 The SlNetSock_TransceiverRxOverHead_t structure holds the data for Rx transceiver mode using a raw socket when using SlNetSock_recv function. More...
 

Enumerations

enum  SlNetSockTxInhibitThreshold_e {
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MIN = 1,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_LOW = 2,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_DEFAULT = 3,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MED = 4,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_HIGH = 5,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MAX = 6
}
 The SlNetSockTxInhibitThreshold_e enumerations is used in SLNETSOCK_OPPHY_TX_INHIBIT_THRESHOLD PHY level option. More...
 
enum  SlNetSockSecAttrib_e {
  SLNETSOCK_SEC_ATTRIB_PRIVATE_KEY = 0,
  SLNETSOCK_SEC_ATTRIB_LOCAL_CERT = 1,
  SLNETSOCK_SEC_ATTRIB_PEER_ROOT_CA = 2,
  SLNETSOCK_SEC_ATTRIB_DH_KEY = 3,
  SLNETSOCK_SEC_ATTRIB_METHOD = 4,
  SLNETSOCK_SEC_ATTRIB_CIPHERS = 5,
  SLNETSOCK_SEC_ATTRIB_ALPN = 6,
  SLNETSOCK_SEC_ATTRIB_EXT_CLIENT_CHLNG_RESP = 7,
  SLNETSOCK_SEC_ATTRIB_DOMAIN_NAME = 8
}
 The SlNetSockSecAttrib_e enumerations is used for security attribute object in SlNetSock_secAttribSet function. More...
 

Functions

int32_t SlNetSock_init (int32_t flags)
 Initialize the slnetsock module. More...
 
int16_t SlNetSock_create (int16_t domain, int16_t type, int16_t protocol, uint32_t ifBitmap, int16_t flags)
 Create an endpoint for communication. More...
 
int32_t SlNetSock_close (int16_t sd)
 Gracefully close socket. More...
 
int32_t SlNetSock_shutdown (int16_t sd, int16_t how)
 Shutting down parts of a full-duplex connection. More...
 
int16_t SlNetSock_accept (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Accept a connection on a socket. More...
 
int32_t SlNetSock_bind (int16_t sd, const SlNetSock_Addr_t *addr, int16_t addrlen)
 Assign a name to a socket. More...
 
int32_t SlNetSock_listen (int16_t sd, int16_t backlog)
 Listen for connections on a socket. More...
 
int32_t SlNetSock_connect (int16_t sd, const SlNetSock_Addr_t *addr, SlNetSocklen_t addrlen)
 Initiate a connection on a socket. More...
 
int32_t SlNetSock_connectUrl (int16_t sd, const char *url)
 Initiate a connection on a socket by URL. More...
 
int32_t SlNetSock_getPeerName (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Return address info about the remote side of the connection. More...
 
int32_t SlNetSock_getSockName (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Get local address info by socket descriptor
Returns the local address info of the socket descriptor. More...
 
int32_t SlNetSock_select (int16_t nsds, SlNetSock_SdSet_t *readsds, SlNetSock_SdSet_t *writesds, SlNetSock_SdSet_t *exceptsds, SlNetSock_Timeval_t *timeout)
 Monitor socket activity. More...
 
int32_t SlNetSock_sdsSet (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t SET function. More...
 
int32_t SlNetSock_sdsClr (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t CLR function. More...
 
int32_t SlNetSock_sdsClrAll (SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t ZERO function. More...
 
int32_t SlNetSock_sdsIsSet (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t ISSET function. More...
 
int32_t SlNetSock_setOpt (int16_t sd, int16_t level, int16_t optname, void *optval, SlNetSocklen_t optlen)
 Set socket options-. More...
 
int32_t SlNetSock_getOpt (int16_t sd, int16_t level, int16_t optname, void *optval, SlNetSocklen_t *optlen)
 Get socket options. More...
 
int32_t SlNetSock_recv (int16_t sd, void *buf, uint32_t len, uint32_t flags)
 Read data from TCP socket. More...
 
int32_t SlNetSock_recvFrom (int16_t sd, void *buf, uint32_t len, uint32_t flags, SlNetSock_Addr_t *from, SlNetSocklen_t *fromlen)
 Read data from socket. More...
 
int32_t SlNetSock_send (int16_t sd, const void *buf, uint32_t len, uint32_t flags)
 Write data to TCP socket. More...
 
int32_t SlNetSock_sendTo (int16_t sd, const void *buf, uint32_t len, uint32_t flags, const SlNetSock_Addr_t *to, SlNetSocklen_t tolen)
 Write data to socket. More...
 
int32_t SlNetSock_getIfID (uint16_t sd)
 Get interface ID from socket descriptor (sd) More...
 
SlNetSockSecAttrib_t * SlNetSock_secAttribCreate (void)
 Creates a security attributes object. More...
 
int32_t SlNetSock_secAttribDelete (SlNetSockSecAttrib_t *secAttrib)
 Deletes a security attributes object. More...
 
int32_t SlNetSock_secAttribSet (SlNetSockSecAttrib_t *secAttrib, SlNetSockSecAttrib_e attribName, void *val, uint16_t len)
 set a security attributes More...
 
int32_t SlNetSock_startSec (int16_t sd, SlNetSockSecAttrib_t *secAttrib, uint8_t flags)
 Start a security session on an opened socket. More...
 
Copyright 2017, Texas Instruments Incorporated