All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Functions
sysctl.c File Reference
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_nvic.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_flash.h"
#include "cpu.h"
#include "debug.h"
#include "interrupt.h"
#include "sysctl.h"

Macros

#define FLASH_PP_MAINSS_S   16
 
#define SysCtlXtalCfgToIndex(a)   ((a & 0x7c0) >> 6)
 
#define MAX_VCO_ENTRIES   2
 
#define MAX_XTAL_ENTRIES   18
 
#define PLL_M_TO_REG(mi, mf)   ((uint32_t)mi | (uint32_t)(mf << SYSCTL_PLLFREQ0_MFRAC_S))
 
#define PLL_N_TO_REG(n)   ((uint32_t)(n - 1) << SYSCTL_PLLFREQ1_N_S)
 
#define PLL_Q_TO_REG(q)   ((uint32_t)(q - 1) << SYSCTL_PLLFREQ1_Q_S)
 
#define SYSCTL_PPBASE   0x400fe300
 
#define SYSCTL_SRBASE   0x400fe500
 
#define SYSCTL_RCGCBASE   0x400fe600
 
#define SYSCTL_SCGCBASE   0x400fe700
 
#define SYSCTL_DCGCBASE   0x400fe800
 
#define SYSCTL_PCBASE   0x400fe900
 
#define SYSCTL_PRBASE   0x400fea00
 

Functions

uint32_t SysCtlSRAMSizeGet (void)
 
uint32_t SysCtlFlashSizeGet (void)
 
uint32_t SysCtlFlashSectorSizeGet (void)
 
bool SysCtlPeripheralPresent (uint32_t ui32Peripheral)
 
bool SysCtlPeripheralReady (uint32_t ui32Peripheral)
 
void SysCtlPeripheralPowerOn (uint32_t ui32Peripheral)
 
void SysCtlPeripheralPowerOff (uint32_t ui32Peripheral)
 
void SysCtlPeripheralReset (uint32_t ui32Peripheral)
 
void SysCtlPeripheralEnable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralDisable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralSleepEnable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralSleepDisable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralDeepSleepEnable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralDeepSleepDisable (uint32_t ui32Peripheral)
 
void SysCtlPeripheralClockGating (bool bEnable)
 
void SysCtlIntRegister (void(*pfnHandler)(void))
 
void SysCtlIntUnregister (void)
 
void SysCtlIntEnable (uint32_t ui32Ints)
 
void SysCtlIntDisable (uint32_t ui32Ints)
 
void SysCtlIntClear (uint32_t ui32Ints)
 
uint32_t SysCtlIntStatus (bool bMasked)
 
void SysCtlLDODeepSleepSet (uint32_t ui32Voltage)
 
uint32_t SysCtlLDODeepSleepGet (void)
 
void SysCtlSleepPowerSet (uint32_t ui32Config)
 
void SysCtlDeepSleepPowerSet (uint32_t ui32Config)
 
void SysCtlReset (void)
 
void SysCtlSleep (void)
 
void SysCtlDeepSleep (void)
 
uint32_t SysCtlResetCauseGet (void)
 
void SysCtlResetCauseClear (uint32_t ui32Causes)
 
void SysCtlMOSCConfigSet (uint32_t ui32Config)
 
uint32_t SysCtlPIOSCCalibrate (uint32_t ui32Type)
 
void SysCtlResetBehaviorSet (uint32_t ui32Behavior)
 
uint32_t SysCtlResetBehaviorGet (void)
 
uint32_t SysCtlClockFreqSet (uint32_t ui32Config, uint32_t ui32SysClock)
 
void SysCtlDeepSleepClockConfigSet (uint32_t ui32Div, uint32_t ui32Config)
 
void SysCtlVoltageEventConfig (uint32_t ui32Config)
 
uint32_t SysCtlVoltageEventStatus (void)
 
void SysCtlVoltageEventClear (uint32_t ui32Status)
 
bool SysCtlVCOGet (uint32_t ui32Crystal, uint32_t *pui32VCOFrequency)
 
uint32_t SysCtlNMIStatus (void)
 
void SysCtlNMIClear (uint32_t ui32Ints)
 
void SysCtlClockOutConfig (uint32_t ui32Config, uint32_t ui32Div)
 
void SysCtlAltClkConfig (uint32_t ui32Config)
 

Variable Documentation

§ ui32Frequency

uint32_t ui32Frequency

§ ui32MemTiming

uint32_t ui32MemTiming
Copyright 2017, Texas Instruments Incorporated