All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Functions
interrupt.c File Reference
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_nvic.h"
#include "cpu.h"
#include "debug.h"
#include "interrupt.h"

Macros

#define NUM_INTERRUPTS   155
 

Functions

bool IntMasterDisable (void)
 
void IntRegister (uint32_t ui32Interrupt, void(*pfnHandler)(void))
 
void IntUnregister (uint32_t ui32Interrupt)
 
void IntPriorityGroupingSet (uint32_t ui32Bits)
 
uint32_t IntPriorityGroupingGet (void)
 
void IntPrioritySet (uint32_t ui32Interrupt, uint8_t ui8Priority)
 
int32_t IntPriorityGet (uint32_t ui32Interrupt)
 
void IntEnable (uint32_t ui32Interrupt)
 
void IntDisable (uint32_t ui32Interrupt)
 
uint32_t IntIsEnabled (uint32_t ui32Interrupt)
 
void IntPendSet (uint32_t ui32Interrupt)
 
void IntPendClear (uint32_t ui32Interrupt)
 
void IntPriorityMaskSet (uint32_t ui32PriorityMask)
 
uint32_t IntPriorityMaskGet (void)
 
void IntTrigger (uint32_t ui32Interrupt)
 
Copyright 2017, Texas Instruments Incorporated