All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
crc.h
Go to the documentation of this file.
1 //*****************************************************************************
2 //
3 // crc.h - Defines and Macros for CRC module.
4 //
5 // Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
6 // Software License Agreement
7 //
8 // Redistribution and use in source and binary forms, with or without
9 // modification, are permitted provided that the following conditions
10 // are met:
11 //
12 // Redistributions of source code must retain the above copyright
13 // notice, this list of conditions and the following disclaimer.
14 //
15 // Redistributions in binary form must reproduce the above copyright
16 // notice, this list of conditions and the following disclaimer in the
17 // documentation and/or other materials provided with the
18 // distribution.
19 //
20 // Neither the name of Texas Instruments Incorporated nor the names of
21 // its contributors may be used to endorse or promote products derived
22 // from this software without specific prior written permission.
23 //
24 // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
25 // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
26 // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
27 // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
28 // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
29 // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
30 // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
31 // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
32 // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
33 // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
34 // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
35 //
36 //*****************************************************************************
37 
38 #ifndef __DRIVERLIB_CRC_H__
39 #define __DRIVERLIB_CRC_H__
40 
41 #include <stdint.h>
42 #include <stdbool.h>
43 
44 //*****************************************************************************
45 //
46 // If building with a C++ compiler, make all of the definitions in this header
47 // have a C binding.
48 //
49 //*****************************************************************************
50 #ifdef __cplusplus
51 extern "C"
52 {
53 #endif
54 
55 //*****************************************************************************
56 //
57 // The following defines are used in the ui32Config argument of the
58 // ECConfig function.
59 //
60 //*****************************************************************************
61 #define CRC_CFG_INIT_SEED 0x00000000 // Initialize with seed
62 #define CRC_CFG_INIT_0 0x00004000 // Initialize to all '0s'
63 #define CRC_CFG_INIT_1 0x00006000 // Initialize to all '1s'
64 #define CRC_CFG_SIZE_8BIT 0x00001000 // Input Data Size
65 #define CRC_CFG_SIZE_32BIT 0x00000000 // Input Data Size
66 #define CRC_CFG_RESINV 0x00000200 // Result Inverse Enable
67 #define CRC_CFG_OBR 0x00000100 // Output Reverse Enable
68 #define CRC_CFG_IBR 0x00000080 // Bit reverse enable
69 #define CRC_CFG_ENDIAN_SBHW 0x00000020 // Swap byte in half-word
70 #define CRC_CFG_ENDIAN_SHW 0x00000010 // Swap half-word
71 #define CRC_CFG_TYPE_P8005 0x00000000 // Polynomial 0x8005
72 #define CRC_CFG_TYPE_P1021 0x00000001 // Polynomial 0x1021
73 #define CRC_CFG_TYPE_P4C11DB7 0x00000002 // Polynomial 0x4C11DB7
74 #define CRC_CFG_TYPE_P1EDC6F41 0x00000003 // Polynomial 0x1EDC6F41
75 #define CRC_CFG_TYPE_TCPCHKSUM 0x00000008 // TCP checksum
76 
77 //*****************************************************************************
78 //
79 // Function prototypes.
80 //
81 //*****************************************************************************
82 extern void CRCConfigSet(uint32_t ui32Base, uint32_t ui32CRCConfig);
83 extern uint32_t CRCDataProcess(uint32_t ui32Base, uint32_t *pui32DataIn,
84  uint32_t ui32DataLength, bool bPPResult);
85 extern void CRCDataWrite(uint32_t ui32Base, uint32_t ui32Data);
86 extern uint32_t CRCResultRead(uint32_t ui32Base, bool bPPResult);
87 extern void CRCSeedSet(uint32_t ui32Base, uint32_t ui32Seed);
88 
89 //*****************************************************************************
90 //
91 // Mark the end of the C bindings section for C++ compilers.
92 //
93 //*****************************************************************************
94 #ifdef __cplusplus
95 }
96 #endif
97 
98 #endif // __DRIVERLIB_CRC_H__
void CRCConfigSet(uint32_t ui32Base, uint32_t ui32CRCConfig)
Definition: crc.c:95
uint32_t CRCDataProcess(uint32_t ui32Base, uint32_t *pui32DataIn, uint32_t ui32DataLength, bool bPPResult)
Definition: crc.c:251
uint32_t CRCResultRead(uint32_t ui32Base, bool bPPResult)
Definition: crc.c:203
void CRCDataWrite(uint32_t ui32Base, uint32_t ui32Data)
Definition: crc.c:173
void CRCSeedSet(uint32_t ui32Base, uint32_t ui32Seed)
Definition: crc.c:140
Copyright 2017, Texas Instruments Incorporated