All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Functions
adc.c File Reference
#include <ti/devices/msp432e4/inc/msp432e411y.h>
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_adc.h"
#include "inc/hw_sysctl.h"
#include "adc.h"
#include "debug.h"
#include "interrupt.h"

Macros

#define ADC_SEQ   (ADC_O_SSMUX0)
 
#define ADC_SEQ_STEP   (ADC_O_SSMUX1 - ADC_O_SSMUX0)
 
#define ADC_SSMUX   (ADC_O_SSMUX0 - ADC_O_SSMUX0)
 
#define ADC_SSEMUX   (ADC_O_SSEMUX0 - ADC_O_SSMUX0)
 
#define ADC_SSCTL   (ADC_O_SSCTL0 - ADC_O_SSMUX0)
 
#define ADC_SSFIFO   (ADC_O_SSFIFO0 - ADC_O_SSMUX0)
 
#define ADC_SSFSTAT   (ADC_O_SSFSTAT0 - ADC_O_SSMUX0)
 
#define ADC_SSOP   (ADC_O_SSOP0 - ADC_O_SSMUX0)
 
#define ADC_SSDC   (ADC_O_SSDC0 - ADC_O_SSMUX0)
 
#define ADC_SSTSH   (ADC_O_SSTSH0 - ADC_O_SSMUX0)
 

Functions

void ADCIntRegister (uint32_t ui32Base, uint32_t ui32SequenceNum, void(*pfnHandler)(void))
 
void ADCIntUnregister (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCIntDisable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCIntEnable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
uint32_t ADCIntStatus (uint32_t ui32Base, uint32_t ui32SequenceNum, bool bMasked)
 
void ADCIntClear (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceEnable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceDisable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Trigger, uint32_t ui32Priority)
 
void ADCSequenceStepConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Step, uint32_t ui32Config)
 
int32_t ADCSequenceOverflow (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceOverflowClear (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
int32_t ADCSequenceUnderflow (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceUnderflowClear (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
int32_t ADCSequenceDataGet (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t *pui32Buffer)
 
void ADCProcessorTrigger (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSoftwareOversampleConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Factor)
 
void ADCSoftwareOversampleStepConfigure (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t ui32Step, uint32_t ui32Config)
 
void ADCSoftwareOversampleDataGet (uint32_t ui32Base, uint32_t ui32SequenceNum, uint32_t *pui32Buffer, uint32_t ui32Count)
 
void ADCHardwareOversampleConfigure (uint32_t ui32Base, uint32_t ui32Factor)
 
void ADCComparatorConfigure (uint32_t ui32Base, uint32_t ui32Comp, uint32_t ui32Config)
 
void ADCComparatorRegionSet (uint32_t ui32Base, uint32_t ui32Comp, uint32_t ui32LowRef, uint32_t ui32HighRef)
 
void ADCComparatorReset (uint32_t ui32Base, uint32_t ui32Comp, bool bTrigger, bool bInterrupt)
 
void ADCComparatorIntDisable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCComparatorIntEnable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
uint32_t ADCComparatorIntStatus (uint32_t ui32Base)
 
void ADCComparatorIntClear (uint32_t ui32Base, uint32_t ui32Status)
 
void ADCIntDisableEx (uint32_t ui32Base, uint32_t ui32IntFlags)
 
void ADCIntEnableEx (uint32_t ui32Base, uint32_t ui32IntFlags)
 
uint32_t ADCIntStatusEx (uint32_t ui32Base, bool bMasked)
 
void ADCIntClearEx (uint32_t ui32Base, uint32_t ui32IntFlags)
 
void ADCReferenceSet (uint32_t ui32Base, uint32_t ui32Ref)
 
uint32_t ADCReferenceGet (uint32_t ui32Base)
 
void ADCPhaseDelaySet (uint32_t ui32Base, uint32_t ui32Phase)
 
uint32_t ADCPhaseDelayGet (uint32_t ui32Base)
 
void ADCSequenceDMAEnable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
void ADCSequenceDMADisable (uint32_t ui32Base, uint32_t ui32SequenceNum)
 
bool ADCBusy (uint32_t ui32Base)
 
void ADCClockConfigSet (uint32_t ui32Base, uint32_t ui32Config, uint32_t ui32ClockDiv)
 
uint32_t ADCClockConfigGet (uint32_t ui32Base, uint32_t *pui32ClockDiv)
 
Copyright 2017, Texas Instruments Incorporated