--------------------------------------------------------------------------- 1 (Local) ./src/ti/sysbios/family/arm/lm4/Seconds.c:173 SV.TAINTED.LOOP_BOUND (2:Error) Analyze Unvalidated integer value 'seconds_1' is received from '0x1074774016' at line 170 and can be used in a loop condition at line 173. * Seconds.c:170: Tainted data 'seconds_1' resides at the arbitrary constant memory location * Seconds.c:173: Tainted data 'seconds_1' is used as a loop boundary Current status 'Analyze' --------------------------------------------------------------------------- 2 (Local) ./src/ti/sysbios/family/arm/lm4/Seconds.c:173 SV.TAINTED.LOOP_BOUND (2:Error) Analyze Unvalidated integer value 'seconds_2' is received from '0x1074774016' at line 172 and can be used in a loop condition at line 173. * Seconds.c:172: Tainted data 'seconds_2' resides at the arbitrary constant memory location * Seconds.c:173: Tainted data 'seconds_2' is used as a loop boundary Current status 'Analyze' Summary: 2 Local 2 Total Issue(s)