UDMAMSP432.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
53 #ifndef ti_drivers_dma_UDMAMSP432__include
54 #define ti_drivers_dma_UDMAMSP432__include
55 
56 #include <stdint.h>
57 #include <stdbool.h>
58 
59 #include <ti/drivers/dpl/HwiP.h>
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
68 typedef void (*UDMAMSP432_ErrorFxn)(uintptr_t arg);
69 
111 typedef struct {
114  uint8_t intNum;
115  uint8_t intPriority;
117 
127 typedef struct {
128  void *object;
129  void const *hwAttrs;
131 
136 
142 typedef struct {
143  bool unused;
145 
154 typedef struct {
155  uint32_t dmaChannel;
156  uint32_t structSelect;
157  uint32_t ctlOptions;
158  uint32_t transferMode;
161  uint32_t transferSize;
163 
173 typedef struct {
174  uint32_t dmaChannel;
175  uint32_t ctlOptions;
176  uint32_t transferMode;
180  uint32_t transferSize;
182 
199 extern void UDMAMSP432_close(UDMAMSP432_Handle handle, uint32_t channelNum, uint8_t intNum);
210 extern void UDMAMSP432_init();
211 
230 extern UDMAMSP432_Handle UDMAMSP432_open(uint32_t channelNum, uint8_t intNum, uint32_t priority,
231  void (*hwiFxn)(uintptr_t), uintptr_t arg);
232 
245 extern bool UDMAMSP432_setupTransfer(UDMAMSP432_Transfer *transfer);
246 
263 
276 
277 #ifdef __cplusplus
278 }
279 #endif
280 
281 #endif /* ti_drivers_dma_UDMAMSP432__include */
uint32_t structSelect
Definition: UDMAMSP432.h:156
UDMAMSP432_Config * UDMAMSP432_Handle
A handle that is returned from a UDMAMSP432_open() call.
Definition: UDMAMSP432.h:135
UDMAMSP432 Transfer configuration.
Definition: UDMAMSP432.h:154
bool unused
Definition: UDMAMSP432.h:143
uint32_t dmaChannel
Definition: UDMAMSP432.h:174
void * dmaAlternateDestination
Definition: UDMAMSP432.h:179
uint32_t transferMode
Definition: UDMAMSP432.h:158
uint32_t ctlOptions
Definition: UDMAMSP432.h:175
uint8_t intNum
Definition: UDMAMSP432.h:114
void * dmaTransferDestination
Definition: UDMAMSP432.h:160
void * dmaPrimaryDestination
Definition: UDMAMSP432.h:178
void UDMAMSP432_close(UDMAMSP432_Handle handle, uint32_t channelNum, uint8_t intNum)
Function to close the DMA driver.
UDMAMSP432 Ping Pong Transfer configuration.
Definition: UDMAMSP432.h:173
void * object
Definition: UDMAMSP432.h:128
uint32_t transferSize
Definition: UDMAMSP432.h:161
bool UDMAMSP432_setupTransfer(UDMAMSP432_Transfer *transfer)
Function to set up a DMA channel for data transfer.
UDMAMSP432_Handle UDMAMSP432_open(uint32_t channelNum, uint8_t intNum, uint32_t priority, void(*hwiFxn)(uintptr_t), uintptr_t arg)
Function to initialize the MSP432 DMA peripheral and corresponding interrupt.
bool UDMAMSP432_setupPingPongTransfer(UDMAMSP432_PingPongTransfer *transfer)
Function to set up a DMA channel for ping pong data transfer.
void const * hwAttrs
Definition: UDMAMSP432.h:129
uint32_t transferSize
Definition: UDMAMSP432.h:180
uint32_t dmaChannel
Definition: UDMAMSP432.h:155
uint8_t intPriority
Definition: UDMAMSP432.h:115
UDMAMSP432 Global configuration.
Definition: UDMAMSP432.h:127
void * controlBaseAddr
Definition: UDMAMSP432.h:112
UDMAMSP432_ErrorFxn dmaErrorFxn
Definition: UDMAMSP432.h:113
void * dmaTransferSource
Definition: UDMAMSP432.h:177
void(* UDMAMSP432_ErrorFxn)(uintptr_t arg)
UDMA error function pointer.
Definition: UDMAMSP432.h:68
uint32_t transferMode
Definition: UDMAMSP432.h:176
UDMAMSP432 object.
Definition: UDMAMSP432.h:142
UDMAMSP432 Hardware attributes.
Definition: UDMAMSP432.h:111
void * dmaTransferSource
Definition: UDMAMSP432.h:159
void UDMAMSP432_init()
Function to initialize the MSP432 DMA driver.
uint32_t ctlOptions
Definition: UDMAMSP432.h:157
void UDMAMSP432_PingPongToggleBuffer(UDMAMSP432_PingPongTransfer *transfer)
Function to toggle between two buffers during ping pong mode.
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale