![]() |
![]() |
#include <stdint.h>#include <ti/devices/msp432p4xx/inc/msp.h>#include <stdbool.h>Go to the source code of this file.
Macros | |
| #define | PSS_KEY_VALUE PSS_KEY_KEY_VAL |
| #define | PSS_SVSMH PSS_IE_SVSMHIE |
| #define | PSS_FULL_PERFORMANCE_MODE 0x01 |
| #define | PSS_NORMAL_PERFORMANCE_MODE 0x00 |
Functions | |
| void | PSS_enableHighSidePinToggle (bool activeLow) |
| void | PSS_disableHighSidePinToggle (void) |
| void | PSS_enableHighSide (void) |
| void | PSS_disableHighSide (void) |
| void | PSS_setHighSidePerformanceMode (uint_fast8_t powerMode) |
| uint_fast8_t | PSS_getHighSidePerformanceMode (void) |
| void | PSS_enableHighSideMonitor (void) |
| void | PSS_disableHighSideMonitor (void) |
| void | PSS_setHighSideVoltageTrigger (uint_fast8_t triggerVoltage) |
| uint_fast8_t | PSS_getHighSideVoltageTrigger (void) |
| void | PSS_enableInterrupt (void) |
| void | PSS_disableInterrupt (void) |
| uint32_t | PSS_getInterruptStatus (void) |
| void | PSS_clearInterruptFlag (void) |
| void | PSS_enableForcedDCDCOperation (void) |
| void | PSS_disableForcedDCDCOperation (void) |
| void | PSS_registerInterrupt (void(*intHandler)(void)) |
| void | PSS_unregisterInterrupt (void) |