54 #include <ti/devices/msp432p4xx/inc/msp.h>
62 #define PSS_KEY_VALUE PSS_KEY_KEY_VAL
64 #define PSS_SVSMH PSS_IE_SVSMHIE
66 #define PSS_FULL_PERFORMANCE_MODE 0x01
67 #define PSS_NORMAL_PERFORMANCE_MODE 0x00
uint_fast8_t PSS_getHighSidePerformanceMode(void)
Definition: pss.c:125
void PSS_clearInterruptFlag(void)
Definition: pss.c:188
void PSS_enableForcedDCDCOperation(void)
Definition: pss.c:52
void PSS_disableHighSidePinToggle(void)
Definition: pss.c:86
void PSS_registerInterrupt(void(*intHandler)(void))
Definition: pss.c:195
void PSS_disableInterrupt(void)
Definition: pss.c:176
void PSS_disableHighSideMonitor(void)
Definition: pss.c:142
uint32_t PSS_getInterruptStatus(void)
Definition: pss.c:183
uint_fast8_t PSS_getHighSideVoltageTrigger(void)
Definition: pss.c:163
void PSS_setHighSidePerformanceMode(uint_fast8_t powerMode)
Definition: pss.c:113
void PSS_disableForcedDCDCOperation(void)
Definition: pss.c:61
void PSS_enableHighSideMonitor(void)
Definition: pss.c:133
void PSS_setHighSideVoltageTrigger(uint_fast8_t triggerVoltage)
Definition: pss.c:151
void PSS_unregisterInterrupt(void)
Definition: pss.c:208
void PSS_enableHighSidePinToggle(bool activeLow)
Definition: pss.c:71
void PSS_enableInterrupt(void)
Definition: pss.c:169
void PSS_disableHighSide(void)
Definition: pss.c:104
void PSS_enableHighSide(void)
Definition: pss.c:95