![]() |
![]() |
#include <stdint.h>
#include <stdbool.h>
#include <ti/devices/msp432p4xx/inc/msp.h>
Go to the source code of this file.
Macros | |
#define | PCM_KEY 0x695A0000 |
#define | PCM_AM_LDO_VCORE0 0x00 |
#define | PCM_AM_LDO_VCORE1 0x01 |
#define | PCM_AM_DCDC_VCORE0 0x04 |
#define | PCM_AM_DCDC_VCORE1 0x05 |
#define | PCM_AM_LF_VCORE0 0x08 |
#define | PCM_AM_LF_VCORE1 0x09 |
#define | PCM_LPM0_LDO_VCORE0 0x10 |
#define | PCM_LPM0_LDO_VCORE1 0x11 |
#define | PCM_LPM0_DCDC_VCORE0 0x14 |
#define | PCM_LPM0_DCDC_VCORE1 0x15 |
#define | PCM_LPM0_LF_VCORE0 0x18 |
#define | PCM_LPM0_LF_VCORE1 0x19 |
#define | PCM_LPM3 0x20 |
#define | PCM_LPM4 0x21 |
#define | PCM_LPM35_VCORE0 0xC0 |
#define | PCM_LPM45 0xA0 |
#define | PCM_VCORE0 0x00 |
#define | PCM_VCORE1 0x01 |
#define | PCM_VCORELPM3 0x02 |
#define | PCM_LDO_MODE 0x00 |
#define | PCM_DCDC_MODE 0x01 |
#define | PCM_LF_MODE 0x02 |
#define | PCM_SHUTDOWN_PARTIAL PCM_LPM35_VCORE0 |
#define | PCM_SHUTDOWN_COMPLETE PCM_LPM45 |
#define | PCM_DCDCERROR PCM_IE_DCDC_ERROR_IE |
#define | PCM_AM_INVALIDTRANSITION PCM_IE_AM_INVALID_TR_IE |
#define | PCM_SM_INVALIDCLOCK PCM_IE_LPM_INVALID_CLK_IE |
#define | PCM_SM_INVALIDTRANSITION PCM_IE_LPM_INVALID_TR_IE |
Functions | |
bool | PCM_setCoreVoltageLevel (uint_fast8_t voltageLevel) |
uint8_t | PCM_getCoreVoltageLevel (void) |
bool | PCM_setCoreVoltageLevelWithTimeout (uint_fast8_t voltageLevel, uint32_t timeOut) |
bool | PCM_setCoreVoltageLevelNonBlocking (uint_fast8_t voltageLevel) |
bool | PCM_setPowerMode (uint_fast8_t powerMode) |
bool | PCM_setPowerModeWithTimeout (uint_fast8_t powerMode, uint32_t timeOut) |
bool | PCM_setPowerModeNonBlocking (uint_fast8_t powerMode) |
uint8_t | PCM_getPowerMode (void) |
bool | PCM_setPowerState (uint_fast8_t powerState) |
bool | PCM_setPowerStateWithTimeout (uint_fast8_t powerState, uint32_t timeout) |
uint8_t | PCM_getPowerState (void) |
bool | PCM_setPowerStateNonBlocking (uint_fast8_t powerState) |
bool | PCM_shutdownDevice (uint32_t shutdownMode) |
bool | PCM_gotoLPM0 (void) |
bool | PCM_gotoLPM3 (void) |
bool | PCM_gotoLPM0InterruptSafe (void) |
bool | PCM_gotoLPM3InterruptSafe (void) |
bool | PCM_gotoLPM4 (void) |
bool | PCM_gotoLPM4InterruptSafe (void) |
void | PCM_enableRudeMode (void) |
void | PCM_disableRudeMode (void) |
void | PCM_enableInterrupt (uint32_t flags) |
void | PCM_disableInterrupt (uint32_t flags) |
uint32_t | PCM_getInterruptStatus (void) |
uint32_t | PCM_getEnabledInterruptStatus (void) |
void | PCM_clearInterruptFlag (uint32_t flags) |
void | PCM_registerInterrupt (void(*intHandler)(void)) |
void | PCM_unregisterInterrupt (void) |