![]() |
![]() |
#include <stdint.h>
#include <ti/devices/msp432p4xx/driverlib/lcd_f.h>
#include <ti/devices/msp432p4xx/driverlib/interrupt.h>
Functions | |
void | LCD_F_initModule (LCD_F_Config *initParams) |
Initializes the LCD_F Module. More... | |
void | LCD_F_turnOn (void) |
Turns on the LCD_F module. More... | |
void | LCD_F_turnOff (void) |
Turns the LCD_F off. More... | |
void | LCD_F_clearAllMemory (void) |
Clears all LCD_F memory registers. More... | |
void | LCD_F_clearAllBlinkingMemory (void) |
Clears all LCD_F blinking memory registers. More... | |
void | LCD_F_selectDisplayMemory (uint_fast16_t displayMemory) |
Selects display memory. More... | |
void | LCD_F_setBlinkingControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t mode) |
Sets the blinking control register. More... | |
void | LCD_F_setAnimationControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t frames) |
Sets the animation control register. More... | |
void | LCD_F_enableAnimation (void) |
Enables animation on the LCD_F controller. More... | |
void | LCD_F_disableAnimation (void) |
Enables animation on the LCD_F controller. More... | |
void | LCD_F_clearAllAnimationMemory (void) |
Clears all LCD_F animation memory registers. More... | |
void | LCD_F_setPinAsLCDFunction (uint_fast8_t pin) |
Sets the LCD_F pins as LCD function pin. More... | |
void | LCD_F_setPinAsPortFunction (uint_fast8_t pin) |
Sets the LCD_F pins as port function pin. More... | |
void | LCD_F_setPinsAsLCDFunction (uint_fast8_t startPin, uint8_t endPin) |
Sets the LCD_F pins as LCD function pin. More... | |
void | LCD_F_setPinAsCOM (uint8_t pin, uint_fast8_t com) |
Sets the LCD_F pin as a common line. More... | |
void | LCD_F_setPinAsSEG (uint_fast8_t pin) |
Sets the LCD_F pin as a segment line. More... | |
void | LCD_F_selectBias (uint_fast16_t bias) |
Selects the bias level. More... | |
void | LCD_F_setVLCDSource (uint_fast16_t v2v3v4Source, uint_fast16_t v5Source) |
Sets the voltage source for V2/V3/V4 and V5. More... | |
void | LCD_F_clearInterrupt (uint32_t mask) |
Clears the LCD_F selected interrupt flags. More... | |
uint32_t | LCD_F_getInterruptStatus (void) |
Returns the status of the selected interrupt flags. More... | |
uint32_t | LCD_F_getEnabledInterruptStatus (void) |
Returns the status of the selected interrupt flags masked with the currently enabled interrupts. More... | |
void | LCD_F_enableInterrupt (uint32_t mask) |
Enables the LCD_F selected interrupts. More... | |
void | LCD_F_disableInterrupt (uint32_t mask) |
Disables the LCD_F selected interrupts. More... | |
void | LCD_F_registerInterrupt (void(*intHandler)(void)) |
void | LCD_F_unregisterInterrupt (void) |