![]() |
![]() |
The Texas Instruments® MSP432® Peripheral Driver Library is a set of drivers for accessing the peripherals found on the MSP430 family of microcontrollers. While they are not drivers in the pure operating system sense (that is, they do not have a common interface and do not connect into a global device driver infrastructure), they do provide a mechanism that makes it easy to use the device's peripherals.
The capabilities and organization of the drivers are governed by the following design goals:
Some consequences of these design goals are:
For many applications, the drivers can be used as is. But in some cases, the drivers will have to be enhanced or rewritten in order to meet the functionality, memory, or processing requirements of the application. If so, the existing driver can be used as a reference on how to operate the peripheral.
Each MSP430ware driverlib API takes in the base address of the corresponding peripheral as the first parameter. This base address is obtained from the msp430 device specific header files (or from the device datasheet). The example code for the various peripherals show how base address is used. When using CCS, the eclipse shortcut "Ctrl + Space" helps. Type __MSP430 and "Ctrl + Space", and the list of base addresses from the included device specific header files is listed.
The following tool chains are supported: