![]() |
![]() |
#include <stdbool.h>
#include <ti/devices/msp432p4xx/inc/msp.h>
Go to the source code of this file.
Data Structures | |
struct | __sFlashCtl_ProtectionRegister |
Macros | |
#define | FLASH_A_BURST_PRG_BIT 0x03 |
#define | FLASH_A_SECTOR_SIZE 4096 |
#define | FLASH_A_PROGRAM_ERROR FLCTL_A_IFG_PRG_ERR |
#define | FLASH_A_BENCHMARK_INT FLCTL_A_IFG_BMRK |
#define | FLASH_A_ERASE_COMPLETE FLCTL_A_IFG_ERASE |
#define | FLASH_A_BRSTPRGM_COMPLETE FLCTL_A_IFG_PRGB |
#define | FLASH_A_WRDPRGM_COMPLETE FLCTL_A_IFG_PRG |
#define | FLASH_A_POSTVERIFY_FAILED FLCTL_A_IFG_AVPST |
#define | FLASH_A_PREVERIFY_FAILED FLCTL_A_IFG_AVPRE |
#define | FLASH_A_BRSTRDCMP_COMPLETE FLCTL_A_IFG_RDBRST |
#define | FLASH_A_NORMAL_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_0 |
#define | FLASH_A_MARGIN0_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_1 |
#define | FLASH_A_MARGIN1_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_2 |
#define | FLASH_A_PROGRAM_VERIFY_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_3 |
#define | FLASH_A_ERASE_VERIFY_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_4 |
#define | FLASH_A_LEAKAGE_VERIFY_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_5 |
#define | FLASH_A_MARGIN0B_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_9 |
#define | FLASH_A_MARGIN1B_READ_MODE FLCTL_A_BANK0_RDCTL_RD_MODE_10 |
#define | FLASH_A_PRGBRSTCTLSTAT_BURSTSTATUS_COMPLETE FLCTL_A_PRGBRST_CTLSTAT_BURST_STATUS_7 |
#define | FLASH_A_BANK0 0x00 |
#define | FLASH_A_BANK1 0x01 |
#define | FLASH_A_DATA_READ 0x00 |
#define | FLASH_A_INSTRUCTION_FETCH 0x01 |
#define | FLASH_A_MAIN_MEMORY_SPACE_BANK0 0x01 |
#define | FLASH_A_MAIN_MEMORY_SPACE_BANK1 0x02 |
#define | FLASH_A_INFO_MEMORY_SPACE_BANK0 0x03 |
#define | FLASH_A_INFO_MEMORY_SPACE_BANK1 0x04 |
#define | FLASH_A_MAIN_SPACE FLCTL_A_RDBRST_CTLSTAT_MEM_TYPE_0 |
#define | FLASH_A_INFO_SPACE FLCTL_A_RDBRST_CTLSTAT_MEM_TYPE_1 |
#define | FLASH_A_1_PATTERN FLCTL_A_RDBRST_CTLSTAT_DATA_CMP |
#define | FLASH_A_0_PATTERN 0x00 |
#define | FLASH_A_SECTOR0 FLCTL_A_BANK0_MAIN_WEPROT_PROT0 |
#define | FLASH_A_SECTOR1 FLCTL_A_BANK0_MAIN_WEPROT_PROT1 |
#define | FLASH_A_SECTOR2 FLCTL_A_BANK0_MAIN_WEPROT_PROT2 |
#define | FLASH_A_SECTOR3 FLCTL_A_BANK0_MAIN_WEPROT_PROT3 |
#define | FLASH_A_SECTOR4 FLCTL_A_BANK0_MAIN_WEPROT_PROT4 |
#define | FLASH_A_SECTOR5 FLCTL_A_BANK0_MAIN_WEPROT_PROT5 |
#define | FLASH_A_SECTOR6 FLCTL_A_BANK0_MAIN_WEPROT_PROT6 |
#define | FLASH_A_SECTOR7 FLCTL_A_BANK0_MAIN_WEPROT_PROT7 |
#define | FLASH_A_SECTOR8 FLCTL_A_BANK0_MAIN_WEPROT_PROT8 |
#define | FLASH_A_SECTOR9 FLCTL_A_BANK0_MAIN_WEPROT_PROT9 |
#define | FLASH_A_SECTOR10 FLCTL_A_BANK0_MAIN_WEPROT_PROT10 |
#define | FLASH_A_SECTOR11 FLCTL_A_BANK0_MAIN_WEPROT_PROT11 |
#define | FLASH_A_SECTOR12 FLCTL_A_BANK0_MAIN_WEPROT_PROT12 |
#define | FLASH_A_SECTOR13 FLCTL_A_BANK0_MAIN_WEPROT_PROT13 |
#define | FLASH_A_SECTOR14 FLCTL_A_BANK0_MAIN_WEPROT_PROT14 |
#define | FLASH_A_SECTOR15 FLCTL_A_BANK0_MAIN_WEPROT_PROT15 |
#define | FLASH_A_SECTOR16 FLCTL_A_BANK0_MAIN_WEPROT_PROT16 |
#define | FLASH_A_SECTOR17 FLCTL_A_BANK0_MAIN_WEPROT_PROT17 |
#define | FLASH_A_SECTOR18 FLCTL_A_BANK0_MAIN_WEPROT_PROT18 |
#define | FLASH_A_SECTOR19 FLCTL_A_BANK0_MAIN_WEPROT_PROT19 |
#define | FLASH_A_SECTOR20 FLCTL_A_BANK0_MAIN_WEPROT_PROT20 |
#define | FLASH_A_SECTOR21 FLCTL_A_BANK0_MAIN_WEPROT_PROT21 |
#define | FLASH_A_SECTOR22 FLCTL_A_BANK0_MAIN_WEPROT_PROT22 |
#define | FLASH_A_SECTOR23 FLCTL_A_BANK0_MAIN_WEPROT_PROT23 |
#define | FLASH_A_SECTOR24 FLCTL_A_BANK0_MAIN_WEPROT_PROT24 |
#define | FLASH_A_SECTOR25 FLCTL_A_BANK0_MAIN_WEPROT_PROT25 |
#define | FLASH_A_SECTOR26 FLCTL_A_BANK0_MAIN_WEPROT_PROT26 |
#define | FLASH_A_SECTOR27 FLCTL_A_BANK0_MAIN_WEPROT_PROT27 |
#define | FLASH_A_SECTOR28 FLCTL_A_BANK0_MAIN_WEPROT_PROT28 |
#define | FLASH_A_SECTOR29 FLCTL_A_BANK0_MAIN_WEPROT_PROT29 |
#define | FLASH_A_SECTOR30 FLCTL_A_BANK0_MAIN_WEPROT_PROT30 |
#define | FLASH_A_SECTOR31 FLCTL_A_BANK0_MAIN_WEPROT_PROT31 |
#define | FLASH_A_NOVER 0 |
#define | FLASH_A_BURSTPOST FLCTL_A_PRGBRST_CTLSTAT_AUTO_PST |
#define | FLASH_A_BURSTPRE FLCTL_A_PRGBRST_CTLSTAT_AUTO_PRE |
#define | FLASH_A_REGPRE FLCTL_A_PRG_CTLSTAT_VER_PRE |
#define | FLASH_A_REGPOST FLCTL_A_PRG_CTLSTAT_VER_PST |
#define | FLASH_A_FULLVER |
#define | FLASH_A_COLLATED_WRITE_MODE 0x01 |
#define | FLASH_A_IMMEDIATE_WRITE_MODE 0x02 |
#define | __INFO_FLASH_A_TECH_START__ 0x00200000 |
#define | __INFO_FLASH_A_TECH_MIDDLE__ 0x00204000 |
Typedefs | |
typedef struct __sFlashCtl_ProtectionRegister | __FlashCtl_ProtectionRegister |
Functions | |
void | FlashCtl_A_getMemoryInfo (uint32_t addr, uint32_t *bankNum, uint32_t *sectorNum) |
void | FlashCtl_A_enableReadBuffering (uint_fast8_t memoryBank, uint_fast8_t accessMethod) |
void | FlashCtl_A_disableReadBuffering (uint_fast8_t memoryBank, uint_fast8_t accessMethod) |
bool | FlashCtl_A_protectMemory (uint32_t startAddr, uint32_t endAddr) |
bool | FlashCtl_A_unprotectMemory (uint32_t startAddr, uint32_t endAddr) |
bool | FlashCtl_A_isMemoryRangeProtected (uint32_t startAddr, uint32_t endAddr) |
bool | FlashCtl_A_isMemoryProtected (uint32_t addr) |
bool | FlashCtl_A_verifyMemory (void *verifyAddr, uint32_t length, uint_fast8_t pattern) |
bool | FlashCtl_A_performMassErase (void) |
void | FlashCtl_A_initiateMassErase (void) |
bool | FlashCtl_A_eraseSector (uint32_t addr) |
bool | FlashCtl_A_programMemory (void *src, void *dest, uint32_t length) |
void | FlashCtl_A_setProgramVerification (uint32_t verificationSetting) |
void | FlashCtl_A_clearProgramVerification (uint32_t verificationSetting) |
void | FlashCtl_A_enableWordProgramming (uint32_t mode) |
void | FlashCtl_A_disableWordProgramming (void) |
uint32_t | FlashCtl_A_isWordProgrammingEnabled (void) |
bool | FlashCtl_A_setReadMode (uint32_t flashBank, uint32_t readMode) |
uint32_t | FlashCtl_A_getReadMode (uint32_t flashBank) |
void | FlashCtl_A_setWaitState (uint32_t bank, uint32_t waitState) |
uint32_t | FlashCtl_A_getWaitState (uint32_t bank) |
void | FlashCtl_A_enableInterrupt (uint32_t flags) |
void | FlashCtl_A_disableInterrupt (uint32_t flags) |
uint32_t | FlashCtl_A_getEnabledInterruptStatus (void) |
uint32_t | FlashCtl_A_getInterruptStatus (void) |
void | FlashCtl_A_clearInterruptFlag (uint32_t flags) |
void | FlashCtl_A_registerInterrupt (void(*intHandler)(void)) |
void | FlashCtl_A_unregisterInterrupt (void) |
void | FlashCtl_A_initiateSectorErase (uint32_t addr) |
uint8_t | __FlashCtl_A_remaskData8Post (uint8_t data, uint32_t addr) |
uint8_t | __FlashCtl_A_remaskData8Pre (uint8_t data, uint32_t addr) |
uint32_t | __FlashCtl_A_remaskData32Post (uint32_t data, uint32_t addr) |
uint32_t | __FlashCtl_A_remaskData32Pre (uint32_t data, uint32_t addr) |
void | __FlashCtl_A_remaskBurstDataPost (uint32_t addr, uint32_t size) |
void | __FlashCtl_A_remaskBurstDataPre (uint32_t addr, uint32_t size) |