SysCtl_A

System Control A module used for miscellaneous system configurations on MSP432P4111. More...

System Control A module used for miscellaneous system configurations on MSP432P4111.


Module Operation


Note that this module is for use exclusively on the MSP432P4111. If using the MSP432P401, please refer to the non-a variant.

The SysCtl_A module is a conglomeration of miscellaneous system control modules that do not fit into any specific hardware peripheral.

Some of the functionalities of the SysCtl_A module include:


Programming Example



Copyright 2017, Texas Instruments Incorporated