![]() |
![]() |
#include <stdint.h>#include <stdbool.h>Go to the source code of this file.
Macros | |
| #define | LZ4_MAGIC_NUMBER 0x184d2204 |
| #define | LZ4_MAX_BLOCK_SIZE 0x00100000 |
| #define | LZ4_FLG_VERSION 0x40 |
| #define | LZ4_FLG_BLOCK_INDEP 0x20 |
| #define | LZ4_FLG_BLOCK_CHECKSUM 0x10 |
| #define | LZ4_FLG_CONTENT_SIZE 0x08 |
| #define | LZ4_FLG_CONTENT_CHECKSUM 0x04 |
| #define | LZ4_BD_BYTE 0x70 |
| #define | LZ4_MIN_MATCH 4 |
| #define | LZ4_LAST_MATCH_DIST 12 |
| #define | LZ4_LAST_LITERAL_LENGTH 5 |
| #define | LZ4_TOKEN_LITERAL_MASK 0xf0 |
| #define | LZ4_TOKEN_MATCH_MASK 0x0f |
| #define | LZ4_HASH_VALUE 0x9E3779B1 |