Macros | Functions
timer32.h File Reference
#include <stdint.h>
#include <stdbool.h>
#include <ti/devices/msp432p4xx/inc/msp.h>

Go to the source code of this file.

Macros

#define TIMER32_CMSIS(x)   ((Timer32_Type *) x)
 
#define TIMER_OFFSET   0x020
 
#define TIMER32_0_BASE   (uint32_t)TIMER32_1
 
#define TIMER32_1_BASE   (uint32_t)TIMER32_2
 
#define TIMER32_0_INTERRUPT   INT_T32_INT1
 
#define TIMER32_1_INTERRUPT   INT_T32_INT2
 
#define TIMER32_COMBINED_INTERRUPT   INT_T32_INTC
 
#define TIMER32_16BIT   0x00
 
#define TIMER32_32BIT   0x01
 
#define TIMER32_PRESCALER_1   0x00
 
#define TIMER32_PRESCALER_16   0x04
 
#define TIMER32_PRESCALER_256   0x08
 
#define TIMER32_FREE_RUN_MODE   0x00
 
#define TIMER32_PERIODIC_MODE   0x01
 

Functions

void Timer32_initModule (uint32_t timer, uint32_t preScaler, uint32_t resolution, uint32_t mode)
 
void Timer32_setCount (uint32_t timer, uint32_t count)
 
void Timer32_setCountInBackground (uint32_t timer, uint32_t count)
 
uint32_t Timer32_getValue (uint32_t timer)
 
void Timer32_startTimer (uint32_t timer, bool oneShot)
 
void Timer32_haltTimer (uint32_t timer)
 
void Timer32_enableInterrupt (uint32_t timer)
 
void Timer32_disableInterrupt (uint32_t timer)
 
void Timer32_clearInterruptFlag (uint32_t timer)
 
uint32_t Timer32_getInterruptStatus (uint32_t timer)
 
void Timer32_registerInterrupt (uint32_t timerInterrupt, void(*intHandler)(void))
 
void Timer32_unregisterInterrupt (uint32_t timerInterrupt)
 

Copyright 2017, Texas Instruments Incorporated