System Control A module used for miscellaneous system configurations on MSP432P4111.
More...
System Control A module used for miscellaneous system configurations on MSP432P4111.
Module Operation
Note that this module is for use exclusively on the MSP432P4111. If using the MSP432P401, please refer to the non-a variant.
The SysCtl_A module is a conglomeration of miscellaneous system control modules that do not fit into any specific hardware peripheral.
Some of the functionalities of the SysCtl_A module include:
- Configure and enable/disable NMI sources
- Retrieve the SRAM/Flash size through software calls
- Disable/enable SRAM banks completely as well as disable retention during sleep
- Enable/disable GPIO glitch filters
- Change the type of reset that occurs on a WDT violation
Programming Example