54 #include <ti/devices/msp432p4xx/inc/msp.h>
55 #include <ti/devices/msp432p4xx/driverlib/interrupt.h>
156 #define DMA_TaskStructEntry(transferCount, \
165 (((srcIncrement) == UDMA_SRC_INC_NONE) ? (void *)(srcAddr) : \
166 ((void *)(&((uint8_t *)(srcAddr))[((transferCount) << \
167 ((srcIncrement) >> 26)) - 1]))), \
168 (((dstIncrement) == UDMA_DST_INC_NONE) ? (void *)(dstAddr) : \
169 ((void *)(&((uint8_t *)(dstAddr))[((transferCount) << \
170 ((dstIncrement) >> 30)) - 1]))), \
171 (srcIncrement) | (dstIncrement) | (itemSize) | (arbSize) | \
172 (((transferCount) - 1) << 4) | \
173 ((((mode) == UDMA_MODE_MEM_SCATTER_GATHER) || \
174 ((mode) == UDMA_MODE_PER_SCATTER_GATHER)) ? \
175 (mode) | UDMA_MODE_ALT_SELECT : (mode)), 0 \
184 #define UDMA_ATTR_USEBURST 0x00000001
185 #define UDMA_ATTR_ALTSELECT 0x00000002
186 #define UDMA_ATTR_HIGH_PRIORITY 0x00000004
187 #define UDMA_ATTR_REQMASK 0x00000008
188 #define UDMA_ATTR_ALL 0x0000000F
196 #define UDMA_MODE_STOP 0x00000000
197 #define UDMA_MODE_BASIC 0x00000001
198 #define UDMA_MODE_AUTO 0x00000002
199 #define UDMA_MODE_PINGPONG 0x00000003
200 #define UDMA_MODE_MEM_SCATTER_GATHER \
202 #define UDMA_MODE_PER_SCATTER_GATHER \
204 #define UDMA_MODE_ALT_SELECT 0x00000001
211 #define UDMA_DST_INC_8 0x00000000
212 #define UDMA_DST_INC_16 0x40000000
213 #define UDMA_DST_INC_32 0x80000000
214 #define UDMA_DST_INC_NONE 0xc0000000
215 #define UDMA_SRC_INC_8 0x00000000
216 #define UDMA_SRC_INC_16 0x04000000
217 #define UDMA_SRC_INC_32 0x08000000
218 #define UDMA_SRC_INC_NONE 0x0c000000
219 #define UDMA_SIZE_8 0x00000000
220 #define UDMA_SIZE_16 0x11000000
221 #define UDMA_SIZE_32 0x22000000
222 #define UDMA_DST_PROT_PRIV 0x00200000
223 #define UDMA_SRC_PROT_PRIV 0x00040000
224 #define UDMA_ARB_1 0x00000000
225 #define UDMA_ARB_2 0x00004000
226 #define UDMA_ARB_4 0x00008000
227 #define UDMA_ARB_8 0x0000c000
228 #define UDMA_ARB_16 0x00010000
229 #define UDMA_ARB_32 0x00014000
230 #define UDMA_ARB_64 0x00018000
231 #define UDMA_ARB_128 0x0001c000
232 #define UDMA_ARB_256 0x00020000
233 #define UDMA_ARB_512 0x00024000
234 #define UDMA_ARB_1024 0x00028000
235 #define UDMA_NEXT_USEBURST 0x00000008
243 #define UDMA_PRI_SELECT 0x00000000
244 #define UDMA_ALT_SELECT 0x00000008
256 #define DMA_CH0_RESERVED0 0x00000000
257 #define DMA_CH0_EUSCIA0TX 0x01000000
258 #define DMA_CH0_EUSCIB0TX0 0x02000000
259 #define DMA_CH0_EUSCIB3TX1 0x03000000
260 #define DMA_CH0_EUSCIB2TX2 0x04000000
261 #define DMA_CH0_EUSCIB1TX3 0x05000000
262 #define DMA_CH0_TIMERA0CCR0 0x06000000
263 #define DMA_CH0_AESTRIGGER0 0x07000000
268 #define DMA_CH1_RESERVED0 0x00000001
269 #define DMA_CH1_EUSCIA0RX 0x01000001
270 #define DMA_CH1_EUSCIB0RX0 0x02000001
271 #define DMA_CH1_EUSCIB3RX1 0x03000001
272 #define DMA_CH1_EUSCIB2RX2 0x04000001
273 #define DMA_CH1_EUSCIB1RX3 0x05000001
274 #define DMA_CH1_TIMERA0CCR2 0x06000001
275 #define DMA_CH1_AESTRIGGER1 0x07000001
280 #define DMA_CH2_RESERVED0 0x00000002
281 #define DMA_CH2_EUSCIA1TX 0x01000002
282 #define DMA_CH2_EUSCIB1TX0 0x02000002
283 #define DMA_CH2_EUSCIB0TX1 0x03000002
284 #define DMA_CH2_EUSCIB3TX2 0x04000002
285 #define DMA_CH2_EUSCIB2TX3 0x05000002
286 #define DMA_CH2_TIMERA1CCR0 0x06000002
287 #define DMA_CH2_AESTRIGGER2 0x07000002
292 #define DMA_CH3_RESERVED0 0x00000003
293 #define DMA_CH3_EUSCIA1RX 0x01000003
294 #define DMA_CH3_EUSCIB1RX0 0x02000003
295 #define DMA_CH3_EUSCIB0RX1 0x03000003
296 #define DMA_CH3_EUSCIB3RX2 0x04000003
297 #define DMA_CH3_EUSCIB2RX3 0x05000003
298 #define DMA_CH3_TIMERA1CCR2 0x06000003
299 #define DMA_CH3_RESERVED1 0x07000003
304 #define DMA_CH4_RESERVED0 0x00000004
305 #define DMA_CH4_EUSCIA2TX 0x01000004
306 #define DMA_CH4_EUSCIB2TX0 0x02000004
307 #define DMA_CH4_EUSCIB1TX1 0x03000004
308 #define DMA_CH4_EUSCIB0TX2 0x04000004
309 #define DMA_CH4_EUSCIB3TX3 0x05000004
310 #define DMA_CH4_TIMERA2CCR0 0x06000004
311 #define DMA_CH4_RESERVED1 0x07000004
316 #define DMA_CH5_RESERVED0 0x00000005
317 #define DMA_CH5_EUSCIA2RX 0x01000005
318 #define DMA_CH5_EUSCIB2RX0 0x02000005
319 #define DMA_CH5_EUSCIB1RX1 0x03000005
320 #define DMA_CH5_EUSCIB0RX2 0x04000005
321 #define DMA_CH5_EUSCIB3RX3 0x05000005
322 #define DMA_CH5_TIMERA2CCR2 0x06000005
323 #define DMA_CH5_RESERVED1 0x07000005
328 #define DMA_CH6_RESERVED0 0x00000006
329 #define DMA_CH6_EUSCIA3TX 0x01000006
330 #define DMA_CH6_EUSCIB3TX0 0x02000006
331 #define DMA_CH6_EUSCIB2TX1 0x03000006
332 #define DMA_CH6_EUSCIB1TX2 0x04000006
333 #define DMA_CH6_EUSCIB0TX3 0x05000006
334 #define DMA_CH6_TIMERA3CCR0 0x06000006
335 #define DMA_CH6_EXTERNALPIN 0x07000006
340 #define DMA_CH7_RESERVED0 0x00000007
341 #define DMA_CH7_EUSCIA3RX 0x01000007
342 #define DMA_CH7_EUSCIB3RX0 0x02000007
343 #define DMA_CH7_EUSCIB2RX1 0x03000007
344 #define DMA_CH7_EUSCIB1RX2 0x04000007
345 #define DMA_CH7_EUSCIB0RX3 0x05000007
346 #define DMA_CH7_TIMERA3CCR2 0x06000007
347 #define DMA_CH7_ADC14 0x07000007
353 #define DMA_INT0 INT_DMA_INT0
354 #define DMA_INT1 INT_DMA_INT1
355 #define DMA_INT2 INT_DMA_INT2
356 #define DMA_INT3 INT_DMA_INT3
357 #define DMA_INTERR INT_DMA_ERR
359 #define DMA_CHANNEL_0 0
360 #define DMA_CHANNEL_1 1
361 #define DMA_CHANNEL_2 2
362 #define DMA_CHANNEL_3 3
363 #define DMA_CHANNEL_4 4
364 #define DMA_CHANNEL_5 5
365 #define DMA_CHANNEL_6 6
366 #define DMA_CHANNEL_7 7
725 void *srcAddr,
void *dstAddr, uint32_t transferSize);
752 void *taskList, uint32_t isPeriphSG);
961 void (*intHandler)(
void));
1002 #endif // __UDMA_H__
uint32_t DMA_getChannelSize(uint32_t channelStructIndex)
Definition: dma.c:538
struct _DMA_ControlTable DMA_ControlTable
void DMA_disableChannelAttribute(uint32_t channelNum, uint32_t attr)
Definition: dma.c:208
volatile uint32_t spare
Definition: dma.h:84
void DMA_enableModule(void)
Definition: dma.c:38
void DMA_assignChannel(uint32_t mapping)
Definition: dma.c:635
uint32_t DMA_getChannelMode(uint32_t channelStructIndex)
Definition: dma.c:590
void DMA_setChannelControl(uint32_t channelStructIndex, uint32_t control)
Definition: dma.c:315
void DMA_assignInterrupt(uint32_t interruptNumber, uint32_t channel)
Definition: dma.c:725
void DMA_setControlBase(void *controlTable)
Definition: dma.c:110
uint32_t DMA_getInterruptStatus(void)
Definition: dma.c:754
volatile uint32_t control
Definition: dma.h:79
volatile void * dstEndAddr
Definition: dma.h:74
void DMA_requestChannel(uint32_t channelNum)
Definition: dma.c:142
volatile void * srcEndAddr
Definition: dma.h:69
uint32_t DMA_getChannelAttribute(uint32_t channelNum)
Definition: dma.c:261
void * DMA_getControlBase(void)
Definition: dma.c:124
void DMA_enableChannel(uint32_t channelNum)
Definition: dma.c:70
bool DMA_isChannelEnabled(uint32_t channelNum)
Definition: dma.c:96
void DMA_setChannelScatterGather(uint32_t channelNum, uint32_t taskCount, void *taskList, uint32_t isPeriphSG)
Definition: dma.c:469
void DMA_enableChannelAttribute(uint32_t channelNum, uint32_t attr)
Definition: dma.c:155
void DMA_registerInterrupt(uint32_t intChannel, void(*intHandler)(void))
Definition: dma.c:803
void DMA_disableChannel(uint32_t channelNum)
Definition: dma.c:83
void DMA_requestSoftwareTransfer(uint32_t channel)
Definition: dma.c:749
void DMA_disableInterrupt(uint32_t interruptNumber)
Definition: dma.c:784
void DMA_setChannelTransfer(uint32_t channelStructIndex, uint32_t mode, void *srcAddr, void *dstAddr, uint32_t transferSize)
Definition: dma.c:347
uint32_t DMA_getErrorStatus(void)
Definition: dma.c:54
void DMA_unregisterInterrupt(uint32_t intChannel)
Definition: dma.c:827
void DMA_clearInterruptFlag(uint32_t intChannel)
Definition: dma.c:759
void DMA_enableInterrupt(uint32_t interruptNumber)
Definition: dma.c:764
void * DMA_getControlAlternateBase(void)
Definition: dma.c:133
void DMA_clearErrorStatus(void)
Definition: dma.c:62
void DMA_disableModule(void)
Definition: dma.c:46