Source code, library and examples have to converted to Simplelink MSP432 SDK format
Graphics_Display constant and Graphics_initContext() have been modified. Please refer to grlib_migrationGuide.html for details of how to migrate from version 3.21.00.00 to current version
Pre-compiled grlib library is now provided for all the IDE. Makefile and projects to re-build this library is also provided
The base address/module instance name in MSP432 code examples have been changed from {PERIPHERAL_NAME}_MODULE to {PERIPHERAL_NAME}_BASE per the new device header file definitions. For example TIMER_A0_MODULE to TIMER_A0_BASE
The driverlib code examples have been updated with the following new files per each IDE requirement
system_msp432p401r.c
startup_msp432p401r_ccs.c
startup_msp432p401r_ewarm.c
2.01.00.01
Added Mac OSX and Linux support for Image Reformer.
2.00.00.17:
Added new APIs that are compliant with Texas Instruments new coding
guidelines.
Added support to draw:
Buttons
Image Buttons
Radio Buttons
Check Boxes
Please refer to the updated example projects which have been updated to use
the new buttons APIs.
Added three new examples:
MSP-EXP432P401R_GrlibExample
This example showcases grlib on MSP-EXP432P401R + BOOSTXL-K350SVG-S1
Boosterpack
MSP-EXP430F5529LP_GrLibExample
This example showcases grlib on MSP-EXP430F5529LP + BOOSTXL-K350SVG-S1
Boosterpack
MSP-EXP430FR4133_Grlib_Example
This example showcases grlib on MSP-EXP430FR4133 + 430BOOST-SHARP96
Boosterpack
Grlib can now be built in DRIVERLIB_LEAGACY_MODE
1.20.03.05:
Updated driverlib to version 1_80_00_18
Grlib can now be built in DRIVERLIB_LEAGACY_MODE
1.20.02.04:
Updated MSP-EXP430FR5969_Grlib_Example and MSP-EXP430G2_Grlib_Example example projects
Splited driver file "Sharp96x96.c" and "Sharp96x96.h" in LCD specific functionality and device specific functionality
All fucntionality related to Sharp96x96 LCD are contained in "Sharp96x96.c" and "Sharp96x96.h"
All device specific fucntionality are contained in "HAL_MSP-EXP430xxx_Sharp96x96.c" and "HAL_MSP-EXP430xxx_Sharp96x96.h"
1.20.01.01:
Converted GRLib Source Code to use C99 data types.
Removed IAR project binaries from:
Empty_Project_MSP430FR5xx_6xx_Grlib_Example
Empty_Project_MSP430FR57xx_Grlib_Example
MSP-EXP430F5659_Grlib_Example
1.20.00.09:
Added MSP-EXP430G2_Grlib_Example
CCS project uses projectspec file which allows copying files to workspace instead of linking files
Updated
MSP-EXP430FR5969 example to disable the GPIO power-on default
high-impedance mode to activate previously configured port settings
MSP430 Image Reformer Tool is not included in Graphics Library standalone version
MSP430 Image Reformer con be launch for CCS TI Resource Explorer
Removed device specific pin definition on LCD driver files for generic pin definition contained in lcddriver header file.
Removed unecessary removed unnecessary commented out code
Fixed improper SPI communication closeout on Sharp LCD drivers
Remove extra pin initialization from Sharp LCD Initialization routine
Fixed Byte reversal function for MSP-EXP430FR5969
1.10.00.00:
Fixed MSP-EXP430FR5969 to accomodate hardware changes on Sharp96x96 Boosterpack
Implemented bit revesal function on assembly for sharp lcds
Created empty project examples for MSP430F5xx_6xx, MSP430FR57xx, MSP430FR5xx_6xx using driverlib.