|
Radio Control Layer (RCL)
|
The following tables list the events handled.
| RCL Event (In) | Description |
|---|---|
| RCL_EventSetup | Setup has been performed |
| RCL_EventTimerStart | Timer-based start signalled |
| RCL Event (Out) | Description |
|---|---|
| RCL_EventCmdStarted | Command handler has accepted and started executing |
| RCL_EventLastCmdDone | The RCL is finished with the command |
| RCL_EventRxEntryAvail | An RX entry has been made available |
| RCL_EventRxBufferFinished | An RX multi-buffer is finished |
| RCL_EventTxBufferFinished | A TX buffer is finished |
| LRF Event | Description |
|---|---|
| LRF_EventOpDone | The PBE operation has finished |
| LRF_EventOpError | Something went wrong. Cause located in the PBE ENDCAUSE register |
| LRF_EventRxOk | Packet received with CRC OK and not to be ignored by the MCU |
| LRF_EventRxNok | Packet received with CRC error |
| LRF_EventRxIgnored | Packet received, but may be ignored by MCU |
| LRF_EventRxEmpty | Empty packet received |
| LRF_EventTxDone | Packet transmitted. Note: In this handler, this also means the packet is ACK'd. |