Debugging

External Resources

Debug Interfaces

The CC23xx and CC27xx platform supports serial wire debug (SWD) debug interface. SWD is an ARM bi-directional 2-wire protocol that communicates with the JTAG test access port controller, and allows for complete debug functionality. The SWD debug is inherently compatible with Texas Instruments’ XDS family of debug probes.

The hardware resources included on the devices for debugging are listed as follows. Not all debugging functionality is available in all combinations of debug probe and IDE.

  • Data Watchpoint and Trace Unit (DWT) - 2 watchpoints on memory access.

  • Breakpoint unit (BPU) - 4 breakpoint registers.

XDS110 Debug Probe

Some CC23xx and CC27xx platforms, like the LP-EM-CC2340R5 have a split-LaunchPad design, which is includes a detachable XDS110 debug board. The CC23xx LaunchPad supports a 20-pin LP-EM debug connector, and this is the assumed debug probe for most development.

The XDS110 is the latest entry level debug probe (emulators) for TI embedded processors. Designed to be a complete solution that delivers JTAG and SWD connectivity at a low cost, the XDS110 is the debug probe of choice for entry-level debugging of TI microcontrollers, processors and SimpleLink devices. Also, both Core Processor and System Trace are available for all Arm and DSP devices that support Embedded Trace Buffer (ETB).

It is possible to buy the XDS110 as a standalone debugger. For example: XDS110ET LaunchPad

Configuring Debugger in Code Composer Studio

If only one debug probe is attached, CCS will automatically select the connected debug probe when a debug session is started. You can start a debug session by clicking the debug icon img_icon_debug_ccs on the toolbar.

If more than one debug probe is attached when a debug session is started, CCS will prompt you to select a debug probe as seen in Figure 38. CCS will save the selected debug probe in the target configuration for the project.

../../../_images/ccs_probe_select.png

Figure 38. CCS Probe Selection

To set or change the selected debug probe for a project, it is necessary to set the serial number for the probe in the project’s target configuration.

  1. Open the target configuration file.

../../../_images/ccs_targetconfig_file_cc23xx.png
  1. Open the Advanced pane.

../../../_images/ccs_targetconfig_advanced_pane_cc23xx.png
  1. Choose the top-level debugger entry.

../../../_images/ccs_targetconfig_probe_cc23xx.png
  1. Enter the serial number.

../../../_images/ccs_targetconfig_serial.png

Find The Serial Number

To find the serial number for XDS110 debug probe, open a command prompt and run the xdsdfu.exe command for your CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -e. For UniFlash, the command will be: <UNIFLASH_INSTALL_DIR>\deskdb\content\TICloudAgent\win\ccs_base\common\uscif\xds110\xdsdfu.exe -e. This will enumerate all the attached XDS110 debug probes. This should result in output like the following.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -e

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...


<<<< Device 0 >>>>

VID: 0x0451    PID: 0xbef3
Device Name:   XDS110 Embed with CMSIS-DAP
Version:       3.0.0.22
Manufacturer:  Texas Instruments
Serial Num:    LS420073
Mode:          Runtime
Configuration: Standard

Found 1 devices.

C:\>

Note

More information of the tool can be found in <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\XDS110SupportReadMe.pdf

For XDS100 series debug probes, open a command prompt and run the xds100serial.exe command for your CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds100serial.exe. This should result in output like the following:

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds100serial.exe
Scanning for XDS100 emulators...

VID/PID    Type            Serial #    Description
0403/a6d1  XDS100v3        06EB12213144  Texas Instruments XDS100v3

C:\>

Configure the Serial Number

Open the xdsdfu.exe command for your CCS version, e.g.

  • <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -m

  • <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -s LS470000 -r

These will first switch XDS110 to DFU mode if it is already in runtime mode, then set the serial number to the LS470000. The output should be like the following.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -m

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...


<<<< Device 0 >>>>

VID: 0x0451    PID: 0xbef3
Device Name:   XDS110 Embed with CMSIS-DAP
Version:       3.0.0.22
Manufacturer:  Texas Instruments
Serial Num:    L1100JU9
Mode:          Runtime
Configuration: Standard

Switching device into DFU mode.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -s LS470000 -r

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...

Setting serial number to "LS470000"...

C:\>

Program Board ID on LP-EM Boards

It is possible that in some very rare circumstances different LP-EM Boards are with the same Board ID or with empty Board ID. In this case:

  • UniFlash may not identify the device correctly

  • CCS may not identify the board correctly

Programming the different Board ID to each board should help. It can be done also by open a command prompt and run the xdsdfu.exe command. Plug only one LP-EM board to the host PC. Unplug all other boards. For CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -p. For UniFlash, the command will be: <UNIFLASH_INSTALL_DIR>\deskdb\content\TICloudAgent\win\ccs_base\common\uscif\xds110\xdsdfu.exe -p. This should result in output like the following:

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -p LS47XXXX

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...

Setting serial number prefix to "LS47XXXX"...

The serial prefix was set in EEPROM.
Power cycle the XDS110 for the change to take effect.

After running the command, unplug and re-plug the LP-EM board to the host PC to acknowledge the new Board ID to the host PC.

Connecting to the XDS Debugger

If only one debugger is attached, the IDE uses it automatically when you click the img_icon_debug_ccs button in CCS

If multiple debuggers are connected, you must choose the individual debugger to use. The following steps detail how to select a debugger in CCS

Breakpoints

Comparators in the Flash Patch and Breakpoint Unit (FPB) of the CC23xx LaunchPad are used to break on an instruction fetch. This can be used to patch a function as it is fetched from instruction memory. Or these comparators can be used to supply a Breakpoint (BKPT) instruction to the CPU. These instructions halt the processors operation, waiting for the debug probe.

Considerations

While breakpoints are a useful tool for debugging code online, they have the possibility of altering the execution flow of a piece of code.

Breakpoints and Timing

Synchronous RF protocols are timing sensitive. Breakpoints can easily halt the execution long enough to lose network timing and break the link.

To still be able to debug, place breakpoints as close as possible to where the relevant debug information can be read or step through the relevant code segment to debug.

After you hit a breakpoint and read out the necessary debug information, it is recommended that you reset the device and re-establish the connection.

Breakpoints and Optimization

When compiler optimizations are enabled, toggling a breakpoint on a line of C code may not result in the expected behavior. Some examples include the following.

Code is removed or not compiled in

Toggling a breakpoint in the IDE results in a breakpoint somewhere other than the intended line. Some IDEs disable breakpoints on nonexistent code.

Code block is part of a common subexpression

A breakpoint might be trigged from a function or piece of code near the marked line. This might have been due to the compiler reusing sections.

An if clause is represented by a conditional branch in assembly

A breakpoint inside an if clause always breaks on the conditional statement, even when the condition is not true.

TI recommends selecting an optimization level as low as possible when debugging. See sect_debug_optim for information on modifying optimization levels.

Note

Due to limitation of Cotex-CM0+, the number of breakpoints for CC23xx or CC27xx devices is 4. Check breakpoints limitation of ARM Cortex-CM0+. During programming stage, debugger will use 3. Breakpoints set by application will be ignored if more than one breakpoint is used by the application. It is possible to gain one more breakpoint back by implementing the following steps. Right click on the project, go to Debug As->Debug Configuration->Target, unchecked ‘Enable CIO function use’.

../../../_images/gain_one_more_breakpoint.png

Breakpoints in CCS

Note

CCS reserves one hardware breakpoint for instruction stepping.

To toggle a breakpoint, do any of the following.

  • Double-click the area to the left of the line number.

  • Press Ctrl + Shift + B.

  • Right-click on the line.

A breakpoint set on line 207 in CCS Eclipse, and line 73 on CCS Theia looks like the following.

../../../_images/ccs_breakpoint_ex.png

Figure 39. Breakpoint on line 207. Debugger halted at start of main().

../../../_images/ccs_theia_breakpoint_ex.png

Figure 40. CCS Theia Breakpoint on line 73.

For an overview of the active and inactive breakpoints, click on ViewBreakpoints.

../../../_images/ccs_breakpoint_list.png

Figure 41. List of breakpoints. Right-click to edit options, or de-select to deactivate.

../../../_images/ccs_theia_breakpoint_list.png

Figure 42. Once you enter debug window on CCS Theia, the breakpoints are automatically listed.

To set a conditional break, do as follows.

  1. Right-click the breakpoint in the overview.

  2. Choose Properties.

When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.

Note

Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.

Breakpoints in IAR

Note

IAR reserves one comparator for instruction stepping.

To toggle a breakpoint, do any of the following.

  • Single-click the area to the left of the line number.

  • Go to the line and press F9 to toggle breakpoint

  • Right-click on the line and select Toggle Breakpoint (Code).

A breakpoint looks like this:

../../../_images/iar_breakpoint_ex.png

Figure 43. Breakpoint on PIN_init(). Debugger halted at start of main().

For an overview of the active and inactive breakpoints, click ViewBreakpoints.

../../../_images/iar_breakpoint_list.png

Figure 44. List of breakpoints. Right-click to edit options, or de-select to deactivate.

To set a conditional break, do as follows.

  1. Right-click the breakpoint in the overview.

  2. Choose Edit….

When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.

Note

Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.

Watching Variables and Registers

Debuggers offer several ways of viewing the state of a halted program. Global variables are statically placed during link-time and can end up anywhere in the RAM or Flash of the chip. These variables can be viewed when then target is halted by the debugger through the Watch and Expression windows.

Unless removed due to optimizations, global variables are always available in these views. Local variables or variables that are only valid inside a limited scope are only viewable in that scope. Such variables can also be viewed with the Watch or Expression views, and may also be automatically displayed when breaking or stepping through code.

Considerations

Local variables are often placed in CPU registers and not on the stack. These variables also have a limited lifetime even within the scope in which they are valid. Depending on the optimization performed, a variable placed in a register may not have a cohesive view of the current state of the variable. Some possible solutions are:

  • Move the variable to global scope, so it remains accessible in RAM.

  • Make the variable volatile, so the compiler doesn’t place the value in a register.

  • Make a shadow copy of the variable that is global and volatile.

Variables in CCS

You can view Global Variables by doing either of the following.

  • Select ViewExpressions.

  • Select a variable name in code.

  • Right-click and select Add Watch Expression.

../../../_images/ccs_watch.png

Figure 45. Variable watch window. Note that you can cast values, get address and sizeof, etc.

  • Select ViewVariables to auto-variables that are present at the current location when stepping through code.

../../../_images/ccs_locals.png

Figure 46. Local variables. This screenshot is taken during execution of an application function.

../../../_images/ccs_theia_locals.png

Figure 47. CCS Theia Local variables. Once debug mode is entered you can view the local variables automatically.

Variables in IAR

To view Global Variables, do either of the following.

  • Right-click on the variable.

    • Select Add to Watch: varName.

  • Select ViewWatch

    • Enter the name of the variable.

../../../_images/iar_watch.png

Figure 48. Variable watch window. Note that you can cast values, get address and sizeof, etc.

View –> Locals show the local variables in IAR.

../../../_images/iar_locals.png

Figure 49. Local variables. This screenshot is taken during execution of the Simple Peripheral init function.

Note

IAR may remove the variable during optimization and inline the usage of the value. If so, add the __root directive in front.

Memory Overview

This section aims to describe the various memory regions available on the device as well as how they are used by the stack and application. The chapter starts with an overview of the memory map of the device, and then each section goes into detail on how this memory region is used. See the CC23xx SimpleLink Wireless MCU Technical Reference Manual for more details.

Memory Watchpoints

As mentioned in Debug Interfaces, the Data Watchpoint and Trace Unit (DWT module) contains four memory watchpoints that allow breakpoints on memory access. The hardware match functionality looks only at the address. If intended for use on a variable, the variable must be statically allocated.

Note

If a data watchpoint with value match is used, two of the four watchpoints are used.

Watchpoints in CCS

Warning

Watchpoint are not available on CC2340R5 and CC2340R21

  1. Right-click on a global variable.

  2. Select BreakpointHardware Watchpoint.

  3. Go to the list of breakpoints (ViewBreakpoints).

  4. Right-click and edit the Breakpoint Properties to configure the watchpoint.

../../../_images/ccs_watchpoint_add.png

Figure 50. Adding a watchpoint on a variable.

This example configuration ensures that if 0x42 is written to the memory location for Characteristic 1 in the Bluetooth Low Energy basic_ble example project the device halts execution.

../../../_images/ccs_watchpoint_configure.png

Figure 51. Configuring a hardware watchpoint to break on 8-bit write with value 0x42.

Watchpoints in IAR

  1. Right-click a variable (global).

  2. Select Set Data Breakpoint for 'myVar' to add it to the active breakpoints.

  3. Go to the list of breakpoints (View –> Breakpoints)

  4. Choose Edit... to set up whether the watchpoint should match on read, write, or any access.

../../../_images/iar_watchpoint_configure.png

Figure 52. Configuring a hardware watchpoint to break on 8-bit write with value 0x42.

RTOS Object Viewer

Debuggers may include the RTOS Object Viewer (ROV) plug-in that provides insight into the current state of RTOS, including task states, stacks, and so forth.

This section discusses some ROV views useful for debugging and profiling. More details can be found in the RTOS User’s Guide, including documentation on how to add log events to application code.

Scanning the BIOS for Errors

The BIOS Scan for errors view goes through the available ROV modules and reports on errors. This functionality can be a good point to start if anything has gone wrong. This scan only shows errors related to RTOS modules and only the errors it can catch.

../../../_images/rov_bios_scan.png

Figure 53. Scan for errors. Here a Task Stack has been overrun.

Viewing the State of Each Task

The Task Detailed view is useful for seeing the state of each task and its related runtime stack usage. This example shows the state the first time the user-thread is called. Figure 54. shows the Bluetooth low energy stack task, represented by its ICall proxy, the Idle task, the simple_peripheral task and the GAPRole task.

../../../_images/rov_task_detailed.png

Figure 54. Detailed view of the Tasks. Notice the address of the overrun task matches the instance id from Scan for errors.

The following list explains the column in Figure 54.

address

This column shows the memory location of the Task_Struct instance for each task.

priority

This column shows the RTOS priority for the task.

mode

This column shows the current state of the task.

fxn

This column shows the name of the entry function of the task.

arg0, arg1

These columns show arbitrary values that can be given to entry function of the task. In the image, the ICall_taskEntry is given 0xb001, which is the flash location of the entry function of the RF stack image and 0x20003a30 (the location of bleUserCfg_t user0Cfg, defined in main()).

stackPeak

This column shows the maximum run-time stack memory used based on watermark in RAM, where the stacks are prefilled with 0xBE and there is a sentinel word at the end of the run-time stack.

Note

Function calls may push the stack pointer out of the run-time stack, but not actually write to the entire area. A stack peak near stackSize but not exceeding it may indicate stack overflow.

stackSize

This column shows the size of the runtime stack, configured when instantiating a task.

stackBase

This column shows the logical top of the runtime stack of the task (usage starts at stackBase + stackSize and grows down to this address).

Viewing the System Stack

The Hwi Module view allows profiling of the system stack used during boot or for main(), Hwi execution, and Swi execution.

../../../_images/rov_hwi_module.png

Figure 55. Viewing the System Stack in the Hwi view of ROV

The hwiStackPeak, hwiStackSize, and hwiStackBase can be used to check for system stack overflow.

ROV in CCS

To access the ROV while in a debug session in CCS:

../../../_images/ccs_rov_enable.png

Attention

You can enable live watch on ROV to automatically retrieve up to date information, however, the refreshing rate is not frequent. You can also pause the debugger or manually click refresh button to enforce a ROV information update.

Using the Memory Browser

Open the memory browser at ViewMemory Browser to explore the memory on the CC23xx or CC27xx. In CCS, you can index by address or by symbol name.

Basic BLE Task’s stack (Note the A5 watermark).

GAPRole Task’s stack has probably overflowed as it is completely filled.

../../../_images/mem_browser_sbp_stack-cc23xx.png
../../../_images/mem_browser_gaprole_stack.png

The solution in this case would be to increase the stack size for the failing task and see what the stack peak really is. The stackPeak reported in Detailed ROV Task is relying on how many watermark bytes are overwritten, so it can’t know how much the overrun amounts to.

../../../_images/rov_task_detailed_cc2340.png

Figure 56. Detailed ROV Task

Because stacks are utilized from higher addresses towards lower addressed (upwards in the picture), stacks that overrun will tend to overwrite data at locations immediately before the stack.

Connect the debugger to a running target

Connecting the debugger to a target can help when you want to see the status of your target after it has been running for several hours, or even days; or if you cannot reproduce a crash with the debugger attached. Once the debugger connected to the target, all the usual functionalities (break points, step-by-step, variable view, ROV, memory view…) are available.

This step-by-step guide will help you to configure CCS in order to connect to a running target

  1. Modify the GEL file

    In a very simplistic view, the GEL files describe the way the device’s debugger has to act (more details can be found in the CCS’s help). By default, the GEL files ask the device to reset when the debugger is started up. Fortunately we can modify this:

    1. Identify the GEL file to modify

      • Start a debug session as always

      • (If needed), display the debug view

      • Right-click on the program being, “Open GEL files View”.

      • In the GEL files list, open the corresponding GEL file by double-clicking it. Chose cc26x2.gel for CC26x2 and CC13x2 devices. Chose cc26x0.gel for CC26x0 and CC13x0 devices.

      ../../../_images/locate_gel_file.png

      Figure 57. Locate the GEL file to modify.

      Figure 57. shows how to find the GEL file to modify.

      Note

      Another possibility consists in looking directly in <CCS directory>\ccs_base\emulation\gel for the GEL file.

      Caution

      The modifications done in a GEL file affect all the devices using the same GEL files. In other words, it affects all the CC26X2 and CC13X2 if you modified cc26x2.gel, and all the CC26x0 and CC13x0 if you modified cc26x0.gel. By default, two different CCS versions do not use the same GEL files.

    2. In the StartUp() function, comment out the code executing the reset. If needed, an explicit comment will help you to identify the code to comment out.

      Listing 17. The StartUp() function after modification.
       1StartUp(int major, int minor, int patch)
       2{
       3    /* Initialize memory map */
       4    memorymap_init();
       5
       6    /* Debugger specific handling */
       7    if(GEL_MatchesConnection(".*TIXDS.*") == 1)
       8    {
       9        GEL_LoadGel("$(GEL_file_dir)/cc26xx_connect_util.gel");
      10        GEL_LoadGel("$(GEL_file_dir)/cc26x2_xds.gel");
      11
      12        DefineResets(0);
      13
      14        // Issue Board Reset to ensure device is in a known state
      15        // Note: If you want to attach to a running target without resetting the
      16        //       device, you must comment out the following 4 lines:
      17    //  if(!GEL_IsConnected())
      18    //  {
      19    //      GEL_AdvancedReset("Board Reset");
      20    //  }
      21    }
      22    else if(GEL_MatchesConnection(".*JLink.*") == 1)
      23    {
      24        GEL_LoadGel("$(GEL_file_dir)/cc26xx_jlink.gel");
      25    }
      26    else
      27    {
      28        GEL_TextOut("Error: Unknown debugger.\n");
      29        return;
      30    }
      31}
      
    3. Save your modification and close the file. Stop your debugging session

    Caution

    The modification of the debug configurations only affects one project.

  2. Modify the Debug Configuration of your project

    Once you have clicked CCS’s debug button (the green bug), CCS is doing a lot of actions for you. For example, CCS loads the program and stops the execution of the code on the target. In our case, we don’t want CCS to load the program (as we already have a running program…). In addition, we don’t necessarily want to stop the execution of the code on the target. Fortunately, the way CCS is running a debug session is highly configurable. So let’s adapt those configurations to our needs.

    1. On the right of the Debug button, there is an arrow. Click this arrow and select Debug Configurations….

    2. Select your project

    3. Prevent CCS from loading the program: in the Program tab, chose the proper Loading options (Load symbols only)

      ../../../_images/debug_configuration_1.png

      Figure 58. Open the Debug configurations and modify the loading options.

    4. Prevent CCS from stopping the target: in the Target tab, deselect the option Halt the target on a connect

    ../../../_images/debug_configuration_2.png

    Figure 59. In the Debug configurations, modify the Connection options.

  3. [Optional] Prevent CCS from building the program before load

    As no program will be loaded, it is a bit useless to ask CCS to build an image when you start a debug session. As result, you can disable this option by using the small arrow at the right of the Flash button. Click on Build Project Before Load in order to disable the option.

    ../../../_images/build_project_before_load.png

    Figure 60. Disable “Build Project Before Load” option.

    Now, the debug button does not anymore load code on the device. So, how can you load a new image on the device? The easiest way is to use the Flash button and select the image to flash. Don’t forget to rebuild your image manually (as we have disabled the option before). Another solution consists in undoing all the configuration changes we did before. A third solution consists in using a different version of CCS.

Tip

You are all set now! Let the code running and, when needed, connect to the running target by using the Debug button as you usually do.

Deciphering Exceptions

Several possible exception causes exist. If an exception is caught, an exception handler function can be called. Arm Cortex User Guide describes more about exception handler. There are ways to determine whether the hang up is due to the hard fault. One is to watch the Program Counter (PC) register which will indicate operation in the hard fault handler. The second method is to watch the special-purpose program status registers (xPSR).

../../../_images/exception_registers.png

Figure 61. Exception Registers

Key Registers to Read During an Exception

When entering an exception handler, the following registers provide critical information for debugging. The CC23xx family uses the Cortex-M0+ core, while devices like the CC27xx and CC35xx use the Cortex-M33 core. Both cores share common exception handling concepts but the Cortex-M33 provides additional fault status registers for more detailed diagnostics.

Core Registers (Stacked by Hardware)

When an exception occurs, the ARM Cortex-M0+ and Cortex-M33 automatically push the following registers onto the stack:

Table 4. Stacked Registers

Register

Description

R0-R3

General-purpose registers that were in use at the time of the exception.

R12

Intra-procedure scratch register.

LR (R14)

Link Register containing the return address before the exception.

PC (R15)

Program Counter pointing to the instruction that caused the exception (or the next instruction, depending on exception type).

xPSR

Combined Program Status Register containing condition flags, exception number, and thumb state.

The stack frame layout (from lower to higher addresses) is: R0, R1, R2, R3, R12, LR, PC, xPSR

Program Status Register (xPSR)

The xPSR register is a combination of three status registers:

Table 5. xPSR Bit Fields

Bits

Field

Description

[31]

N

Negative flag: Set if result of last operation was negative.

[30]

Z

Zero flag: Set if result of last operation was zero.

[29]

C

Carry flag: Set if last operation resulted in a carry.

[28]

V

Overflow flag: Set if last operation caused signed overflow.

[24]

T

Thumb state bit: Always 1 for Cortex-M0+/M33 (Thumb mode only).

[8:0]

Exception

Exception number currently being serviced (0 = Thread mode). Cortex-M0+ uses bits [5:0], Cortex-M33 uses bits [8:0] for more exception sources.

Common exception numbers in the xPSR exception field:

  • 0: Thread mode (no exception active)

  • 2: NMI (Non-Maskable Interrupt)

  • 3: HardFault

  • 4: MemManage Fault (Cortex-M33 only)

  • 5: BusFault (Cortex-M33 only)

  • 6: UsageFault (Cortex-M33 only)

  • 7: SecureFault (Cortex-M33 with TrustZone only)

  • 11: SVCall (Supervisor Call)

  • 14: PendSV

  • 15: SysTick

  • 16+: External interrupts (IRQ0 starts at 16)

Extracting the Faulting Address

To determine where the fault occurred, read the stacked PC value from the exception stack frame. In your fault handler:

void HardFault_Handler(void)
{
    __asm volatile (
        "MRS R0, MSP        \n"  // Get Main Stack Pointer
        "LDR R1, [R0, #24]  \n"  // Load stacked PC (6th word = 24 bytes offset)
        "BKPT #0            \n"  // Breakpoint for debugger
    );
}

Alternatively, in the debugger, manually inspect the stack:

  1. Read the current SP (Stack Pointer) value

  2. The stacked PC is at offset SP + 24 (6 words × 4 bytes)

  3. The stacked xPSR is at offset SP + 28

Common HardFault Causes on Cortex-M0+

Since the Cortex-M0+ has a simplified fault model (only HardFault, no separate MemManage/BusFault/UsageFault), common causes include:

  • Invalid memory access: Accessing unmapped or protected memory regions

  • Unaligned access: Accessing 16-bit or 32-bit data at odd addresses

  • Invalid instruction: Executing from non-executable memory or corrupted code

  • Stack overflow: SP pointing to invalid memory

  • Division by zero: If enabled in NVIC configuration

  • Invalid exception return: Corrupted EXC_RETURN value in LR

Cortex-M33 Fault Status Registers

The Cortex-M33 provides detailed fault status registers that give specific information about what caused a fault. These registers are located in the System Control Block (SCB).

Configurable Fault Status Register (CFSR) - 0xE000ED28

The CFSR is a 32-bit register combining three fault status registers:

  • Bits [31:16]: UsageFault Status Register (UFSR)

  • Bits [15:8]: BusFault Status Register (BFSR)

  • Bits [7:0]: MemManage Fault Status Register (MMFSR)

MemManage Fault Status Register (MMFSR) - CFSR[7:0]
Table 8. MMFSR Bit Fields

Bit

Name

Description

[7]

MMARVALID

MMFAR holds a valid fault address.

[5]

MLSPERR

MemManage fault during FP lazy state preservation.

[4]

MSTKERR

MemManage fault on stacking for exception entry.

[3]

MUNSTKERR

MemManage fault on unstacking for exception return.

[1]

DACCVIOL

Data access violation. The MMFAR contains the faulting address.

[0]

IACCVIOL

Instruction access violation.

BusFault Status Register (BFSR) - CFSR[15:8]
Table 9. BFSR Bit Fields

Bit

Name

Description

[15]

BFARVALID

BFAR holds a valid fault address.

[13]

LSPERR

BusFault during FP lazy state preservation.

[12]

STKERR

BusFault on stacking for exception entry.

[11]

UNSTKERR

BusFault on unstacking for exception return.

[10]

IMPRECISERR

Imprecise data bus error. May not have exact faulting address.

[9]

PRECISERR

Precise data bus error. BFAR contains the faulting address.

[8]

IBUSERR

Instruction bus error.

UsageFault Status Register (UFSR) - CFSR[31:16]
Table 10. UFSR Bit Fields (CFSR bits [31:16])

Bit

Name

Description

[25]

DIVBYZERO

Divide by zero (when DIV_0_TRP is enabled in CCR).

[24]

UNALIGNED

Unaligned memory access (when UNALIGN_TRP is enabled in CCR).

[20]

STKOF

Stack overflow detected (ARMv8-M/Cortex-M33 only).

[19]

NOCP

Attempted to access a coprocessor that does not exist or is disabled.

[18]

INVPC

Invalid PC load via EXC_RETURN (invalid value in LR).

[17]

INVSTATE

Invalid state (e.g., attempting to execute ARM instructions).

[16]

UNDEFINSTR

Undefined instruction executed.

HardFault Status Register (HFSR) - 0xE000ED2C

Table 11. HFSR Bit Fields

Bit

Name

Description

[31]

DEBUGEVT

Debug event occurred (e.g., breakpoint with debug not enabled).

[30]

FORCED

Forced HardFault. Indicates the HardFault was caused by a configurable fault that was escalated (e.g., BusFault with handler disabled).

[1]

VECTTBL

Vector table read fault on exception processing.

Fault Address Registers

Table 12. Fault Address Registers

Register

Address

Description

MMFAR

0xE000ED34

MemManage Fault Address Register. Valid when MMFSR.MMARVALID is set.

BFAR

0xE000ED38

BusFault Address Register. Valid when BFSR.BFARVALID is set.

SFAR

0xE000EDE8

SecureFault Address Register (TrustZone). Valid when SFSR.SFARVALID is set.

SecureFault Status Register (SFSR) - 0xE000EDE4

For Cortex-M33 with TrustZone enabled:

Table 13. SFSR Bit Fields

Bit

Name

Description

[7]

LSERR

Lazy state error during floating-point lazy stacking.

[6]

SFARVALID

SFAR contains a valid address.

[5]

LSPERR

Lazy state preservation error.

[4]

INVTRAN

Invalid transition from Secure to Non-secure state.

[3]

APTS

Attribution unit poisoning error.

[2]

INVIS

Invalid Secure state entry from Non-secure state.

[1]

INVER

Invalid exception return from Non-secure state.

[0]

INVEP

Invalid entry point to Secure state.

Reading Fault Registers in Code (Cortex-M33)

#include <stdint.h>

/* SCB Fault Status Register addresses */
#define SCB_CFSR   (*(volatile uint32_t *)0xE000ED28)
#define SCB_HFSR   (*(volatile uint32_t *)0xE000ED2C)
#define SCB_MMFAR  (*(volatile uint32_t *)0xE000ED34)
#define SCB_BFAR   (*(volatile uint32_t *)0xE000ED38)
#define SCB_SFSR   (*(volatile uint32_t *)0xE000EDE4)
#define SCB_SFAR   (*(volatile uint32_t *)0xE000EDE8)

/* Extract sub-registers from CFSR */
#define CFSR_MMFSR  (SCB_CFSR & 0xFF)
#define CFSR_BFSR   ((SCB_CFSR >> 8) & 0xFF)
#define CFSR_UFSR   ((SCB_CFSR >> 16) & 0xFFFF)

void HardFault_Handler(void)
{
    volatile uint32_t cfsr  = SCB_CFSR;
    volatile uint32_t hfsr  = SCB_HFSR;
    volatile uint32_t mmfar = SCB_MMFAR;
    volatile uint32_t bfar  = SCB_BFAR;

    /* Check if FORCED bit is set - fault escalated from configurable fault */
    if (hfsr & (1 << 30)) {
        /* Check MemManage fault */
        if (cfsr & 0xFF) {
            if (cfsr & (1 << 7)) {
                /* MMFAR valid - mmfar contains faulting address */
            }
        }
        /* Check BusFault */
        if ((cfsr >> 8) & 0xFF) {
            if (cfsr & (1 << 15)) {
                /* BFAR valid - bfar contains faulting address */
            }
        }
        /* Check UsageFault */
        if ((cfsr >> 16) & 0xFFFF) {
            /* Check specific usage fault bits */
        }
    }

    /* Clear fault status bits by writing 1s */
    SCB_CFSR = cfsr;
    SCB_HFSR = hfsr;

    __asm volatile ("BKPT #0");  /* Breakpoint for debugger */
    while (1);
}

Debugger Quick Reference for Cortex-M33

When stopped in a fault handler, read these memory addresses:

  1. 0xE000ED28 (CFSR): Combined fault status - check which fault type occurred

  2. 0xE000ED2C (HFSR): HardFault status - check FORCED bit [30]

  3. 0xE000ED34 (MMFAR): MemManage fault address (if CFSR[7]=1)

  4. 0xE000ED38 (BFAR): BusFault address (if CFSR[15]=1)

  5. Stack pointer + 24: Stacked PC (faulting instruction address)

  6. Stack pointer + 28: Stacked xPSR

Debugging guide for serial interfaces

The aim of this chapter is to give some pointers on what to check if some issues are seen when using the UART, SPI, or I2C interfaces.

Note: TI only supports how to use the serial interface modules and the TI supplied drivers for these interfaces. TI are not able to help on the usage of a non-TI device connected to I2C, SPI or UART.

I2C

  • The I2C interface needs an external pull-up resistor. On the LauchPad these are 3.3 kOhm.

  • Measure the waveform on the I2C interface with an oscilloscope to verify the SCL and SDA levels

  • Monitor the interface with a logic analyzer. Check that data on the bus is the same as the wanted data.

  • Check the interface by reading out the device ID of the sensor.

  • Check the slave address. The I2C module uses a 7-bit address. The last 8th bit is the data direction bit. This last bit is appended automatically by the driver/HW. The Slave address given to the driver has therefore to be 7-bit.

  • Ensure that the readCount and writeCount is according to the register size used. If the result register in the sensor is 16-bit, the readCount has to be set to 2.

SPI

  • Monitor the interface with a logic analyzer. Compare the waveform with the waveform given in the datasheet for the device you are communicating with.

  • Check that the CSn is set correctly.

  • Check that the frame format is set correctly. Check if the device you are communicating with uses SPO = 1 or 0 and SPH = 1 or 0.

UART

  • Make sure to connect the TX pin of one device to the RX pin of the other device, and vice versa. If flow control is enabled, then the same applies towards the CTS and RTS pins.

  • Verify all communication settings between devices, including baud rate, data length, stop/parity bits and flow control.

  • Evaluate the interface with a logic analyzer or oscilloscope, using an analyzer tool if possible to convert the waveforms into their numerical counterpart.