Hardware Architecture¶
The CC23xx Family¶
Arm Cortex-M0+ (Device Core)¶
The device core (CM0+) is designed to run the wireless protocol stack from the radio layer up to the user application. By only using one core for the solution, the CC23xx family is optimized for both cost and power.
Flash, RAM, and Peripherals¶
Depending on the model, devices in the CC23xx family contain between 256 kB-512 kB of in-system programmable flash memory and 28 kB-64 kB of SRAM. See the table below for a breakdown each device. The CC23xx also hosts a full range of peripherals including UART, I2C, AES, RNG, temperature and battery monitors, timers, and 1 SSI.
Note
Within the SDK and related software tools, the CC2340R2 refers to the CC2340R2(1) device and the CC2340R5 refers to the CC2340R5(2) device. The precise device names are used in the following table.
CC2340R21 |
CC2340R22 |
CC2340R5 |
CC2340R5-Q1 |
CC2340R53 |
|
|---|---|---|---|---|---|
Flash |
256 kB |
256 kB |
512 kB |
512 kB |
512 kB |
SRAM |
28 kB |
36 kB |
36 kB |
36 kB |
64 kB |
The CC27xx Family¶
Arm Cortex-M33 (Device Core)¶
The Cortex-M33 (CM33) core within the CC27xx is responsible for both interfacing to the radio hardware and implementing the PHY layer of the protocol stack with BLE5-Stack. It translates instructions into bits that are sent over the air using the radio in an optimized manner for BLE performance and power-consumption.
Hardware Security Module¶
The Hardware Security Module (HSM) is used to create an isolated environment for cryptographic, key management, secure counters, and random number generation operations. The HSM supports energy-efficient operations for the following functions: Key Agreement Schemes, Signature Processing, Message Authentication Codes, Block Cipher Modes of Operation, Hash Algorithms, and Random Number Generation.
The HSM has its own RAM that is not accessable to the rest of the system but the HSM does have the capability to access the system memory directly. The SimpleLink Low Power F3 SDK includes the necessary firmware and drivers for all the HSM operations and functions.
Trusted Firmware-M¶
The CC27xx supports Trusted Firmware-M (TF-M) for Armv8-M that implements the Secure Processing Environment (SPE) for the CM33 that enables PSA (Platform Security Architecture) Certification. TF-M consists of:
- Secure Boot to authenticate Non-Secure Processing Environment (NPSE)
and Secure Processing Environment (SPE) firmware image integrity.
TF-M Core for controlling the isolation, communication and execution within SPE and with NSPE.
Crypto, Internal Trusted Storage (ITS), Protected Storage (PS), and Firmware Update and Attestation Secure Services.
This enables the device to have secure connections with cloud services and protect sensitive data, keys, and certificates.
Peripherals and Devices With or Without CAN¶
The CC27xx also hosts a full range of peripherals across hardware variants including:
2x UART modules that uses universal asynchronous TX/RX functions with flexible baud-rate generation up to 3 MBPS and an IRDA SIR operation mode
2x SPI controllers and peripherals up to 12MHz with configurable phase and polarity
1x I2C to communicate with devices at 100KHz and 400KHz as a controller and/or a target
1x I2S for digital audio and pulse-density modulation microphones
1x VCE post-processing accelerator for fast and efficient Channel Sounding execution
1x Temperature and battery monitors
23 GPIOs, four with high-drive capability and ten with analog capabilities
1x 32-bit timer and 3x 16-bit timers
1x System timer
1x Watchdog timer
1x Real-time Clock
1x Low-power comparator
1x 12-bit ADC
1x Buck DC-DC converter
The CAN-FD module supports both CAN (1Mbps) and CAN-FD (controllable 5Mbps with 64B/frame)
Table 7. below shows the notable device differences.
Device |
CAN-FD |
Flash (kB) |
SRAM (kB) |
+20dBm PA |
|---|---|---|---|---|
CC2745P10-Q1 |
Yes |
1024 |
162 |
Yes |
CC2745R10-Q1 |
Yes |
1024 |
162 |
No |
CC2745R7-Q1 |
Yes |
768 |
128 |
No |
CC2744R7-Q1 |
No |
768 |
128 |
No |
Note
Industrial grade devices do not include CAN-FD support.
Flash and RAM¶
As shown in Table 7. above, the CC2745x10-Q1 contains 1024 kB of in-system programmable flash memory and 162 kB of no parity SRAM (or 144 kB with parity), whereas the CC274xx7-Q1 has 864 kB flash memory and 128 kB of SRAM. The flash is split into erasable pages of 2 kB. The CC27xx also contains 8 kB of cache SRAM that can be utilized to extend RAM capacity or can function as a normal cache to increase application performance.
Figure 45. SimpleLink™ CC27xx Block Diagram¶
Programming Internal Flash With the ROM Bootloader¶
The CC23xx or CC27xx internal flash memory can be programmed using the bootloader located in device ROM. Both UART and SPI protocols are supported. See the CC23xx SimpleLink Wireless MCU Technical Reference Manual for more details on the programming protocol and requirements.
Note
Because the ROM bootloader uses predefined DIO pins for internal flash programming, allocate these pins in the board layout. The CC23xx SimpleLink Wireless MCU Technical Reference Manual has more details on the pins allocated to the bootloader based on the chip package type.
Startup Sequence¶
For a complete description of the CC23xx or CC27xx reset sequence, see the CC23xx SimpleLink Wireless MCU Technical Reference Manual.
Resets¶
Note
Reset on the CC23xx or CC27xx may only be done by using hard resets. A hard reset turns off and on the device, resetting all the registers and memory. On the other hand, a soft reset restarts the microcontroller without losing RAM content.
From the software, this reset can be accomplished using Power_reset()
function call from the Power Manager driver (Power.h).
For more information, please review TI Drivers API Reference section.
// Import Power Driver definitions.
#include <ti/drivers/Power.h>
// Resets the system and causes it to reboot.
Power_reset();
In CCS, select Board Reset (automatic) from the reset menu:
Figure 46. Board Reset¶