33 #ifndef ti_drivers_rcl_hal_RCL_Hal__include 34 #define ti_drivers_rcl_hal_RCL_Hal__include 38 void RCL_Hal_initFsm(
void (*setupFsmCb)(
void),
void (*schedFsmCb)(
void),
39 void (*commandFsmCb)(
void));
uint32_t RCL_Hal_getHfxtRatioDefault(void)
Definition: RCLLPF3_Hal.c:529
uint32_t RCL_Hal_getCommandIfgReg(void)
Definition: RCLLPF3_Hal.c:110
uint32_t RCL_Hal_getCurrentTime(void)
Definition: RCLLPF3_Hal.c:188
void RCL_Hal_powerReleaseSwTcxoUpdateConstraint(void)
Definition: RCLLPF3_Hal.c:476
uint32_t RCL_Hal_getHfxtRatio(void)
Definition: RCLLPF3_Hal.c:524
int16_t RCL_Hal_getTemperature(void)
void RCL_Hal_powerSetStandbyConstraint(void)
Definition: RCLLPF3_Hal.c:449
void RCL_Hal_cancelSetupTime(void)
Definition: RCLLPF3_Hal.c:268
void RCL_Hal_triggerSchedulerFsm(void)
Definition: RCLLPF3_Hal.c:182
HalTimerEvent
Definition: RCL_Hal.h:72
void RCL_Hal_armCmdStartCap(void)
void RCL_Hal_setupCmdDoneCap(void)
RCL_PowerEvent
Definition: RCL_Hal.h:81
void RCL_Hal_setupHardStopTime(uint32_t stopTime)
Definition: RCLLPF3_Hal.c:225
void RCL_Hal_armCmdDoneCap(void)
void RCL_Hal_triggerCommandFsm(void)
Definition: RCLLPF3_Hal.c:170
void RCL_Hal_setupCmdStartCap(void)
void RCL_Hal_clearCommandRadioInterrupt(uint32_t mask)
Definition: RCLLPF3_Hal.c:367
uint8_t RCL_Hal_setDcdcIpeakSetting(uint8_t setting)
Definition: RCLLPF3_Hal.c:404
void RCL_Hal_disableAllCommandRadioInterrupts(void)
Definition: RCLLPF3_Hal.c:378
void RCL_Hal_disableAllDispatchRadioInterrupts(void)
Definition: RCLLPF3_Hal.c:384
void RCL_Hal_enableClkBuffer(void)
Definition: RCLLPF3_Hal.c:291
void RCL_Hal_enableSetupTimeIrq(void)
Definition: RCLLPF3_Hal.c:199
void RCL_Hal_powerClose(void)
Definition: RCLLPF3_Hal.c:498
void RCL_Hal_setTemperatureNotification(int16_t currentTemperature, uint16_t temperatureRange, void(*rclTemperatureNotify)(int16_t))
Definition: RCLLPF3_Hal.c:553
uint32_t RCL_Hal_getCmdStartCap(void)
void RCL_Hal_setupPacketTimeout(uint32_t stopTime)
void RCL_Hal_disableHardStopTimeIrq(void)
Definition: RCLLPF3_Hal.c:238
void RCL_Hal_setupStartTime(uint32_t startTime)
Definition: RCLLPF3_Hal.c:217
void RCL_Hal_powerSetSwTcxoUpdateConstraint(void)
Definition: RCLLPF3_Hal.c:468
uint32_t RCL_Hal_getCmdDoneCap(void)
void RCL_Hal_powerOpen(void(*rclPowerNotifyFunction)(RCL_PowerEvent))
Definition: RCLLPF3_Hal.c:489
uint32_t RCL_Hal_getDispatchIfgReg(void)
Definition: RCLLPF3_Hal.c:123
void RCL_Hal_enableGracefulStopTimeIrq(void)
Definition: RCLLPF3_Hal.c:250
void RCL_Hal_setupSetupTime(uint32_t setupTime)
Definition: RCLLPF3_Hal.c:204
void RCL_Hal_initFsm(void(*setupFsmCb)(void), void(*schedFsmCb)(void), void(*commandFsmCb)(void))
Definition: RCLLPF3_Hal.c:137
void RCL_Hal_cancelHardStopTime(void)
Definition: RCLLPF3_Hal.c:278
void RCL_Hal_cancelStartTime(void)
Definition: RCLLPF3_Hal.c:273
void RCL_Hal_cancelPacketTimeout(void)
void RCL_Hal_initDispatchRadioInterrupts(uint32_t mask)
Definition: RCLLPF3_Hal.c:355
void RCL_Hal_stopTemperatureNotification(void)
Definition: RCLLPF3_Hal.c:565
void RCL_Hal_armSyncFoundCap(void)
void RCL_Hal_powerReleaseStandbyConstraint(void)
Definition: RCLLPF3_Hal.c:458
void RCL_Hal_setRclClockEnable(uint16_t mask)
Definition: RCLLPF3_Hal.c:390
void RCL_Hal_setupSyncFoundCap(void)
Definition: RCLLPF3_Hal.c:299
void RCL_Hal_disableCommandRadioInterrupt(uint32_t mask)
Definition: RCLLPF3_Hal.c:372
void RCL_Hal_cancelGracefulStopTime(void)
Definition: RCLLPF3_Hal.c:283
void RCL_Hal_enableHardStopTimeIrq(void)
Definition: RCLLPF3_Hal.c:233
uint16_t RCL_Hal_getVddsVoltage(void)
void RCL_Hal_temperatureInit(void)
Definition: RCLLPF3_Hal.c:507
void RCL_Hal_triggerDispatchFsm(void)
Definition: RCLLPF3_Hal.c:176
void RCL_Hal_enableCommandRadioInterrupt(uint32_t mask)
Definition: RCLLPF3_Hal.c:361
void RCL_Hal_clearRclClockEnable(uint16_t mask)
Definition: RCLLPF3_Hal.c:397
uint32_t RCL_Hal_getSyncFoundCap(void)
HalTimerEvent RCL_Hal_checkClearTimerCompare(void)
Definition: RCLLPF3_Hal.c:310
void RCL_Hal_setupGracefulStopTime(uint32_t stopTime)
Definition: RCLLPF3_Hal.c:243