Radio Control Layer (RCL)
LRFLPF3_Interface_Generic.c File Reference
#include <stdint.h>
#include <ti/drivers/rcl/lrf/LRFLPF3_Interface_Generic.h>
#include <ti/drivers/rcl/commands/generic.h>
#include <ti/devices/DeviceFamily.h>
+ Include dependency graph for LRFLPF3_Interface_Generic.c:

Functions

void LRF_Interface_Generic_configOpNesbPrx (uint16_t lrfOpCfg, uint8_t addrLen, const RCL_ConfigAddress *syncWordCfg)
 
void LRF_Interface_Generic_updateSyncWordCfg (RCL_ConfigAddress *syncWordCfg)
 
void LRF_Interface_Generic_setModulationMode (uint32_t sendCw, uint32_t whitenMode, LRF_ModulationCtrl *modulationCtrl)
 
void LRF_Interface_Generic_disableSyncSearch (bool disableSyncWordA, bool disableSyncWordB, LRF_SyncSearchCtrl *syncSearchCtrl)
 

Function Documentation

§ LRF_Interface_Generic_configOpNesbPrx()

void LRF_Interface_Generic_configOpNesbPrx ( uint16_t  lrfOpCfg,
uint8_t  addrLen,
const RCL_ConfigAddress *  syncWordCfg 
)

Referenced by RCL_Handler_Nesb_Prx().

§ LRF_Interface_Generic_updateSyncWordCfg()

void LRF_Interface_Generic_updateSyncWordCfg ( RCL_ConfigAddress *  syncWordCfg)

Referenced by RCL_Handler_Nesb_Prx().

§ LRF_Interface_Generic_setModulationMode()

§ LRF_Interface_Generic_disableSyncSearch()

void LRF_Interface_Generic_disableSyncSearch ( bool  disableSyncWordA,
bool  disableSyncWordB,
LRF_SyncSearchCtrl *  syncSearchCtrl 
)