#include <stdint.h>
#include <ti/devices/DeviceFamily.h>
Go to the source code of this file.
§ LRF_INTERFACE_ENDCAUSE_STAT_ENDOK
| #define LRF_INTERFACE_ENDCAUSE_STAT_ENDOK (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ENDOK) |
§ LRF_INTERFACE_ENDCAUSE_STAT_RXTIMEOUT
| #define LRF_INTERFACE_ENDCAUSE_STAT_RXTIMEOUT (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_RXTIMEOUT) |
§ LRF_INTERFACE_ENDCAUSE_STAT_NOSYNC
| #define LRF_INTERFACE_ENDCAUSE_STAT_NOSYNC (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_NOSYNC) |
§ LRF_INTERFACE_ENDCAUSE_STAT_RXERR
| #define LRF_INTERFACE_ENDCAUSE_STAT_RXERR (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_RXERR) |
§ LRF_INTERFACE_ENDCAUSE_STAT_CONNECT
| #define LRF_INTERFACE_ENDCAUSE_STAT_CONNECT (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_CONNECT) |
§ LRF_INTERFACE_ENDCAUSE_STAT_MAXNAK
| #define LRF_INTERFACE_ENDCAUSE_STAT_MAXNAK (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_MAXNAK) |
§ LRF_INTERFACE_ENDCAUSE_STAT_SCANRSP
| #define LRF_INTERFACE_ENDCAUSE_STAT_SCANRSP (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_SCANRSP) |
§ LRF_INTERFACE_ENDCAUSE_STAT_EOPSTOP
| #define LRF_INTERFACE_ENDCAUSE_STAT_EOPSTOP (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_EOPSTOP) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_RXF
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_RXF (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_RXF) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_TXF
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_TXF (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_TXF) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_SYNTH
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_SYNTH (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_SYNTH) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_STOP
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_STOP (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_STOP) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_PAR
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_PAR (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_PAR) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_BADOP
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_BADOP (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_BADOP) |
§ LRF_INTERFACE_ENDCAUSE_STAT_ERR_INTERNAL
| #define LRF_INTERFACE_ENDCAUSE_STAT_ERR_INTERNAL (uint16_t)(PBE_COMMON_RAM_ENDCAUSE_STAT_ERR_INTERNAL) |
§ LRF_Interface_sendOp()
| static void LRF_Interface_sendOp |
( |
uint16_t |
op | ) |
|
|
inlinestatic |
§ LRF_Interface_programSyncWordA()
| static void LRF_Interface_programSyncWordA |
( |
uint32_t |
syncWord | ) |
|
|
inlinestatic |
§ LRF_Interface_programSyncWordB()
| static void LRF_Interface_programSyncWordB |
( |
uint32_t |
syncWord | ) |
|
|
inlinestatic |
§ LRF_Interface_getCmdEndCause()
| static uint16_t LRF_Interface_getCmdEndCause |
( |
void |
| ) |
|
|
inlinestatic |
§ LRF_Interface_isCmdEndCauseEopStop()
| static bool LRF_Interface_isCmdEndCauseEopStop |
( |
void |
| ) |
|
|
inlinestatic |
§ LRF_Interface_isCmdEndCauseEndOk()
| static bool LRF_Interface_isCmdEndCauseEndOk |
( |
uint16_t |
endCause | ) |
|
|
inlinestatic |
§ LRF_Interface_isCmdEndCauseEndedWithoutSync()
| static bool LRF_Interface_isCmdEndCauseEndedWithoutSync |
( |
uint16_t |
endCause | ) |
|
|
inlinestatic |