|
Radio Control Layer (RCL)
|
#include <stdint.h>#include <stdlib.h>#include <ti/drivers/rcl/RCL_Command.h>#include <ti/drivers/rcl/RCL_Debug.h>#include <ti/drivers/rcl/LRF.h>#include <ti/log/Log.h>
Include dependency graph for LRF.c:Functions | |
| LRF_SetupResult | LRF_loadImage (const LRF_TOPsmImage *image, uint32_t destinationAddress) |
| void | LRF_initSettingsState (LRF_ApplySettingsState *state, LRF_ApplySettingsBase includeBase, uint16_t phyFeatures) |
| LRF_SetupResult | LRF_applySettings (LRF_ConfigWord *config, LRF_ApplySettingsState *state, int32_t bufferAvailWords) |
| LRF_TxPowerTable_Entry | LRF_TxPowerTable_findValueExtended (const LRF_TxPowerTable *table, LRF_TxPowerTable_Index powerLevel, bool roundUp, bool returnBoundaryOnOutOfRange) |
| Search for settings corresponding to tx power in the tx power table with extended options. More... | |
| LRF_SetupResult LRF_loadImage | ( | const LRF_TOPsmImage * | image, |
| uint32_t | destinationAddress | ||
| ) |
References SetupResult_ErrorImageLen, SetupResult_Ok, and TOPSM_RAM_SZ.
Referenced by __attribute__().
| void LRF_initSettingsState | ( | LRF_ApplySettingsState * | state, |
| LRF_ApplySettingsBase | includeBase, | ||
| uint16_t | phyFeatures | ||
| ) |
References LRF_ApplySettingsState::includeBase, LRF_resetSettingsState(), and LRF_ApplySettingsState::phyFeatures.
Referenced by __attribute__(), and LRF_resetSettingsState().
| LRF_SetupResult LRF_applySettings | ( | LRF_ConfigWord * | config, |
| LRF_ApplySettingsState * | state, | ||
| int32_t | bufferAvailWords | ||
| ) |
References HW_Region_Clear, HW_Write_16bit, HW_Write_16bit_masked, HW_Write_16bit_sparse, HW_Write_32bit, LRF_ApplySettingsState::includeBase, LRF_ApplySettings_NoBase, LRF_BASE_ADDR, LRF_RegionOperation_Invalid, LRF_RegionOperation_Skip, LRF_ConfigWord::masked, MAX_REG_CONFIG_LEN, Par_Reference_32bit, Par_Region_Clear, Par_Write_32bit, PBE_RAM_BASE_ADDR, LRF_ApplySettingsState::phyFeatures, RCL_Debug_assert, LRF_ConfigWord::region, LRF_ConfigWord::segment, SetupResult_ErrorConfigLen, SetupResult_ErrorElemAddrAlign, SetupResult_ErrorElemLen, SetupResult_ErrorElemType, SetupResult_ErrorParRange, SetupResult_Ok, SetupResult_Ok_Partial, LRF_ConfigWord::sparse, SW_Region_Clear, SW_Write_16bit, SW_Write_16bit_sparse, SW_Write_32bit, swParamList, swParamListSz, LRF_ConfigWord::value16, and LRF_ConfigWord::value32.
Referenced by __attribute__(), and LRF_resetSettingsState().
| LRF_TxPowerTable_Entry LRF_TxPowerTable_findValueExtended | ( | const LRF_TxPowerTable * | table, |
| LRF_TxPowerTable_Index | powerLevel, | ||
| bool | roundUp, | ||
| bool | returnBoundaryOnOutOfRange | ||
| ) |
Search for settings corresponding to tx power in the tx power table with extended options.
| table | pointer to the tx power table to be searched |
| powerLevel | requested power level |
| roundUp | decides if round up or down when an exact match is not found |
| returnBoundaryOnOutOfRange | if true, return boundary values instead of invalid when out of range |
References LRF_getRawTxPower(), LRF_TxPower_Use_Max, LRF_TxPower_Use_Min, LRF_TxPower_Use_Raw, LRF_TxPowerEntry_INVALID_VALUE, LRF_TxPowerTable::numEntries, LRF_TxPowerTable_Entry::power, LRF_TxPowerTable::powerTable, and LRF_TxPowerTable_Index::rawValue.
Referenced by LRF_resetSettingsState(), LRF_TxPowerTable_findValue(), and RCL_txPowerLookup().