SimpleLink™ Low Power F3 SDK 9.12.00.19 Release Notes
Table of Contents
Introduction
The SimpleLink™ Low Power F3 Software Development Kit (SDK) delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC23xx and CC27xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC23xx and CC27xx wireless MCU users by packaging essential software components, such as:
- Bluetooth® Low Energy (BLE) protocol stack
- Zigbee® protocol stack supporting low power wireless mesh networks
- Proprietary RF layer
- TI Drivers
All of the above are provided in one easy-to-use software package along with example applications and documentation.
The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit TI SimpleLink Wireless Connectivity.
This is version 9.12.00.19 of the SimpleLink Low Power F3 SDK.
Supported Features and Limitations
CC23xx
| TI Crypto Driver Overview | Support Status | Additional Comment |
|---|---|---|
| AES-CCM | Supported | |
| AES-ECB | Supported | AESECB_oneStepDecrypt, AESECB_setupDecrypt not supported |
| AES-GCM | Supported | |
| AES-CTR | Supported | |
| AES-CBC | Supported | AESCBC_oneStepDecrypt, AESCBC_setupDecrypt not supported |
| AES-CTR-DRBG | Supported | |
| AES-CMAC | Supported | |
| SHA-256 | Supported | |
| ECDH | Supported | |
| ECIES | Supported | |
| RNG | Supported | |
| TRNG | Not Supported |
CC27xx
| TI Crypto Driver Overview | Support Status | Additional Comment |
|---|---|---|
| AES-CCM | Supported | HSM |
| AES-ECB | Supported | HSM |
| AES-GCM | Supported | HSM |
| AES-CTR | Supported | HSM |
| AES-CBC | Supported | HSM |
| AES-CTR-DRBG | Not Supported | This is supported via RNG |
| AES-CMAC | Supported | HSM |
| ECDH | Supported | HSM |
| ECDSA | Supported | HSM |
| RNG | Supported | HSM (AES-CTR-DRBG) |
| TRNG | Supported | HSM |
LAES & HSM Limitations
The CC27xx family of devices now include a Hardware Security Module (HSM) for cryptographic and key storage features.
For crypto drivers that support the HSM and LAES, a failure in the HSM bootup process will be cached in the driver’s handle or will return a NULL handle (AESGCM, ECC, RNG Drivers). If the user attempts to perform an HSM operation later, it will return an error due to the cached initialization error. LAES operations would continue to function without issue in that case.
For drivers that support running operations on both hardware accelerators, for primarily AES drivers, a switch has been implemented so that the driver knows which engine to use to execute the operation on. This switch is part of the cryptography operation’s key. The key encoding of each key, part of the input parameters to drivers’ APIs, holes the value of the engine-of-choice.
- To leverage the HSM hardware accelerator, the user has to call ‘CryptoKeyPlaintextHSM_initKey(..)’ or ‘KeyStore_PSA_initKeyHSM(..)’ API and pass in the plaintext key as well as the key length.
- To leverage the LAES hardware accelerator, the user has to call ‘CryptoKeyPlaintext_initKey()(..)’ API and pass in the plaintext key as well as the key length.
NOTE:
- Please refer to each driver’s top level header file for driver-specific limitations.
- Mass erasing the CC27xx without retaining protected sectors will result in the erasure of the HSM firmware. Please see the Quick Start Guide: Build your first program for the CC23xx or CC27xx device on how to re-flash the HSM firmware.
- Starting SDK version 9.10, the crypto drivers are removed from the drivers library and moved into a separate secure drivers library: source/ti/drivers/secure/lib.
- Starting SDK version 9.10, if SysConfig generated libraries linker is not used, the secure drivers library will need to be added manually into the respective linker settings.
Documentation
What’s New
- Production-ready release for CC2745R10-Q1 E1, CC2744R7-Q1, CC2755R10, CC2745R7-Q1, CC2745P10-Q1 and CC2340R53-Q1 including finalized characterized RF settings.
- Bluetooth LE Channel Sounding preview.
Note: The ble_toolbox GUI for Channel Sounding and Connection Monitor is not yet functional. The GUI will be enabled in a future release.
Refer to the Document Overview for the individual release notes and details for starting development with each SDK component.
Migration to CCS v20+ (Theia)
Starting from 9.10 SDK, CCS v20+ (Theia) is the only supported CCS IDE. Please see Migration Guide for help migrating from CCS Eclipse IDE to CCS v20+ (Theia).
Documentation and Video collateral can be found here:
- Getting Started Video
- CCS Academy
- Migration Guide
- CCS User’s Guide
- Getting Started Video
- Quick Tip Videos
Transition Roadmap
| Version | Date | CCS IDE support |
|---|---|---|
| 8.10 and 8.20 | 1H 2024 | CCS 12.x is the primary development environment. CCS v20+ (Theia) is also supported, but may have minor feature gaps. |
| 8.40 | 2H 2024 | CCS v20+ (Theia) is the primary development environment. CCS 12.x is deprecated - that is, it’s supported, but not recommended. |
| 9.10 and later | 2025 | CCS v20+ (Theia) is the only supported CCS IDE. |
For more information on CCS v20+ (Theia), see the CCS v20+ (Theia) Users Guide.
Operating System Support
- Microsoft® Windows® 10
- Ubuntu 22.04 LTS 64-bit
- macOS 13.x
Dependencies
The sample applications included in this SDK were built & tested with the IDEs and listed below:
- TI Code Composer Studio: CCS 20.1.0
- TI ARM Clang Compiler: 4.0.2.LTS
- SysConfig: 1.23.01
- UniFlash: 9.0.0
- IAR Embedded Workbench: 9.60.3
Compiler Settings: Default CCS configurations (optimization level z)
Note: Earlier IDE/toolchain versions are not supported and compatibility with newer versions of supported IDEs is not assured.
Device Support
This SDK supports the following SimpleLink CC23XX and CC27XX wireless MCUs:
| Device | Orderable Part Number (OPN) | LaunchPad | Product Page | Migrate from these examples |
|---|---|---|---|---|
| CC2340R5RKP | CC2340R52E0RKPR, CC2340R52N0RKPR | LP-EM-CC2340R5 | CC2340R5 | N/A |
| CC2340R5RGE | CC2340R52E0RGER, CC2340R52N0RGER | N/A | CC2340R5 | LP-EM-CC2340R5 |
| CC2340R5RHB-Q1 | CC2340R52E0WRHBRQ1 | N/A | CC2340R5-Q1 | LP-EM-CC2340R5 |
| CC2340R53RKP | CC2340R53E0RKPR, CC2340R53N0RKPR | LP-EM-CC2340R53 | CC2340R5 | N/A |
| CC2340R53RHB-Q1 | CC2340R53E0WRHBRQ1 | N/A | CC2340R5 | LP-EM-CC2340R53 |
| CC2340R22RKP* | CC2340R22E0RKPR, CC2340R22N0RKPR | N/A | CC2340R2 | LP-EM-CC2340R5 |
| CC2340R2RGE* | CC2340R21N0RGER | N/A | CC2340R2 | LP-EM-CC2340R5 |
| CC2745R10-Q1 | CC2745R10E0WRHARQ1 | LP-EM-CC2745R10-Q1 | CC2745R10-Q1 | N/A |
| CC2745R10-Q1 | CC2745R10E1WRHARQ1 | LP-EM-CC2745R10-Q1 | CC2745R10-Q1 | N/A |
| CC2755R10 | CC2755R105E0WRHAR | N/A | CC2755R10 | LP-EM-CC2745R10-Q1 |
| CC2744R7-Q1 | CC2744R74E0WRHARQ1 | N/A | CC2744R7-Q1 | LP-EM-CC2745R10-Q1 |
Note *CC2340R2x only supports Bluetooth Low Energy stack and PropRF stack examples, and does not support Zigbee stack.
Note Use SysConfig to obtain the proper configuration to migrate the project to target board.
The project configuration for each of the device variants mentioned can be obtained starting from the examples projects included in this SDK and using SysConfig migration GUI.
Examples of migration pathways:
- A LaunchPad containing the device that this SDK provides examples for, or
- A LaunchPad this SDK provides examples for that can be used to SysConfig-migrate to the device.
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.