Adjusting CC23xx or CC27xx txPower¶
To optimize application power budget or performance, it is important to change the txPower to achieve the following scenario.
When peer devices are in close range, reduce the TX power can save the power budget.
When you want your device to increase range by increasing the TX power.
Increase the visibility of your application in a crowded environnement
Note
Note that for CC23xx or CC27xx the TX power range goes from -20dBm to 8dBm.
Changing txPower for an advertising set¶
SysConfig can be used to modify the TxPower used for each advertising set.
Open the sysconfig file of your example
Go to RF Stacks > BLE > Advertisement Set > Advertisement Parameters
Change the TX Power field from
The Controller will choose the Tx powertoTX Power ValueA new field appears below called TX Power Value, enter the value in dBm.
Figure 36. txPower configuration¶
Changing txPower at run time¶
To modify the txPower at running time, use the HCI command: HCI_EXT_SetTxPowerDbmCmd(int8 txPower, uint8 fraction)
The txPowerDbm parameter corresponds to the power in dBm value, the fraction is currently not used.
Find more details concerning the HCI function in the
API references section of the user’s guide.
Note
To check whether the txPower value has been updated you can either:
Check the current consumption: the higher the current consumption indicates higher the txPower.
Check the RSSI value: smaller RSSI indicates lower txPower.
RSSI will also vary by environment and that assuming all variables are equal and the devices are in the same location.
Lowering the txPower will lead to a smaller (more negative) RSSI.
HCI_EXT_SetTxPowerDbmCmd(int8 txPower, uint8 fraction)will have no impact on DTM test functions.
Changing txPower for DTM¶
To modify the txPower in DTM for the purpose of running DTM tests, use the HCI command: HCIExt_SetMaxDtmTxPowerDbmCmd(int8 txPower, uint8 fraction)
The txPowerDbm parameter corresponds to the power in dBm value, the fraction is currently not used (i.e. should be set to 0).
Find more details concerning the HCI function in the
API references section of the user’s guide.
Note
When changing txPower using this method, only the DTM test functions such as EnhancedModemTestTxCmd and
HCIExt_ModemTestTxCmd will have the new txPower.
HCIExt_SetMaxDtmTxPowerDbmCmd(int8 txPower, uint8 fraction) will have no impact on the txPower used for
non-DTM functionality such as advertising, connections, etc.
Power Control Feature¶
The Power Control Feature enable us to keep channels less noisy and to save power. The feature enable the option to query the peer device for what is the Accepted Power Reduction (APR) on an active connection and to reduce the amount of power the peer device allows in the connection. The detailed defination of Power Control Request procedure is found in the Bluetooth Core Specifications Version 5.3, Vol 6, Part B, Chapter 5.1.
Depending on the RSSI Monitor feature implemented, there will be an option to enable a monitor of the RSSI value on a specific connection and to ask the peer device autonomously to decrease or increase its power respectively to the RSSI that local device receive in the connection.
Once the power control procedure is done, the TX power changes to the value that was decided for all connection events on a specific connection handle and a specific PHY until another power procedure occurs or the connection is lost.
The power control procedure can be triggered from the host/application layer by the HCI command, or by the peer device in which case the procedure is handled in the controller layer and notify the host/application if configured. Related HCI commands are listed in below. More details about HCI function are in the API references section of the user’s guide.
HCI_LE_EnhancedReadTransmitPowerLevelCmd ( uint16_t connHandle, uint8_t txPhy )
HCI_LE_ReadRemoteTransmitPowerLevelCmd ( uint16_t connHandle, uint8_t txPhy )
HCI_LE_SetTransmitPowerReportingEnableCmd ( uint16_t connHandle, uint8_t localEnable, uint8_t remoteEnable )
HCI_EXT_SendPowerControlRequestCmd ( uint16_t connHandle, uint8_t txPhy, uint8_t deltaPowerDb, uint8_t aprEnable )