Zigbee Configuration¶
These instructions cover all Zigbee sample applications. Configurables differ between standard Zigbee device types (ie. Coordinator, Router, End Device, ZNP) and Green Power Devices (GPD).
Note
SysConfig will only make changes to selected files, listed in the Generated Files view. Any required changes to your application files must be done on your own.
Open An Example Project¶
Open the stand-alone SysConfig tool or import a SysConfig-enabled example project
(found in the {SDK_INSTALL_DIR}/examples/rtos/<board>/zigbee folder) and open the
.syscfg file with the System Configuration Editor.
Zigbee Settings¶
In the RF STACKS → Z-Stack view, you can configure Zigbee stack parameters.
Parameters are explained in the tooltip that appears when you hover over it but
further explanations are provided in the Zigbee 3.0 Overview and
4. Migrate Configuration Header File sections.
Zigbee stack settings are stored in default/sysconfig/ti_zigbee_config.h
(which appears after building the project).
Here is an example of what you would see for an End Device switch example:
Generic Zigbee Options¶
Enable Logging: Enables logging capability for both the Zigbee application and stack.
Zigbee Pro 3.0 Revision: Option to choose between the Zigbee PRO 2017 (R22) or PRO 2023 (R23) specification
Enabled Device Types: The Device Type (Coordinator, Router, End Device, Green Power Device) can be selected. Certain combinations are not supported, like a ZC plus ZED.
Enable Green Power Direct Support: Ability to receive any Green Power frame in both direct or tunneled modes.
Enable use of APIs to Join a Pre-Installed Network: Allow factory new
devices to join using pre-installed network parameters using the APIs in
zb_bdb_preinst_nwk.h
Power Management (ZED only)¶
Power Mode of Operation of ZED: Enabled sleepy or Always-on ZED operation.
Poll Period: Frequency of ZED Data Requests to its parent.
Radio Configuration¶
Primary Channels: Selection of channels for which the Zigbee device forms a network or searches for a network to join.
Transmit Power: Default transmit power in units of dBm.
Network Configuration¶
Default Network Key: Set to 0 to generate a random network key
End Device Timeout: Time after the latest data poll for which a ZED is removed from its parent’s association table.
Green Power Device: Green Power Device Type determines what function the GPD embodies in the network (eg. switch, temperature sensor, etc). Green Power Device ID Type determines how the GPD identifies itself (eg. Configurable GPD ID, IEEE address). If Configurable GPD ID is selected, the developer may choose a 32-bit ID which the GPD will use (sec-green-power-device).
Security Configuration (GPD only)¶
Security settings which are specific towards Green Power devices, such as level and key type, and key, which are further discussed in sec-green-power-security.
Advanced Configuration (GPD only)¶
Data Frame Retries determines how many times the GPD will transmit each packet. Auto-commissioning determines whether the GPD will set the auto-commissioning bit in the packets (sec-green-power-commissioning). Radio Receive After Transmit determines whether the GPD should expect to receive a packet after transmitting. Sequence Number Capability determines whether the GPD will use sequential MAC sequence numbers (sec-green-power-data-frames).
Adjust Your Application¶
When you have finished adjusting the parameters, save the .syscfg file.
You can preview the files which will be generated by clicking the <> symbol. In this example,
ti_devices_config.c, ti_drivers_config.c/h, and ti_zigbee_config.h were generated respectively
by the TI DEVICES, TI DRIVERS, and RF STACKS → Zigbee views.
If you are using the System Configuration stand-alone tool, you will have to
import every generated file to your IDE. For the SysConfig CCS plug-in,
you can generate all the files by building your project. After the build has
completed, you will find the generated files in the output folder of your project,
called default/syscfg. All parameters configured in the Zigbee view of
SysConfig will result in a #define in ti_zigbee_config.h alongside other macros
which are not included in SysConfig.
Attention
Whenever you re-build the project, SysConfig will re-generate the files.
Because of this, any changes made directly to ti_zigbee_config.h will be overwritten.