Custom Hardware¶
This section will explain how to adapt a Zigbee 3.0 application from the SimpleLink Low Power F3 SDK to run on custom hardware. In general, the steps required to migrate a Zigbee 3.0 application from a development kit to a custom board are minimal and involve changing the pin configuration as well as selecting the correct RF configuration. These steps, including a bring up guide, are detailed in the subsections below.
Designing a Custom Board¶
Design guidelines for CC13x2 and CC26x2 boards can be found in the CC13xx/CC26xx Hardware Configuration and PCB Design Considerations app note. This app note includes RF front-end, schematic, PCB, and antenna design considerations. The report also covers crystal oscillator tuning, optimum load impedance as well as a brief explanation of the different power supply configurations.
Note
A similar app note will be produced for the CC23xx or CC27xx devices. In the meantime, we recommend leveraging the reference designs available in the MSR folder.
Creating a Custom Board File¶
Board files are used by TI drivers to store device specific settings and I/O
mapping. The board file abstraction allows one TI-drivers implementation
to support many hardware implementations by just setting up new board files.
Examples utilize SysConfig to generate these board files. The generated
structures are placed in the ti_drivers_config.c and ti_drivers_config.h
files. The SysConfig user interface can be utilized to determine pins and
resources used. Information on pins and resources used is also present in both
of these generated files. It is recommended to use SysConfig to generate the
board files for custom hardware as described
here.
For the CC27xx, a Sleep Clock Accuracy (SCA) of 500 ppm can be achieved by measuring LFOSC to HFXT and periodically calibrating the LFOSC. This can be done by doing the following:
1. Set
Enable LFOSC CompensationinSysConfig->TI Devices->Device Configuration->LFOSC Compensation.
Click on
AddunderLFOSC Compensation Profiles.Fill in the parameters for
LFOSC Compensation Profilesaccording to your system requirments. For BLE applications,System PPM Requirementshould be set to maximum 500 ppm.
RF Temperature Compensation¶
If the selected HFXT source is not accurate enough for the selected RF protocol,
RF temperature Compensation may be enabled via SysConfig → TI Devices
→ Device Configuration. RF Temperature Compensation compensates HFXT frequency
for temperature during radio transmissions. This improves the accuracy of the
CLKSVT and CLKREF over temperature.
Note
Each crystal will have different parameters. You may request the parameters for your specific crystal by contacting the crystal vendor/manufacturer.
HFXT Compensation Threshold: HFXT will only be automatically compensated when the measured device temperature exceeds this threshold (in degrees Celsius). This can help to reduce power consumption if temperature compensation is not required below a certain temperature. If set to -41, then compensation will be enabled across the entire operating temperature range of [-40, +125].
HFXT Compensation Delta: HFXT will be automatically compensated if the temperature drifts more than this delta-value in either direction (in degrees Celsius). For example, if the temperature is measured to 30 degrees when the device boots (measured within
Board_init()), but later drifts to 30 + delta or 30 - delta, then HFXT temperature compensation will be performed, and the temperature setpoint updated accordingly.Note
Temperature is calculated using the Temperature driver. Please see :tidrivers_api:`Temperature.h` for more information.
Configuring Device Parameters for Custom Hardware¶
Set parameters, such as the sleep clock accuracy of the 32.768-kHz crystal.
Define the CCFG parameters in Device Configuration in SysConfig.
Note
For a description of CCFG configuration parameters, see the CC23xx SimpleLink Wireless MCU Technical Reference Manual.
HFXT Amplitude Compensation¶
High Frequency Crystal (HFXT) Amplitude Compensation feature adjusts the power amplitude to ensure the high frequency crystal receives sufficient power. The standard HFXT Amplitude Compensation is always enabled - the CC23xx or CC27xx power driver takes care of this.
HFXT Amplitude Compensation: At boot within
Power_init(), HFXT amplitude is configured to the highest possible value. After this, HFXT amplitude is adjusted to the optimal value each time the device enters standby. It will take up to five iterations after boot until the optimal amplitude is found. This process ensures that the amplitude remains in an optimal range if operating conditions change. This feature will always be enabled, unless Initial HFXT Amplitude Compensation is enabled.Initial HFXT Amplitude Compensation: If the application rarely enters standby, initial HFXT Amplitude Compensation can be enabled when the application requires the optimal amplitude to be found at or after boot. HFXT will take longer to be ready after boot, but when ready the amplitude is already in the optimal range. This process is done asynchronously and is enabled via
SysConfig→TI Devices→Device Configuration→Initial HFXT Amplitude Compensation.Note
Enabling initial HFXT amplitude compensation will result in more flash usage and a longer time from boot to first RF operation.
Initial Board Bring Up¶
When powering up a custom board with the CC23xx or CC27xx for the first time, it is recommended to follow the Board Bring-Up section on CC13xx/CC26xx Hardware Configuration and PCB Design Considerations. After confirming that the board is being powered correctly by the battery or power supply and can be identified by the SWD tool, programming the device with a minimal SW application to verify stability is also suggested.
Using the RGE QFN24 package variant¶
The CC23xx or CC27xx is also available with a 4-mm x 4-mm RGE QFN24 (12 GPIOs) package variant. See the CC23xx Datasheet for all the package options and IO descriptions.
In order to build SimpleLink Low Power F3 SDK project using the RGE package, a few settings must be made in SysConfig.
First open the SysConfig file, click the icon on the top right hand corner
Show Board ViewClick the button
SWITCHSelect
NONEin the Board | New Value fieldSelect the
CC2340R5RGEdevice in the Device field. It automatically updates the package toRGE.Finally click
CONFIRM
Figure 33. Switch to RGE Package¶
After clicking CONFIRM, the pins of the SysConfig file may change. If error
messages appear, check that the pins changed in SysConfig are consistent with
the implemented hardware design.
Figure 34. Check the new configuration generated by SysConfig¶
For each error, review the suggested configuration value, and accept it or modify it.
Tuning HFXT capacitors¶
One of the features offered by SmartRF Studio 8 is the ability to tune the HFXT capacitors. Generally the RF link could be affected by variations in hardware, this is normally difficult to fix; however with HFXT the RF link can be adjusted by changing the two capacitor values in SmartRF Studio 8.
Tip
TI recommends tuning the HFXT capacitors values for the design. The RF performances improvements obtained by tuning the HFXT capacitors values for each unit on the production line generally do not justify the complexity and added costs.
- Download the latest SmartRF 8 Studio
Open SmartRF Studio 8 and open the target device
3. Select the RF settings used by your design. Once SmartRF Studio 8 is open you can view and select various PHYs, to edit a PHY you will need to create a new PHY by clicking on the box next to the PHY name.
4. You can edit various settings on the PHY properties page such as the custom name, frequency, sync word, and tx power.
To tune HFXT cap-array tuning change disable to enable and then edit values as needed.
6. To implement the HFXT capacitors values found in the embedded code, open the project in your favorite IDE open the SysConfig file -> Device Configuration and click on “Override HFXT Cap Array Trims” and input the two values found.