49 #ifndef ti_drivers_uart2_UART2LPF3__include 50 #define ti_drivers_uart2_UART2LPF3__include 58 #include <ti/devices/DeviceFamily.h> 59 #include DeviceFamily_constructPath(inc/hw_types.h) 60 #include DeviceFamily_constructPath(driverlib/udma.h) 71 #define UART2LPF3_FIFO_SIZE 8 UART2LPF3_CodingScheme codingScheme
Definition: UART2LPF3.h:161
int32_t rtsPinMux
Definition: UART2LPF3.h:159
PRELIMINARY UART driver interface
uint32_t txChannelSubscriberId
Definition: UART2LPF3.h:166
uint8_t txChannelEvtMux
Definition: UART2LPF3.h:163
uint8_t rxChannelEvtMux
Definition: UART2LPF3.h:164
Definition: UART2LPF3.h:85
int32_t rxPinMux
Definition: UART2LPF3.h:157
Definition: UART2LPF3.h:83
Definition: UART2LPF3.h:84
UART2LPF3 Hardware attributes.
Definition: UART2LPF3.h:149
Semaphore module for the RTOS Porting Interface.
UART2_BASE_OBJECT Power_NotifyObj preNotify
Definition: UART2LPF3.h:178
uint32_t rxChannelSubscriberId
Definition: UART2LPF3.h:167
uint8_t irLPClkDivider
Definition: UART2LPF3.h:162
struct UART2LPF3_Object * UART2LPF3_Handle
int32_t txPinMux
Definition: UART2LPF3.h:156
uint32_t txChannelMask
Definition: UART2LPF3.h:154
UART2LPF3_CodingScheme
UART TXD/RXD encoding/decoding scheme.
Definition: UART2LPF3.h:81
Power notify object structure.
Definition: Power.h:441
volatile uDMAControlTableEntry * dmaRxTableEntryPri
Definition: UART2LPF3.h:153
int32_t ctsPinMux
Definition: UART2LPF3.h:158
PowerLPF3_Resource powerID
Definition: UART2LPF3.h:160
UART2LPF3 Object.
Definition: UART2LPF3.h:175
uint32_t rxChannelMask
Definition: UART2LPF3.h:155
UART2_BASE_HWATTRS volatile uDMAControlTableEntry * dmaTxTableEntryPri
Definition: UART2LPF3.h:152
Hardware Interrupt module for the RTOS Porting Interface.
bool concatenateFIFO
Definition: UART2LPF3.h:165
Power_NotifyObj postNotify
Definition: UART2LPF3.h:179